# Troubleshoot

> **Deprecation Notice**
> This page describes features that have been removed or replaced in Luxonis Hub. Functionality may be limited and only available to Hub Original customers. Please refer to the up-to-date guides to provision devices, manage fleets, and deploy applications.

## Agent status

If the device is not connecting to the cloud, you can check agent status. Connect to the device via SSH and run:

```bash
hubctl status
```

You will receive information regarding whether the agent is running, if it is connected to the cloud, and a direct link to the
device page in the cloud. The output should look like this:

```bash
$ hubctl status
╔═══════════════════════════════════════════════════════════════╗
║                                                               ║
║ Luxonis Hub Agent (24.55.1308 | linux/arm64 | DepthAI 2.21.2) ║
║                                                               ║
╚═══════════════════════════════════════════════════════════════╝

Web UI                   https://localhost:9010
DepthAI                  2.21.2

Connected to cloud?      yes (https://hub.luxonis.com)
Team                     Luxonis
Pending detections       0

Link to robot in cloud
https://hub.luxonis.com/robots/00000000-0000-0000-0000-000000000000
```

For more information how to use the CLI, please navigate to its [documentation
page](https://docs.luxonis.com/cloud/advanced/legacy/hub-agent/cli.md).

## Agent logs

Agent logs are accessible via SSH or if connected to the Hub through the `Web Terminal` on the device detail page. For information
on how to work with the logs via SSH, please run:

```bash
hubctl help logs
```

## Application logs

When you start the application, logs are available in the `Logs` tab within the application details. You can copy the logs from
there as text if necessary.

## Support file

For uploading support file to Luxonis please use:

```bash
hubctl upload-support
```

Support files are encrypted. For analysis, please copy the hash from the command output and provide it to the Luxonis support
team.

## Frequent problems

### Unable to install application - no such host

A common reason the application cannot be installed is due to DNS resolution issues. The DNS server used by the host system, where
the agent is installed, might be unable to resolve the correct IP address of the GitHub repository needed for the installation. In
such cases, you might encounter a similar `no such host` message in the error log:

```bash
time="2024-05-30T10:23:50+08:00" level=warning msg="Failed to decode the keys [\"storage.imagestore\"] from \"/home/robothub/storage.conf\""
2Error: initializing source docker://ghcr.io/luxonis/robothub-app-v2:2024.117.2129-rvc2-regular: Get "https://ghcr.io/token?scope=repository%3Aluxonis%2Frobothub-app-v2%3Apull&service=ghcr.io": dial tcp: lookup ghcr.io on 192.168.0.1:53: no such host
```

The best solution is to use a public DNS service. There are two options for configuring DNS settings:

Local settings

The first possibility is to set the DNS resolver on the local machine. On a Debian-based system, you can modify the
`/etc/systemd/resolved.conf` file to change the `DNS` and `FallbackDNS` keys. This can also be done through your system's GUI,
making it unnecessary to update configuration files manually.

> **Note**
> This will cause that local network addresses will not be resolved. Use with caution.

Router settings

Another option is to change the DNS settings on your router. This ensures that all devices connected to the network use the same
DNS settings, providing consistency and simplifying management. To do this, you will need access to your router's administration
interface.

Recommended public DNS services

We recommend using `Google Public DNS` or Cloudflare's `1.1.1.1`. You can find step-by-step instructions here:

 * [Google Public DNS](https://developers.google.com/speed/public-dns/docs/using#linux)
 * [1.1.1.1](https://one.one.one.one/dns)