# OCR

> **Deprecation Notice**
> This page describes features that have been removed or replaced in Luxonis Hub. Functionality may be limited and only available to Hub Original customers. Please refer to the up-to-date guides to provision devices, manage fleets, and deploy applications.

This application leverages Optical Character Recognition (OCR) technology to seamlessly extract text from images, particularly
focusing on book covers and spines. By employing advanced neural networks, the application efficiently detects text within images
and recognizes it accurately.

[Video: OCR](https://docs.luxonis.com/static/videos/cloud/OCR.webm)

The OCR process consists of two crucial stages: text detection and text recognition. The text detection model operates directly on
the camera feed, swiftly identifying text regions within the image. Once detected, the text regions are then passed to the text
recognition model, which runs on the host system. This model deciphers the text, converting it into machine-readable format.

![OCR pipeline](https://docs.luxonis.com/static/images/cloud/OCR_reader_pipeline.webp)

The application offers [Open Library](https://openlibrary.org/) integration. It conducts searches based on the recognized text,
retrieving information about the identified books.

The application features a user-friendly frontend interface. Users can easily capture images of book covers or spines using their
device's camera. The application then promptly processes these images, presenting the extracted text in a clear and organized
manner on the frontend.

### View source code

[View source code](https://github.com/luxonis/robothub-examples/tree/main/Luxonis%20Apps/OCR%20reader)