# Video recording

> **Deprecation Notice**
> This page describes features that have been removed or replaced in Luxonis Hub. Functionality may be limited and only available
to Hub Original customers. Please refer to the up-to-date guides to provision devices, manage fleets, and deploy applications.

## Description

Functionality Overview

In addition to its core functionalities, the application offers extended features for video management. Users can choose to stream
the live video feed to a separate frontend application, providing a designated viewing interface. The application also allows for
manually triggered recordings, enabling users to capture specific moments of the video stream. Furthermore, for those seeking more
granular control, the system provides the ability to save the last five minutes of the stream. Advanced configuration options are
also available within the Hub's application configuration tab, allowing users to tailor the application's behavior to their
specific needs.

### View source code

[View source code](https://github.com/luxonis/robothub-examples/tree/main/Luxonis%20Apps/Video_Recording)