# Get started

> **Deprecation Notice**
> This page describes features that have been removed or replaced in Luxonis Hub. Functionality may be limited and only available
to Hub Original customers. Please refer to the up-to-date guides to provision devices, manage fleets, and deploy applications.

### Prerequisites

 * an OAK connected to Luxonis Hub ([Connect OAK](https://docs.luxonis.com/cloud/hub/connect-oak.md))

### Generate the app

Head over to the [Luxonis Hub website](https://hub.luxonis.com/control/apps/team-apps) and head to Apps.

Click on Create App and fill out the name. Pick one of [available templates](https://github.com/luxonis/robothub-app-templates)
(if don't know choose Video Stream).

Click on Create.

In a few seconds the application should appear in the list of your team apps.

### Install the app in development mode

Navigate to the detail of the Device on which you want to develop the app. Click on Apps and then Install App. In the dialog
window select Develop.

Choose the app that you just created and the only version that is available.

Select the OAK device that you want to use for development and click on Install with selected.

Once the app Status shows as Stopped its ready to be used for development.

### Open Luxonis Studio

Click on the application you just installed, which opens the detail page.

In the right panel, a button with text Code Editor opens the Luxonis Hub Studio.

> Because the studio runs locally in the same container as the app, you must be connected to the same network as Robot.

## Next steps

### Understand the template code

Follow our detailed guide that explains every part of the code.

[Understand the template code](https://docs.luxonis.com/cloud/advanced/legacy/perception-apps/examples/template-app.md)

### Luxonis Hub Studio

Discover our web based IDE.

[Luxonis Hub Studio](https://docs.luxonis.com/cloud/advanced/legacy/perception-apps/robothub-studio.md)

### Explore the Camera SDK

DepthAI is our Python library to connect to and configure the camera.

[Explore the Camera SDK](https://docs.luxonis.com/software-v3/depthai.md)

### Explore the Cloud SDK

`robothub` is our Python library that simplifies usage in Luxonis Hub and enables interaction with the cloud.

[Explore the Cloud SDK](https://docs.luxonis.com/cloud/advanced/legacy/perception-apps/robothub-library.md)