# Application Logs

Application Logs provide both real-time and historical insights into the behavior of applications running on your OAK devices.
Through Luxonis Hub, you can view log outputs from running apps on each device to diagnose issues remotely, streamlining debugging
and improving overall system observability.

When viewing logs, the Hub establishes a secure WebRTC connection with the OAK Agent to stream log data in real time, ensuring
low-latency access to application output directly from the device.

> **Open Logs**
> To open application logs, navigate to:
> **Devices → Select a Device → Apps (Tab) → Select an Application → Logs (Tab)**