# Over-the-Air (OTA) Updates

Use this guide when you want to update a supported OAK4 device through the current Luxonis Hub OTA workflow.

> **Current boundary**
> Self-hosted OTA in Hub is not generally available today. For self-hosted systems, the host operating system remains customer-managed.

## Requirements

Before starting the update:

 * confirm the device is online and connected to Hub
 * confirm the device has enough free storage for download and unpacking
 * confirm the device has stable power for the full update and reboot cycle

## Update the device

 1. Open the device in Hub and go to the Device Overview page.
 2. If a newer supported version is available, click the orange Update Available button.
 3. Review the changelog and confirm that you want to start the update.
 4. Wait while the device downloads and applies the update.
 5. Allow the device to reboot and reconnect to Hub.

From the Device Overview, click Update Available when Hub shows a newer supported version for the device.

![Luxonis Hub device overview with Update Available](https://docs.luxonis.com/static/images/cloud/ota-trigger.webp)

Review the changelog and click Update to continue.

![Luxonis Hub OTA update confirmation dialog](https://docs.luxonis.com/static/images/cloud/ota-confirm.webp)

The device downloads the new software and prepares the update before rebooting automatically.

![Luxonis Hub OTA update progress badge](https://docs.luxonis.com/static/images/cloud/ota-progress.webp)

After the device returns, check the update field in the overview and use the ? tooltip for detailed result information.

![Luxonis Hub device info with successful update tooltip](https://docs.luxonis.com/static/images/cloud/ota-success.webp)

## Verify the update

The update is complete when all of the following are true:

 * the device reconnects to Hub after reboot
 * the device overview shows the expected software version
 * the update field reports a successful final state
 * the device is ready for normal app and remote-access workflows again

> **Reboot is required**
> Completing the OTA update requires a device restart. After reboot, all services and applications, including the OAK Agent, will restart automatically.

## Current availability

This page covers:

 * Current: supported OTA flows for OAK4 device software
 * Not current: broad self-hosted OTA for customer-managed Linux hosts
 * Not current: manifest-based rollout or large-scale fleet rollout orchestration

If you are running a self-hosted deployment, you can still use Hub for visibility, remote sessions, and app lifecycle management,
but the host OS lifecycle remains your responsibility.