# Detailed Conversion

## Overview

To make full use of AI models on our devices, they must first be converted into the RVC compiled format for the target platform.
If you would like to understand what conversion is, why it is needed, and some of the key concepts involved, see the
[Conversion](https://docs.luxonis.com/software-v3/ai-inference/conversion.md) section.

While Hub provides a fast and simplified option through the Quick Conversion tool, some workflows require deeper control. The
Detailed Conversion workflow is designed for these more advanced use cases, offering fine-grained configuration parameters and
version/variant management. If you instead prefer a fast, one-off conversion with minimal setup, see the [Quick
Conversion](https://docs.luxonis.com/cloud/hubai/quick-conversion.md) section.

## Conversion

> **Note**
> It is assumed here that the models aimed for conversion have already been uploaded to Hub. If this step has not yet been completed, please refer to the [Model Upload](https://docs.luxonis.com/cloud/hubai/model-registry/upload-download.md) guidelines.

> **Note**
> For custom models, prefer uploading an ONNX NN Archive as the base model whenever possible. A source NN Archive acts as the source of truth for the model's tensor metadata, preprocessing, and optional postprocessing metadata (`heads`), which makes the conversion flow more predictable and usually produces a converted archive that is ready to use in DepthAI without manual edits. If you upload a raw `ONNX` file instead, Hub can infer parts of the tensor structure from the graph, but it cannot infer training-time preprocessing choices or semantic output metadata such as class names and parser selection.

Step by step instructions:

Open [Hub](https://hub.luxonis.com/ai), navigate to the [Models](https://hub.luxonis.com/ai/models) section, open the desired
model, scroll to Model Variants, and click Convert next to the variant you want to export.

Select the target `RVC` platform. The available targets depend on the uploaded base model format. In practice, `ONNX`-based model
sources offer the broadest conversion support across platforms.

Review the prefilled values and adjust them as needed. If the base model is a raw `ONNX` file, enter the source-model input
settings manually. If the base model is an `ONNX` NN Archive, use its `config.json` as the source of truth and only change values
if the archive metadata is incorrect.

Use the reference sections below for the exact meaning of each field.

Click Export to start the conversion. The new model instance first appears as Pending and changes to Success when the export is
ready. You can then download the converted archive or reference it directly through DepthAI.

## Parameter Reference

### Source-model input settings

| Parameter | Category | Meaning |
| --- | --- | --- |
| `Shape` | Source model | Input shape expected by the source model |
| `Mean Values` | Source model | Per-channel values subtracted from the input |
| `Scale Values` | Source model | Per-channel divisors applied after mean subtraction |
| `Encoding From` | Source model | Channel order expected by the source model |
| `Encoding To` | Exported model | Channel order expected by the converted model at runtime |

### Platform and export settings

| Parameter | Category | Meaning |
| --- | --- | --- |
| `Model Instance Name` | Exported model | Name of the converted instance shown in Hub |
| `Ir version` / `Snpe version` | Conversion process | Target conversion format or runtime version |
| `Disable Onnx Simplification` | Conversion process | Disables `ONNX` graph simplification during conversion |
| `Mo Args` | Conversion process | Extra OpenVINO Model Optimizer arguments for `RVC2` and `RVC3` |
| `Compile Tool Args` | Conversion process | Extra OpenVINO compile tool arguments for `RVC2` |
| `POT Target Device` | Conversion process | POT target device for `RVC3` |
| `Convert to blob` | Exported model | Exports `.blob` instead of `.superblob` for `RVC2` |

### Quantization settings

| Parameter | Category | Meaning |
| --- | --- | --- |
| `Quantization Data` | Conversion process | Dataset used to calibrate quantized conversion |
| `Max Quantization Images` | Conversion process | Maximum number of images used during quantization |
| `Target Precision` | Conversion process | Precision target such as `FP16` or `INT8` for `RVC4` |

In the Hub UI, you can choose from the generic datasets listed below:

 * Driving - Images of streets and vehicles (OIv7 classes like Vehicle, Car, Traffic light, etc.)
 * Food - Images of fruit, vegetables, raw and prepared foods (OIv7 classes like Apple, Salad, Pizza, etc.)
 * General - A random subset of OIv7 images representing a diverse set of objects and scenes
 * Indoors - Images of indoor spaces (OIv7 classes like Table, Chair, Fireplace, etc.)
 * Random - Random-pixel images
 * Warehouse - Images of warehouse interiors (a random subset of forklift-1 images)

If you need a custom quantization dataset, use the [Luxonis Hub AI
SDK](https://docs.luxonis.com/cloud/hubai/model-registry/hubai-sdk.md). For more advanced conversion and quantization options, see
the [ModelConverter](https://docs.luxonis.com/software-v3/ai-inference/conversion/rvc-conversion/offline/modelconverter.md)
documentation.

> **Note**
> During conversion, source preprocessing is embedded into the exported model structure. It is generally advised to fill in the relevant parameters (Scale Values, Mean Values, and Encoding) in a way so that the converted model expects BGR input without any additional scaling or mean shifting. The order of preprocessing operations is:

 1. Reversing input channels;
 2. Subtracting mean values;
 3. Dividing by scale values.

Keep this in mind when manipulating inputs, i.e. mean and scale should follow the order of the original color encoding of the
model.

If your original preprocessing is `input = (input / 255.0 - mean) / std` and your runtime input is an 8-bit image in the `[0,255]`
range, enter `Mean Values = 255 * mean` and `Scale Values = 255 * std`. For standard ImageNet RGB normalization, this means `Mean
Values = [123.675, 116.28, 103.53]` and `Scale Values = [58.395, 57.12, 57.375]`. Do not swap mean and scale values when changing
between `RGB` and `BGR`. Only reorder the channels to match the original source-model encoding. Geometric preprocessing such as
resize, crop, or letterboxing is still your responsibility at runtime, so your input pipeline still needs to match the model's
original preprocessing.

## Raw ONNX vs ONNX NN Archive

| Starting point | What Hub can determine automatically | What you still need to define |
| --- | --- | --- |
| Raw `ONNX` | Tensor structure from the graph | Training-time preprocessing choices and semantic output metadata such as class
names and parser configuration |
| `ONNX` NN Archive | Tensor metadata, preprocessing, and optional `heads` metadata from `config.json` | Export choices such as
target platform and conversion-specific options |

If you start from a correctly defined `ONNX` NN Archive, you normally should not edit the exported archive manually. It is
expected that the exported archive differs from the source archive. For example, the model path changes from `model.onnx` to a
compiled artifact such as `.superblob`, `.blob`, or `.dlc`, and `mean` / `scale` can become `null` because preprocessing was baked
into the compiled model.

## Troubleshooting

Not all models can be converted for the desired platform. You can inspect failed conversion logs as follows:

Find the failed job in the Failed Conversions section and open it.

Use the Logs button in the top right corner to download the logs, or inspect the Conversion process logs section directly on the
page.

> **Note**
> If export fails, corrections need to be made either to the model or the utilized conversion parameters. Please consult the [Conversion Troubleshooting](https://docs.luxonis.com/software-v3/ai-inference/conversion/troubleshooting.md) page for more information.