# Training concepts

## Overview

Luxonis Hub connects data preparation, model training, evaluation, and deployment. A Dataset holds samples and their annotations.
A Project defines what to train and links the dataset to one or more models. A successful training run creates a new model version
that can be evaluated, used to annotate more data, or converted for deployment.

## Datasets

A Dataset is a team-owned collection of samples with one or more machine learning tasks. Create one from a task preset, define
custom tasks, or inherit the tasks and classes from an existing project.

While Hub imports data, the dataset status progresses through Pending and Running. A successful import changes it to Ready; an
unsuccessful import changes it to Failed. Open the associated [job](https://docs.luxonis.com/cloud/hubai/training/jobs.md) to
inspect progress or errors.

### Tasks and task names

A task defines the type of prediction, its task name, and its classes. Keypoint tasks also define skeleton labels. The task name
groups related annotations inside the dataset and is passed to LuxonisTrain as `task_name`; matching task names are therefore
required when uploading pre-existing data.

A dataset can contain several tasks. For example, the Keypoint Detection preset combines object detection with nested keypoints,
while Instance Segmentation combines object detection with nested segmentation.

| Task type | Annotation in Hub | Main training metric |
| --- | --- | --- |
| Classification | Predict a class for the image | F1 Score |
| Object Detection | Predict bounding boxes | mean Average Precision (mAP) |
| Semantic Segmentation | Predict polygons or masks | Jaccard Index |
| Keypoint Detection | Predict a box and its skeleton keypoints | mean Average Precision Keypoints |
| Instance Segmentation | Predict a box and its nested polygon | mean Average Precision (mAP) |
| Optical Character Recognition (OCR) | Predict text | OCR Accuracy |

For the underlying annotation structure, task names, and supported dataset parsers, see
[LuxonisParser](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-parser.md).

### Classes

Classes are defined separately for each task. When importing annotated data, Hub keeps only annotations whose type and class match
a dataset task. It drops unmatched annotations.

> **Note**
> Define every class you intend to import before uploading the archive. You can add classes later, but existing classes cannot be removed from a dataset.

### Samples

A sample consists of an image plus its annotations, split, annotation status, and optional tags. Samples can originate from [file
uploads](https://docs.luxonis.com/cloud/hubai/training/datasets/upload.md),
[Snaps](https://docs.luxonis.com/cloud/features/event-storage/snaps.md), or [model
pre-annotation](https://docs.luxonis.com/cloud/hubai/training/datasets/annotate.md).

### Annotation status

Annotation statuses provide an optional review workflow:

`Unannotated` → `Pre-annotated` → `Annotated` → `In Review` → `Completed`

 * Unannotated: has no reviewed annotation work.
 * Pre-annotated: contains machine-generated annotations that should be reviewed.
 * Annotated: indicates that manual annotation work has started or changed.
 * In Review: is ready for a reviewer in an optional QA stage.
 * Completed: is finalized and approved for use by the training workflow.

Editing an Unannotated or Pre-annotated sample automatically changes it to Annotated. Files imported through a regular
annotated-data upload start as Completed, assuming external data has already undergone adequate QA and its annotations are
correct.

> **Completed samples drive readiness checks**
> The train, validation, and test sizes used by run validation and dataset health count Completed samples only. Statuses are optional as a workflow, but samples must be marked Completed before they contribute to those counts.

### Splits

Every sample belongs to one of three splits:

 * Train: teaches the model by updating its weights.
 * Validation: measures generalization during training and is used to select checkpoints.
 * Test: provides a final comparison on data that was not used to update or select the model.

If a training dataset has no completed validation samples, Hub uses the training split for validation. If it has no completed test
samples, Hub falls back to the validation split. An evaluation run requires completed samples in the split you explicitly select.

### Tags

Tags are free-form labels for organizing samples. Use them to filter the sample grid, target model pre-annotation, or select the
subset copied into a dataset version for a training run. When several tags are selected, the AND option requires all tags and the
OR option accepts any selected tag.

### Versions

A dataset version is a read-only snapshot created for a training run. It freezes the chosen samples and annotations so later
dataset edits do not change the run's input. Enabling Version Dataset can add preparation time before training starts, but makes
runs reproducible and easier to compare and analyze dataset drift over time.

If the dataset has not changed since the latest version made with the same tag filter, Hub reuses that version instead of copying
it again. See [Health, Splits & Versions](https://docs.luxonis.com/cloud/hubai/training/datasets/health-splits-versions.md) for
the full workflow.

### Health

Dataset health summarizes three checks based on completed samples:

 * Size: checks whether enough samples are available.
 * Split distribution: checks whether train, validation, and test data are reasonably balanced for their purposes.
 * Class distribution: checks that every class is present and flags severe imbalance.

Each check is Healthy, Unhealthy, or Fail. Health is intended for user guidance and is not a training gate on its own; the run
form separately validates the samples and task mapping it needs.

## Projects

A Project combines a task definition, one or more linked models, and its training and evaluation runs. Creating a project from a
dataset copies the dataset tasks and classes into the project. Project tasks are not modifiable after creation.

### Linked models and architectures

Each project model is paired with an architecture, which determines the trainable model family and default configuration. Hub
offers LuxonisTrain predefined architectures for Detection, Classification, Segmentation, Instance Segmentation, Keypoint
Detection, and OCR. Available families have Light, Medium, or Heavy variants where supported; the Hub form shows only the variants
currently available for the selected task.

Architecture cards compare relative speed and accuracy and show estimated performance for supported RVC platforms. Light
architectures generally favor speed, while heavier architectures generally favor accuracy.

Every successful training run publishes a new version of its linked model. The version contains the trained artifacts and links
back to the run that produced it.

### Training and evaluation runs

A training run combines a project model, dataset or dataset version, checkpoint selection, and compute speed. Its output is a new
model version containing an ONNX [NN Archive](https://docs.luxonis.com/software-v3/ai-inference/nn-archive.md) and a PyTorch
checkpoint.

An evaluation run applies an existing checkpoint to a chosen validation or test split. It records metrics and inference images but
does not train weights or create another model version.

Runs progress through Pending, Running, and then Completed, Failed, or Shutdown.

### Checkpoints

A checkpoint stores model weights from a point in training. Hub exposes two checkpoint-selection strategies:

 * Metric: selects the checkpoint with the best validation value for the task's main metric.
 * Loss: selects the checkpoint with the lowest validation loss.

Use a checkpoint to resume training, run evaluation, or pre-annotate compatible dataset samples. The checkpoint's task names and
classes must match the target workflow.

### Training speed

The training form shows the compute speeds available to the active team. Each option identifies its compute type and affects both
duration and credit consumption. Hub shows a conservative credit estimate for the selected speed before the run is submitted.

## Credits and jobs

Credits allow for training and evaluation compute. Hub reserves the estimate when a run starts, charges actual usage, and releases
unused reserved credits. Learn how balances and interrupted runs work in
[Credits](https://docs.luxonis.com/cloud/hubai/training/credits.md).

Jobs represent background work across Luxonis Hub, including dataset uploads and exports, version creation, pre-annotation,
training, and model conversion. Monitor them from the Jobs page as described in
[Jobs](https://docs.luxonis.com/cloud/hubai/training/jobs.md).

## Put the concepts together

The workflow is iterative: collect samples, annotate and complete them, version the dataset, train and evaluate a model, then
deploy the best model or use its checkpoint to pre-annotate the next batch. Continue with [The training
workflow](https://docs.luxonis.com/cloud/hubai/training/workflow.md) for the end-to-end view.