Minimal working code sample

Demo

Source code

import cv2
import depthai

device = depthai.Device('', False)

p = device.create_pipeline(config={
    "streams": ["metaout", "previewout"],
    "ai": {
        "blob_file": "/path/to/depthai/resources/nn/mobilenet-ssd/mobilenet-ssd.blob.sh14cmx14NCE1",
        "blob_file_config": "/path/to/depthai/resources/nn/mobilenet-ssd/mobilenet-ssd.json",
        'shaves' : 14,
        'cmx_slices' : 14,
        'NN_engines' : 1,
    }
})

if p is None:
    raise RuntimeError("Error initializing pipelne")

detections = []

while True:
    nnet_packets, data_packets = p.get_available_nnet_and_data_packets()

    for nnet_packet in nnet_packets:
        detections = list(nnet_packet.getDetectedObjects())

    for packet in data_packets:
        if packet.stream_name == 'previewout':
            data = packet.getData()
            data0 = data[0, :, :]
            data1 = data[1, :, :]
            data2 = data[2, :, :]
            frame = cv2.merge([data0, data1, data2])

            img_h = frame.shape[0]
            img_w = frame.shape[1]

            for detection in detections:
                pt1 = int(detection.x_min * img_w), int(detection.y_min * img_h)
                pt2 = int(detection.x_max * img_w), int(detection.y_max * img_h)

                cv2.rectangle(frame, pt1, pt2, (0, 0, 255), 2)

            cv2.imshow('previewout', frame)

    if cv2.waitKey(1) == ord('q'):
        break

del p
del device

Explanation

The code is divided into three phases: initialization, processing results and deinitialization.

Initialization is done here, as it’s initializing the device and making sure that the pipeline is created. Please note that sh14cmx14NCE1 in a blob file definition means that this blob was compiled to use 14 MyriadX SHAVEs, 14 MyriadX CMXes and 1 MyriadX Neural Compute Engine. These params needs to be provided in ai configuration, using fields shaves, cmx_slices and NN_engines respectively

device = depthai.Device('', False)

p = device.create_pipeline(config={
    "streams": ["metaout", "previewout"],
    "ai": {
        "blob_file": "/path/to/depthai/resources/nn/mobilenet-ssd/mobilenet-ssd.blob.sh14cmx14NCE1",
        "blob_file_config": "/path/to/depthai/resources/nn/mobilenet-ssd/mobilenet-ssd.json",
        'shaves' : 14,
        'cmx_slices' : 14,
        'NN_engines' : 1,
    }
})

if p is None:
    raise RuntimeError("Error initializing pipelne")

Deinitialization is basically only two lines of code, and whereas it’s not necessary to include it, it’s definitely recommended

del p
del device

Now, the results processing consists of two phases - parsing nnet results and displaying the frames.

Parsing neural network results

Below, you’ll se the part that’s parsing the results from neural network

detections = []

while True:
    nnet_packets, data_packets = p.get_available_nnet_and_data_packets()

    for nnet_packet in nnet_packets:
        detections = list(nnet_packet.getDetectedObjects())

Neural network configuration we specified earlier, in blob_file_config field, allows DepthAI to prepare results in a correct format and remove incorrect entries (e.g. those with confidence below threshold).

Each object in this array is a Detection instance, which we can easily use later in the code

Displaying the frames

for packet in data_packets:
    if packet.stream_name == 'previewout':
        data = packet.getData()
        data0 = data[0, :, :]
        data1 = data[1, :, :]
        data2 = data[2, :, :]
        frame = cv2.merge([data0, data1, data2])

        img_h = frame.shape[0]
        img_w = frame.shape[1]

        for detection in detections:
            pt1 = int(detection.x_min * img_w), int(detection.y_min * img_h)
            pt2 = int(detection.x_max * img_w), int(detection.y_max * img_h)

            cv2.rectangle(frame, pt1, pt2, (0, 0, 255), 2)

        cv2.imshow('previewout', frame)

if cv2.waitKey(1) == ord('q'):
    break

This stage is also divided into three phases - preparing the frame, augumenting the frame and adding control signals

Preparing the frame basically means that we’re transforming the frame to OpenCV-usable form.

First, we need to assure we’re operating on packet from previewout stream, so it’s a frame from 4K color camera.

Next, we get the data from the packet and transform it from CHW (Channel, Height, Width) form used by DepthAI to HWC (Height, Width, Channel) that is used by OpenCV.

for packet in data_packets:
    if packet.stream_name == 'previewout':
        data = packet.getData()  # e.x. shape (3, 300, 300)
        data0 = data[0, :, :]
        data1 = data[1, :, :]
        data2 = data[2, :, :]
        frame = cv2.merge([data0, data1, data2])  # e.x. shape (300, 300, 3)

Augumenting the frame means any process that changes what is being displayed. In this example, I’m adding red rectangles around detected items. You can also add here text displays, latency info - basically whatever your business logic requires.

Since the position of the bounding boxes are returned from neural network as floats in range (0, 1), which specify position of the point relative to it’s width/height, we need to transform it into the actual point on the image (which you can see as we’re doing e.x. int(detection.x_min * img_w)).

Next, using cv2.rectangle, we’re printing the actual rectangle on the frame. Finally, when the frame is ready, we display it using cv2.imshow function.

img_h = frame.shape[0]
img_w = frame.shape[1]

for detection in detections:
    pt1 = int(detection.x_min * img_w), int(detection.y_min * img_h)
    pt2 = int(detection.x_max * img_w), int(detection.y_max * img_h)

    cv2.rectangle(frame, pt1, pt2, (0, 0, 255), 2)

cv2.imshow('previewout', frame)

Adding control signals is the last part, where you can add interactivity to the displayed image. We’re adding just one command - to terminate the program - when you press the q button.

if cv2.waitKey(1) == ord('q'):
    break

Got questions?

We’re always happy to help with code or other questions you might have.