Getting started with OAK IoT devices

Note

This tutorial is intended for OAK-D-IoT-75 and OAK-D-IoT-40, which both have an ESP32 on the board.

Note

Having ESP32 on the device doesn’t mean users will be able to develop the device without the USB-C connection.

In this tutorial we will have a look at:

  • Overview of the ESP32 - DepthAI connection

  • Limitations

  • Common use cases for the ESP32

  • How to get started with the development

Code examples

Code examples can be found in our esp32-spi-message-demo github repository.

Overview

                DepthAI device                        ┌─────┐
┌───────────────────────────────────────────────┐     │  ◎  │
│                                               │     │     │
│                ┌───────────────────ESP32───┐  │  BT |     |
│                │                           │--│◄───►|     |
│                │   (Your ESP32 firmware)   │  │     └─────┘
│                │                           │  │         ┌──────────┐
│                │---------------------------│  │         │          │
│                │     depthai-spi-api       │--│◄───────►├──────────┤
│                └───────▲───────────────────┘  │  WiFi   │  Server  │
│                        │                      │         ├──────────┤
│                        │SPI                   │         │          │
│      Right             │                      │         └──────────┘
│       ┌───┐   ┌───┬────▼───┬─MyriadX(VPU)──┐  │
│       │ ◯ │--►|   │        │               │  │            Host
│ ┌───┐ └───┘   │   │ SpiOut │     ┌─────────┤  │        ┌───────────┐
│ │ ◯ │--------►|   └────────┘     │         │  │        │           │
│ └───┘ ┌───┐   │                  │ XLinkIn │  │  XLink │           │
│Color  │ ◯ |--►| (Your pipeline)  │ XLinkOut│--│◄──────►│           │
│       └───┘   │                  │         │  │        └────┬─┬────┘
│        Left   └──────────────────┴─────────┘  │             │ │
│                                               │           ──┴─┴──
└───────────────────────────────────────────────┘

Overview explained:

  • MyriadX is the VPU on the DepthAI, where you can run your pipeline

  • MyriadX is connected to the host (eg. PC)

  • MyriadX can send Messages to the ESP32 via SPI (using SPIOut node)

  • ESP32 can receive these messages using the depthai-spi-api library (which is an ESP-IDF component).

  • On ESP32 you can run post-processing of the messages and optionally send the results to a server (if connected to a WiFi network) or to a Bluetooth device (eg. a smartphone)

Limitations

Currently, the bottleneck for use cases is the SPI throughput, which is about 200kbps. This means you can’t stream frames over SPI in real-time. This is the current limitation by the SPI driver, but we are planning to look into it and increase the throughput of the SPI to ~8mbps (no ETA yet).

As of now we only support ESP-IDF as the development framework. In the future, we might support Arduino.

Common use cases for the ESP32

TL;DR:

  • Sending metadata results (spatial coordinates, NN results, tracklets etc.)

  • OTA updates

  • Capturing and sending (part of) an image

  • System information logging

  • Sending data to the cloud (eg. AWS/Azure/GCP or any other IOT platform)

  • Sending data to a Bluetooth device (eg. smartphone)

Explained in more detail:

  • You could run spatial object detections and/or object tracking pipeline on the VPU and send tracklets with spatial data over the SPI to the ESP32. On ESP32 you could run some simple filtering and/or NN result decoding and then send final results to the cloud

  • ESP32 can also flash DepthAI bootloader and/or pipeline, which means OTA (over-the-air) updates are supported.

  • We have an example for both sending a whole image and part of an image through the SPI from the VPU to the ESP32

  • Pipeline on the VPU could be configured to send system information (using SystemLogger node) to the ESP32 which would forward them to a logging platform

  • ESP32 also has Bluetooth capabilities, so you could forward the data from the ESP32 to a smartphone

How to get started with the development

  1. Install the ESP-IDF, instructions here.

  2. After setting up the environmental variables, you can build any demo from the esp32-spi-message-demo repository with idf.py build.

  3. After building, you can flash your ESP32 using idf.py -p PORT flash monitor (replace PORT with the ESP32 port, eg. /dev/ttyUSB0). You might need to change the permission of the port with sudo chmod 777 PORT so idf.py can access it.

  4. After flashing the ESP32, you can start the pipeline. If you have used a demo ESP32 code, you should run the corresponding python script from gen2-spi demos.

Got questions?

We’re always happy to help with code or other questions you might have.