Use a Pre-trained OpenVINO model¶
Warning
This example is outdated and we’re working on updating, please proceed with caution
In this tutorial, you’ll learn how to detect faces in real-time, even on a low-powered Raspberry Pi. I’ll introduce you to the OpenVINO, the Open Model Zoo and show you how to run models.

Haven’t heard of OpenVINO or the Open Model Zoo? I’ll start with a quick introduction of why we need these tools.
What is OpenVINO?¶
Under-the-hood, DepthAI uses the Intel Myriad X to perform high-speed model inference. However, you can’t just dump your neural net into the chip and get high-performance for free. That’s where OpenVINO comes in. OpenVINO is a free toolkit that converts a deep learning model into a format that runs on Intel Hardware. Once the model is converted, it’s common to see Frames Per Second (FPS) improve by 25x or more. Are a couple of small steps worth a 25x FPS increase? Often, the answer is yes!
Check the OpenVINO toolkit website for installation instructions. OpenVINO should be installed under /opt/intel. Verify that the version is supported by DepthAI (see Is DepthAI OpenVINO Compatible?).
What is the Open Model Zoo?¶
In machine learning/AI the name for a collection of pre-trained models is called a “model zoo”. The Open Model Zoo is a library of freely-available pre-trained models. The Zoo also contains scripts for downloading those models into a compile-ready format to run on DepthAI.
DepthAI is able to run many of the object detection models in the Zoo. Several of those models are included in the DepthAI Github repositoy.
Clone the Open Model Zoo repository from Github and install its dependencies. Optionally, add the scripts to your path:
export PATH="${PATH}:${PWD}/open_model_zoo/tools/downloader/"
Run DepthAI Default Model¶
The depthai_demo.py
file can be modified directly to you do your bidding, or you can simply pass arguments to it for
which models you want to run.
For simplicity we will do the latter, simply passing arguments so that DepthAI runs the face-detection-retail-0004
instead of the model run by default.
Before switching to using the face-detection-retail-0004
let’s take a baby step and give these command line
options a spin. In this case we’ll just pass in the same neural network that default runs when running
python3 depthai_demo.py
, just to make sure we’re doing it right:
python3 depthai_demo.py -dd
This will then run the a typical demo MobileNetv2 SSD object detector trained on the PASCAL 2007 VOC classes, which are:
Person: person
Animal: bird, cat, cow, dog, horse, sheep
Vehicle: airplane, bicycle, boat, bus, car, motorbike, train
Indoor: bottle, chair, dining table, potted plant, sofa, TV/monitor
I ran this on my iMac (OS X setup here) with a microAI sitting on my desk pointing upwards randomly - and it makes out the corner of my iMac (which is barely visible) and correctly identifies it as tv/monitor:

Run model¶
Now that we’ve got this verified, let’s move on to trying out other models, starting with face-detection-retail-0004
.
To use this model, simply specify the name of the model to be run with the -cnn
flag, as below:
python3 depthai_demo.py -dd -cnn face-detection-retail-0004
Execute the script to see an annotated video stream of face detection:

It’s that easy. Substitute your face for mine, of course.
And if you’d like to try other models, just peruse here and run them by their name, just like above.
Now take some time to play around with the model. You can for example check how far away the model can detect your face:


In the latter image you can see that I’m quite back-lit, which is one of the main challenges in face detection
(and other feature detection). In this case, it’s likely limiting the maximum range for which a face can be detected.
From the testing above, for a confidence threshold of 50%, this range appears to be about 20 feet. You could get longer
range out of the same model by reducing the model confidence threshold (by changing from 0.5
here) at the cost
of increased probability of false positives.
Another limiting factor is that this is a relatively low-resolution model (300x300 pixels), so faces get fairly small fairly fast at a distance. So let’s try another face detection model that uses a higher resolution.
Trying Other Models¶
The flow we walked through works for other pre-trained object detection models in our repository (here), which includes:
face detection for retail (
face-detection-retail-0004
)face detection for driver assistance (
face-detection-adas-0001
)facial landmarks, simple (
landmarks-regression-retail-0009
)facial landmarks, advanced (
facial-landmarks-35-adas-0002
)emotions recognition (
emotions-recognition-retail-0003
)pedestrian detection for driver-assistance (
pedestrian-detection-adas-0002
)person detection for retail environments (
person-detection-retail-0013
)vehicle detection for driver-assistance (
vehicle-detection-adas-0002
)vehicle and license plate detection (
vehicle-license-plate-detection-barrier-0106
)Human Pose Estimation (
human-pose-estimation-0001
)Pedestrian Detection (ADAS) (
pedestrian-detection-adas-0002
)Person, Vehicle and Bike Detection (
person-vehicle-bike-detection-crossroad-1016
)Age and Gender Recognition (
age-gender-recognition-retail-0013
)Pose Estimation on MobileNetV2 (
mobileNetV2-PoseEstimation
)
Models that can be deployed as first CNN in the argument (python3 depthai_demo.py -cnn <model>
)
(vehicle-detection-adas-0002,mobileNetV2-PoseEstimation,yolo-v3,vehicle-license-plate-detection-barrier-0106
,
age-gender-recognition-retail-0013,person-detection-retail-0013,human-pose-estimation-0001,face-detection-adas-0001
,
person-vehicle-bike-detection-crossroad-1016,openpose2,pedestrian-detection-adas-0002,tiny-yolo-v3,openpose,deeplabv3p_person,mobilenet-ssd,face-detection-retail-0004
)
Models that can be deployed as second CNN in the argument (python3 depthai_demo.py -cnn <model_1> -cnn2 <model_2>
)
(landmarks-regression-retail-0009,facial-landmarks-35-adas-0002,emotions-recognition-retail-0003
)
Simply change the paths above to run the other models there, adding the correct labels (or funny ones, should you choose).
Let’s try out face-detection-adas-0001
, which is intended for detecting faces inside the cabin of a vehicle.
(ADAS stands for Advanced Driver-Assistance Systems)
python3 depthai_demo.py -dd -cnn face-detection-adas-0001

So this model actually has a shorter detection distance than the smaller model despite having a higher resolution. Why? Likely because it was intentionally trained to detect only close-in faces since it’s intended to be used in the cabin of a vehicle. (You wouldn’t want to be detecting the faces in cars passing by, for example.)
And also you may notice networks like emotion recognition… those networks are actually intended to be run as a second stage network (as they are meant to be applied only to images that contain only faces). So to use the emotion recognition network, use the command below to tell DepthAI/megaAI to run it as the second stage:
./depthai_demo.py -cnn face-detection-retail-0004 -cnn2 emotions-recognition-retail-0003 -dd -sh 12 -cmx 12 -nce 2

And what is this -dd
option we’ve been running? Why is that there?
It’s there because we wanted to save the best for last. It stands for disable depth (and has the long-form option
--disable_depth
). So if you remove that, DepthAI will now calculate the 3D position of the object being
detected (a face in this example, but it works for any object detector.) (And if you’re using microAI, leave it there,
as microAI is monocular only - no depth information.)
So you get the full 3D position of the detected object, in this case, my face.
So that the full three-dimensional position in meters is returned. See below.
Spatial AI - Augmenting the Model with 3D Position¶
So by default DepthAI is set to return the full 3D position. So in the command above, we actually specify for it to not
be calculated with -dd
(or --disable_depth
).
So let’s run that same command, but with that line omitted, such that 3D results are returned (and displayed):
python3 depthai_demo.py -cnn face-detection-adas-0001

And there you find the 3D position of my mug!
You can than choose other models, change the labels, and you’re off - getting real-time 3D position for the class of interest.
Play with the feature and please share demos that you come up with (especially if you make a robot that stalks your cat) on discuss.luxonis.com and if you run into any issues, please ping us on our Github.
And if you find any errors in these documents, please report an issue on the docs github) on the bottom of this page to give us the correction!
Monocular Neural Inference fused with Stereo Depth¶
We call this mode of spatial AI ‘Monocular Neural Inference fused with Stereo Depth’. To visualize how this mode works, it is helpful to overlay the neural inference bounding box over the depth results directly.
To visualize this, let’s overlay the results directly onto the raw depth information (visualized in OpenCV HOT colormap
):
python3 depthai_demo.py -s metaout depth_raw -bb

So this ‘monocular neural inference fused with stereo disparity depth’ technique works well for objects, particularly bigger objects (like people, faces, etc.).
Stereo Neural Inference¶
Below we’ll use another technique, which we dub ‘stereo neural inference’ (or ‘Stereo AI’) which works well for smaller objects and also pixel-point features like facial landmarks and pose-estimator results, etc.

This can be run with the following command:
./depthai_demo.py -cnn face-detection-retail-0004 -cnn2 landmarks-regression-retail-0009 -cam left_right -dd -sh 12 -cmx 12 -nce 2 -monor 400 -monof 30
And note this is running both parallel neural inference (i.e. on both cameras) and also series neural inference (the landmarks-regression network is running on the results of the face detector).
Got questions?
We’re always happy to help with code or other questions you might have.