# IP rating

An [IP code](https://www.iec.ch/ip-ratings) describes enclosure protection against dust and water. The table below summarizes the
ratings detailed on this page.

| Camera/model | Stated IP rating | Conditions stated in the existing docs |
| --- | --- | --- |
| OAK4-D Pro, OAK4-D, OAK4-S | IP67 | Listed in the OAK4 test summary |
| OAK-4-CS | IP67 with Lens Hood; IP65 without | Lens Hood determines the stated rating |
| OAK-D PoE, OAK-1 PoE, OAK-D ToF, OAK Thermal | IP67 enclosure | No additional accessory conditions specified in that section |
| OAK-D S2 PoE, OAK-D W PoE, OAK-D Pro PoE, OAK-D Pro W PoE | IP65 enclosure | No additional accessory conditions specified in
that section |
| OAK-D-W, OAK-D Pro, OAK-D Pro W, OAK-D-S2 USB | IP66 | Requires the specified waterproof screw-locking USB cable |

## OAK4

All OAK4 camera models except OAK-4-CS are designed to meet IP67 ingress protection requirements in accordance with IEC
60529:2013. [OAK-4-CS](https://shop.luxonis.com/products/oak-4-cs) is rated IP65.

Testing Summary

 * Rating Achieved: IP67 (dust-tight and protected against temporary immersion in water)
 * Tested Models: [OAK4-D Pro](https://shop.luxonis.com/products/oak-4-d-ea), [OAK4-D](https://shop.luxonis.com/products/oak-4-d),
   [OAK4-S](https://shop.luxonis.com/products/oak-4-s-ea)

Test Conditions

 * Devices were fully submerged in their normal service position
 * Immersion depth: 1 meter
 * Duration: 30 minutes Units were non-operational and connected with a test cable during testing

Results

 * No water ingress was observed inside the enclosure
 * Devices maintained normal functionality after testing

This certification ensures the OAK4 devices are suitable for use in demanding environments where exposure to dust and temporary
water immersion may occur. The IP certification along with other environmental documentation can be found in the [store under
Technical Specifications](https://shop.luxonis.com/collections/all).

## OAK

### PoE cameras

Series 1 PoE devices ([OAK-D PoE](hw-catalog://OAK-D PoE) and [OAK-1 PoE](hw-catalog://OAK-1 PoE)), [OAK-D ToF](hw-catalog://OAK-D
ToF), and [OAK Thermal](hw-catalog://OAK Thermal) are shipped with an IP67 rated enclosure. It means that the device is protected
from total dust ingress and that it's protected from water immersion between 15 centimeters and 1 meter in depth.

[OAK-D S2 PoE](hw-catalog://OAK-D S2 PoE) (and all its variants, so [-W](hw-catalog://OAK-D W PoE), [-Pro](hw-catalog://OAK-D Pro
PoE), and [-Pro-W](hw-catalog://OAK-D Pro W PoE)) have IP65 rated enclosure.

PoE enclosures have gaskets which makes them waterproof/dustproof:

#### Internal testing

Here's our testing setup for the enclosures used in our R&D process. The drum, filled with water, has a height of 1 meter. We
conducted extended testing on these two enclosures.

### USB cameras

In 2024 we started shipping an USB with screw-locking mechanism ([shop
link](https://shop.luxonis.com/products/usb-3-cable-type-c-to-type-a)) along with several of our cameras;
[OAK-D-W](https://shop.luxonis.com/products/oak-d-w), [OAK-D Pro](https://shop.luxonis.com/products/oak-d-pro), and [OAK-D Pro
W](https://shop.luxonis.com/products/oak-d-pro-w).

This cable is water-proof, and provides IP66 protection to the cameras. If you wish to have
[OAK-D-S2](https://shop.luxonis.com/products/oak-d-s2) with IP66 protection, you can order this cable separately, as by default it
ships with a standard USB cable (non-waterproof).

#### USB IP certification

For testing and certification we are using a 3rd party certified laboratory. The certificate for the Series 2 USB cameras is
available [here](https://files.luxonis.com/store-files/Series2-ip66-cert.pdf).

The photos and video below were captured during the water resistance certification process.