## Laser Safety

> This product is classified as a
> **Class 1 Laser Product**
> under the
> **EN/IEC 60825-1, Edition 3 (2014)**
> internationally. Test protocol from laser class classification can be downloaded from
> **[here](https://files.luxonis.com/store-files/oak_pro_devices_laser_safety.pdf)**
> .

 * Do not power on the product if any external damage was observed.
 * Do not attempt to open any portion of this laser product.
 * Invisible laser radiation when opened. Avoid direct exposure to the beam.
 * There are no user serviceable parts with this laser product.
 * Modification or service of the stereo module, specifically the infrared projector, may cause the emissions to exceed Class 1.
 * No magnifying optical elements, such as eye loupes and magnifiers, are allowed.
 * Do not try to update camera firmware that is not officially released for specific camera module and revision.