# Shutter Type

OAK cameras support both rolling shutter and global shutter camera sensors. Here's the broad overview of the differences:

 * [Rolling Shutter](#Shutter%2520Type-Rolling%2520Shutter) - The image is captured by scanning the image from top to bottom. This
   means that the image is not captured all at once, but one row at a time. This can cause distortion (jello effect) in the image
   when the camera or the object is moving. Rolling shutter sensors can be higher-resolution without being too expensive.
 * [Global Shutter](#Shutter%2520Type-Global%2520Shutter) - The image is captured all at once. This means that the entire image is
   captured at the same time, which eliminates the jello effect. Global shutter sensors are typically a lot more expensive at
   higher resolutions (above 1MP), that's why our current max supported global shutter sensor is 2.3MP
   ([AR0234](https://docs.luxonis.com/hardware/sensors/AR0234.md)).

## Rolling Shutter

Recommended for applications where higher resolution is needed and the camera or the object isn't moving too fast.

In the image below, green marked time periods represent the exposure of each image row, while blue marks the readout of each image
row. The exposure and readout of each image row is slightly shifted relative to the previous image row. This leads to distortions
caused by the movement of the object during the whole exposure period.

Time difference between starting exposure of each new row ("row time") depends on the sensor, MIPI lanes & config, MIPI speed, and
raw bit depth (8/10/12 bits per pixel). Generally, we can estimate it with row_time = 1 / (maxFps * rows). So for IMX378 @ 1080P,
it would be row_time = 1/(60 * 1080) = 15.4us.

The animation below shows the downside of using rolling shutter while capturing a moving object.

### Estimating Jello effect

Jello effect is the distortion in the image when the camera or the object is moving. It's caused by the time difference between
the starting exposure of each new row. The jello effect depends on:

 * Speed of the object
 * Object size
 * Resolution used

Let's measure the speed/height in the percentage of the FOV. You can use [fov.luxonis.com](https://fov.luxonis.com) to estimate
the speed/height. Let's say we are measuring a box with the height of 50 cm with an OAK-1 (IMX378, normal FOV). Box is moving at 1
meter/sec horizontally, and camera is 2 meters away from the object. This means total Area of Coverage (AoC) length is 2.75m - so
the object moves at 36.4% FOV/second, and has a height of 18% of the FOV.

```python
obj_speed = 0.364  # [fov%/sec]
obj_height = 0.1  # [%] Object height in the FOV
width_pix, height_pix = 1920, 1080  # [pix] 1080P resolution
row_time = 1 / (60 * height_pix) # 15.4 microsec

obj_speed_pix = obj_speed * width_pix # 1920 pix/sec movement
shift_per_row = obj_speed_pix * row_time # 0.0148[pix/row] shift

# Number of rows, 10% of the FOV => 108 rows * shift
total_shift = obj_height * height_pix * shift_per_row
print('Object shift:', total_shift, 'pix') # -> Object shift: 1.16 pix
print('Relative obj shift', total_shift / width_pix * 100, '%') # -> 0.06 %

width_pix, height_pix = 3840, 2160  # [pix] 4K resolution
obj_speed_pix = obj_speed * width_pix
row_time = 1 / (30 * height_pix) # 15.4 microsec, same as 1080P
shift_per_row = obj_speed_pix * row_time
total_shift = obj_height * height_pix * shift_per_row
print('Object shift:', total_shift, 'pix') # -> Object shift: 4.66 pix
# Relative obj shift
print(total_shift / width_pix * 100, '%') # -> 0.12%
```

Is 1.16 pixels shift a lot? It depends on the application. For most applications, it's not a lot, but for some, it might be.

## Global Shutter

Recommended for applications where the camera or the object is moving fast, and for stereo camera pair, where jello effect can
cause issues with disparity matching. There can still be some

In the image below, green marked time periods represent the exposure of each image row, while blue marks the readout of each image
row. The exposure starts and ends at the same time for each image row, while the readout is slightly shifted for every image row.
However, shifted readout times of image rows don't affect the quality of the captured image.

Using global shutter all pixels are exposed at the same time, unlike using rolling shutter. It allows a better quality of the
captured image, even if the object is moving relatively fast. The animation shows how all rows of the image are captured at once.