# Luxonis Cameras in NVIDIA Isaac Sim

Luxonis cameras are officially supported in NVIDIA Isaac Sim, giving robotics teams a simpler way to evaluate perception setups in
simulation before moving to physical hardware. With native Luxonis sensor models available directly inside Isaac Sim and Isaac
Lab, developers can work with camera configurations that reflect real device behavior instead of recreating optics and sensor
parameters by hand.

## What This Enables

 * Faster setup for simulation workflows, with Luxonis cameras ready to place directly in Isaac Sim scenes
 * More realistic sensor evaluation when testing camera placement, mounting positions, and field of view
 * Earlier perception validation before hardware deployment
 * Synthetic data generation with NVIDIA Replicator using the same camera configurations intended for real-world deployment

This is especially useful for teams building autonomous mobile robots, industrial automation systems, warehouse robots, drones,
and research platforms that need a tighter loop between simulation and deployment.

## Getting Started in Isaac Sim

The Luxonis post highlights a simple starting point: in Isaac Sim, open Content Browser -> Isaac Sim -> Sensors -> Luxonis ->
OAK4-D, then drag `oak4_d.usd` into the scene. From there, you can begin testing perception pipelines and evaluating camera
layouts without manual sensor configuration.

### Luxonis Cameras in NVIDIA Isaac Sim Blogpost

Read the full write-up on using Luxonis cameras natively in NVIDIA Isaac Sim and Isaac Lab.

[Read the blogpost](https://discuss.luxonis.com/blog/6904-luxonis-cameras-are-now-officially-supported-in-nvidia-isaac-sim)