RGB & TinyYolo with spatial data¶
This example shows how to run Yolo on the RGB input frame, and how to display both the RGB preview, detections, depth map and spatial information (X,Y,Z). It’s similar to example RGB & MobilenetSSD with spatial data except it is running TinyYolo network. X,Y,Z coordinates are relative to the center of depth map.
setNumClasses - number of YOLO classes setCoordinateSize - size of coordinate setAnchors - yolo anchors setAnchorMasks - anchorMasks26, anchorMasks13 (anchorMasks52 - additionally for full YOLOv4) setIouThreshold - intersection over union threshold setConfidenceThreshold - confidence threshold above which objects are detected
Similar samples:
Demo¶
Setup¶
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the script
git clone https://github.com/luxonis/depthai-python.git
cd depthai-python/examples
python3 install_requirements.py
For additional information, please follow installation guide
This example script requires external file(s) to run. If you are using:
depthai-python, run
python3 examples/install_requirements.py
to download required file(s)dephtai-core, required file(s) will get downloaded automatically when building the example
Source code¶
Also available on GitHub
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99 100 101 102 103 104 105 106 107 108 109 110 111 112 113 114 115 116 117 118 119 120 121 122 123 124 125 126 127 128 129 130 131 132 133 134 135 136 137 138 139 140 141 142 143 144 145 146 147 148 149 150 151 152 153 154 155 156 157 158 159 160 161 162 163 164 165 166 167 168 169 170 171 172 173 174 175 176 177 178 179 180 181 182 183 184 185 186 187 188 189 190 191 192 193 194 195 196 197 198 199 200 201 202 203 204 205 | #!/usr/bin/env python3 from pathlib import Path import sys import cv2 import depthai as dai import numpy as np import time ''' Spatial Tiny-yolo example Performs inference on RGB camera and retrieves spatial location coordinates: x,y,z relative to the center of depth map. Can be used for tiny-yolo-v3 or tiny-yolo-v4 networks ''' # Get argument first nnBlobPath = str((Path(__file__).parent / Path('../models/yolo-v4-tiny-tf_openvino_2021.4_6shave.blob')).resolve().absolute()) if 1 < len(sys.argv): arg = sys.argv[1] if arg == "yolo3": nnBlobPath = str((Path(__file__).parent / Path('../models/yolo-v3-tiny-tf_openvino_2021.4_6shave.blob')).resolve().absolute()) elif arg == "yolo4": nnBlobPath = str((Path(__file__).parent / Path('../models/yolo-v4-tiny-tf_openvino_2021.4_6shave.blob')).resolve().absolute()) else: nnBlobPath = arg else: print("Using Tiny YoloV4 model. If you wish to use Tiny YOLOv3, call 'tiny_yolo.py yolo3'") if not Path(nnBlobPath).exists(): import sys raise FileNotFoundError(f'Required file/s not found, please run "{sys.executable} install_requirements.py"') # Tiny yolo v3/4 label texts labelMap = [ "person", "bicycle", "car", "motorbike", "aeroplane", "bus", "train", "truck", "boat", "traffic light", "fire hydrant", "stop sign", "parking meter", "bench", "bird", "cat", "dog", "horse", "sheep", "cow", "elephant", "bear", "zebra", "giraffe", "backpack", "umbrella", "handbag", "tie", "suitcase", "frisbee", "skis", "snowboard", "sports ball", "kite", "baseball bat", "baseball glove", "skateboard", "surfboard", "tennis racket", "bottle", "wine glass", "cup", "fork", "knife", "spoon", "bowl", "banana", "apple", "sandwich", "orange", "broccoli", "carrot", "hot dog", "pizza", "donut", "cake", "chair", "sofa", "pottedplant", "bed", "diningtable", "toilet", "tvmonitor", "laptop", "mouse", "remote", "keyboard", "cell phone", "microwave", "oven", "toaster", "sink", "refrigerator", "book", "clock", "vase", "scissors", "teddy bear", "hair drier", "toothbrush" ] syncNN = True # Create pipeline pipeline = dai.Pipeline() # Define sources and outputs camRgb = pipeline.create(dai.node.ColorCamera) spatialDetectionNetwork = pipeline.create(dai.node.YoloSpatialDetectionNetwork) monoLeft = pipeline.create(dai.node.MonoCamera) monoRight = pipeline.create(dai.node.MonoCamera) stereo = pipeline.create(dai.node.StereoDepth) nnNetworkOut = pipeline.create(dai.node.XLinkOut) xoutRgb = pipeline.create(dai.node.XLinkOut) xoutNN = pipeline.create(dai.node.XLinkOut) xoutDepth = pipeline.create(dai.node.XLinkOut) xoutRgb.setStreamName("rgb") xoutNN.setStreamName("detections") xoutDepth.setStreamName("depth") nnNetworkOut.setStreamName("nnNetwork") # Properties camRgb.setPreviewSize(416, 416) camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P) camRgb.setInterleaved(False) camRgb.setColorOrder(dai.ColorCameraProperties.ColorOrder.BGR) monoLeft.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P) monoLeft.setCamera("left") monoRight.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P) monoRight.setCamera("right") # setting node configs stereo.setDefaultProfilePreset(dai.node.StereoDepth.PresetMode.HIGH_DENSITY) # Align depth map to the perspective of RGB camera, on which inference is done stereo.setDepthAlign(dai.CameraBoardSocket.CAM_A) stereo.setOutputSize(monoLeft.getResolutionWidth(), monoLeft.getResolutionHeight()) stereo.setSubpixel(True) spatialDetectionNetwork.setBlobPath(nnBlobPath) spatialDetectionNetwork.setConfidenceThreshold(0.5) spatialDetectionNetwork.input.setBlocking(False) spatialDetectionNetwork.setBoundingBoxScaleFactor(0.5) spatialDetectionNetwork.setDepthLowerThreshold(100) spatialDetectionNetwork.setDepthUpperThreshold(5000) # Yolo specific parameters spatialDetectionNetwork.setNumClasses(80) spatialDetectionNetwork.setCoordinateSize(4) spatialDetectionNetwork.setAnchors([10,14, 23,27, 37,58, 81,82, 135,169, 344,319]) spatialDetectionNetwork.setAnchorMasks({ "side26": [1,2,3], "side13": [3,4,5] }) spatialDetectionNetwork.setIouThreshold(0.5) # Linking monoLeft.out.link(stereo.left) monoRight.out.link(stereo.right) camRgb.preview.link(spatialDetectionNetwork.input) if syncNN: spatialDetectionNetwork.passthrough.link(xoutRgb.input) else: camRgb.preview.link(xoutRgb.input) spatialDetectionNetwork.out.link(xoutNN.input) stereo.depth.link(spatialDetectionNetwork.inputDepth) spatialDetectionNetwork.passthroughDepth.link(xoutDepth.input) spatialDetectionNetwork.outNetwork.link(nnNetworkOut.input) # Connect to device and start pipeline with dai.Device(pipeline) as device: # Output queues will be used to get the rgb frames and nn data from the outputs defined above previewQueue = device.getOutputQueue(name="rgb", maxSize=4, blocking=False) detectionNNQueue = device.getOutputQueue(name="detections", maxSize=4, blocking=False) depthQueue = device.getOutputQueue(name="depth", maxSize=4, blocking=False) networkQueue = device.getOutputQueue(name="nnNetwork", maxSize=4, blocking=False) startTime = time.monotonic() counter = 0 fps = 0 color = (255, 255, 255) printOutputLayersOnce = True while True: inPreview = previewQueue.get() inDet = detectionNNQueue.get() depth = depthQueue.get() inNN = networkQueue.get() if printOutputLayersOnce: toPrint = 'Output layer names:' for ten in inNN.getAllLayerNames(): toPrint = f'{toPrint} {ten},' print(toPrint) printOutputLayersOnce = False frame = inPreview.getCvFrame() depthFrame = depth.getFrame() # depthFrame values are in millimeters depth_downscaled = depthFrame[::4] if np.all(depth_downscaled == 0): min_depth = 0 # Set a default minimum depth value when all elements are zero else: min_depth = np.percentile(depth_downscaled[depth_downscaled != 0], 1) max_depth = np.percentile(depth_downscaled, 99) depthFrameColor = np.interp(depthFrame, (min_depth, max_depth), (0, 255)).astype(np.uint8) depthFrameColor = cv2.applyColorMap(depthFrameColor, cv2.COLORMAP_HOT) counter+=1 current_time = time.monotonic() if (current_time - startTime) > 1 : fps = counter / (current_time - startTime) counter = 0 startTime = current_time detections = inDet.detections # If the frame is available, draw bounding boxes on it and show the frame height = frame.shape[0] width = frame.shape[1] for detection in detections: roiData = detection.boundingBoxMapping roi = roiData.roi roi = roi.denormalize(depthFrameColor.shape[1], depthFrameColor.shape[0]) topLeft = roi.topLeft() bottomRight = roi.bottomRight() xmin = int(topLeft.x) ymin = int(topLeft.y) xmax = int(bottomRight.x) ymax = int(bottomRight.y) cv2.rectangle(depthFrameColor, (xmin, ymin), (xmax, ymax), color, 1) # Denormalize bounding box x1 = int(detection.xmin * width) x2 = int(detection.xmax * width) y1 = int(detection.ymin * height) y2 = int(detection.ymax * height) try: label = labelMap[detection.label] except: label = detection.label cv2.putText(frame, str(label), (x1 + 10, y1 + 20), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255) cv2.putText(frame, "{:.2f}".format(detection.confidence*100), (x1 + 10, y1 + 35), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255) cv2.putText(frame, f"X: {int(detection.spatialCoordinates.x)} mm", (x1 + 10, y1 + 50), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255) cv2.putText(frame, f"Y: {int(detection.spatialCoordinates.y)} mm", (x1 + 10, y1 + 65), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255) cv2.putText(frame, f"Z: {int(detection.spatialCoordinates.z)} mm", (x1 + 10, y1 + 80), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255) cv2.rectangle(frame, (x1, y1), (x2, y2), color, cv2.FONT_HERSHEY_SIMPLEX) cv2.putText(frame, "NN fps: {:.2f}".format(fps), (2, frame.shape[0] - 4), cv2.FONT_HERSHEY_TRIPLEX, 0.4, color) cv2.imshow("depth", depthFrameColor) cv2.imshow("rgb", frame) if cv2.waitKey(1) == ord('q'): break |
Also available on GitHub
1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 47 48 49 50 51 52 53 54 55 56 57 58 59 60 61 62 63 64 65 66 67 68 69 70 71 72 73 74 75 76 77 78 79 80 81 82 83 84 85 86 87 88 89 90 91 92 93 94 95 96 97 98 99 100 101 102 103 104 105 106 107 108 109 110 111 112 113 114 115 116 117 118 119 120 121 122 123 124 125 126 127 128 129 130 131 132 133 134 135 136 137 138 139 140 141 142 143 144 145 146 147 148 149 150 151 152 153 154 155 156 157 158 159 160 161 162 163 164 165 166 167 168 169 170 171 172 173 174 175 176 177 178 179 180 181 182 183 184 185 186 187 188 189 190 191 192 193 194 195 196 197 198 199 200 201 202 203 204 | #include <chrono> #include "utility.hpp" // Includes common necessary includes for development using depthai library #include "depthai/depthai.hpp" static const std::vector<std::string> labelMap = { "person", "bicycle", "car", "motorbike", "aeroplane", "bus", "train", "truck", "boat", "traffic light", "fire hydrant", "stop sign", "parking meter", "bench", "bird", "cat", "dog", "horse", "sheep", "cow", "elephant", "bear", "zebra", "giraffe", "backpack", "umbrella", "handbag", "tie", "suitcase", "frisbee", "skis", "snowboard", "sports ball", "kite", "baseball bat", "baseball glove", "skateboard", "surfboard", "tennis racket", "bottle", "wine glass", "cup", "fork", "knife", "spoon", "bowl", "banana", "apple", "sandwich", "orange", "broccoli", "carrot", "hot dog", "pizza", "donut", "cake", "chair", "sofa", "pottedplant", "bed", "diningtable", "toilet", "tvmonitor", "laptop", "mouse", "remote", "keyboard", "cell phone", "microwave", "oven", "toaster", "sink", "refrigerator", "book", "clock", "vase", "scissors", "teddy bear", "hair drier", "toothbrush"}; static std::atomic<bool> syncNN{true}; int main(int argc, char** argv) { using namespace std; using namespace std::chrono; std::string nnPath(BLOB_PATH); // If path to blob specified, use that if(argc > 1) { nnPath = std::string(argv[1]); } // Print which blob we are using printf("Using blob at path: %s\n", nnPath.c_str()); // Create pipeline dai::Pipeline pipeline; // Define sources and outputs auto camRgb = pipeline.create<dai::node::ColorCamera>(); auto spatialDetectionNetwork = pipeline.create<dai::node::YoloSpatialDetectionNetwork>(); auto monoLeft = pipeline.create<dai::node::MonoCamera>(); auto monoRight = pipeline.create<dai::node::MonoCamera>(); auto stereo = pipeline.create<dai::node::StereoDepth>(); auto xoutRgb = pipeline.create<dai::node::XLinkOut>(); auto xoutNN = pipeline.create<dai::node::XLinkOut>(); auto xoutDepth = pipeline.create<dai::node::XLinkOut>(); auto nnNetworkOut = pipeline.create<dai::node::XLinkOut>(); xoutRgb->setStreamName("rgb"); xoutNN->setStreamName("detections"); xoutDepth->setStreamName("depth"); nnNetworkOut->setStreamName("nnNetwork"); // Properties camRgb->setPreviewSize(416, 416); camRgb->setResolution(dai::ColorCameraProperties::SensorResolution::THE_1080_P); camRgb->setInterleaved(false); camRgb->setColorOrder(dai::ColorCameraProperties::ColorOrder::BGR); monoLeft->setResolution(dai::MonoCameraProperties::SensorResolution::THE_400_P); monoLeft->setCamera("left"); monoRight->setResolution(dai::MonoCameraProperties::SensorResolution::THE_400_P); monoRight->setCamera("right"); // setting node configs stereo->setDefaultProfilePreset(dai::node::StereoDepth::PresetMode::HIGH_DENSITY); // Align depth map to the perspective of RGB camera, on which inference is done stereo->setDepthAlign(dai::CameraBoardSocket::CAM_A); stereo->setOutputSize(monoLeft->getResolutionWidth(), monoLeft->getResolutionHeight()); spatialDetectionNetwork->setBlobPath(nnPath); spatialDetectionNetwork->setConfidenceThreshold(0.5f); spatialDetectionNetwork->input.setBlocking(false); spatialDetectionNetwork->setBoundingBoxScaleFactor(0.5); spatialDetectionNetwork->setDepthLowerThreshold(100); spatialDetectionNetwork->setDepthUpperThreshold(5000); // yolo specific parameters spatialDetectionNetwork->setNumClasses(80); spatialDetectionNetwork->setCoordinateSize(4); spatialDetectionNetwork->setAnchors({10, 14, 23, 27, 37, 58, 81, 82, 135, 169, 344, 319}); spatialDetectionNetwork->setAnchorMasks({{"side26", {1, 2, 3}}, {"side13", {3, 4, 5}}}); spatialDetectionNetwork->setIouThreshold(0.5f); // Linking monoLeft->out.link(stereo->left); monoRight->out.link(stereo->right); camRgb->preview.link(spatialDetectionNetwork->input); if(syncNN) { spatialDetectionNetwork->passthrough.link(xoutRgb->input); } else { camRgb->preview.link(xoutRgb->input); } spatialDetectionNetwork->out.link(xoutNN->input); stereo->depth.link(spatialDetectionNetwork->inputDepth); spatialDetectionNetwork->passthroughDepth.link(xoutDepth->input); spatialDetectionNetwork->outNetwork.link(nnNetworkOut->input); // Connect to device and start pipeline dai::Device device(pipeline); // Output queues will be used to get the rgb frames and nn data from the outputs defined above auto previewQueue = device.getOutputQueue("rgb", 4, false); auto detectionNNQueue = device.getOutputQueue("detections", 4, false); auto depthQueue = device.getOutputQueue("depth", 4, false); auto networkQueue = device.getOutputQueue("nnNetwork", 4, false); auto startTime = steady_clock::now(); int counter = 0; float fps = 0; auto color = cv::Scalar(255, 255, 255); bool printOutputLayersOnce = true; while(true) { auto imgFrame = previewQueue->get<dai::ImgFrame>(); auto inDet = detectionNNQueue->get<dai::SpatialImgDetections>(); auto depth = depthQueue->get<dai::ImgFrame>(); auto inNN = networkQueue->get<dai::NNData>(); if(printOutputLayersOnce && inNN) { std::cout << "Output layer names: "; for(const auto& ten : inNN->getAllLayerNames()) { std::cout << ten << ", "; } std::cout << std::endl; printOutputLayersOnce = false; } cv::Mat frame = imgFrame->getCvFrame(); cv::Mat depthFrame = depth->getFrame(); // depthFrame values are in millimeters cv::Mat depthFrameColor; cv::normalize(depthFrame, depthFrameColor, 255, 0, cv::NORM_INF, CV_8UC1); cv::equalizeHist(depthFrameColor, depthFrameColor); cv::applyColorMap(depthFrameColor, depthFrameColor, cv::COLORMAP_HOT); counter++; auto currentTime = steady_clock::now(); auto elapsed = duration_cast<duration<float>>(currentTime - startTime); if(elapsed > seconds(1)) { fps = counter / elapsed.count(); counter = 0; startTime = currentTime; } auto detections = inDet->detections; for(const auto& detection : detections) { auto roiData = detection.boundingBoxMapping; auto roi = roiData.roi; roi = roi.denormalize(depthFrameColor.cols, depthFrameColor.rows); auto topLeft = roi.topLeft(); auto bottomRight = roi.bottomRight(); auto xmin = (int)topLeft.x; auto ymin = (int)topLeft.y; auto xmax = (int)bottomRight.x; auto ymax = (int)bottomRight.y; cv::rectangle(depthFrameColor, cv::Rect(cv::Point(xmin, ymin), cv::Point(xmax, ymax)), color, cv::FONT_HERSHEY_SIMPLEX); int x1 = detection.xmin * frame.cols; int y1 = detection.ymin * frame.rows; int x2 = detection.xmax * frame.cols; int y2 = detection.ymax * frame.rows; uint32_t labelIndex = detection.label; std::string labelStr = to_string(labelIndex); if(labelIndex < labelMap.size()) { labelStr = labelMap[labelIndex]; } cv::putText(frame, labelStr, cv::Point(x1 + 10, y1 + 20), cv::FONT_HERSHEY_TRIPLEX, 0.5, 255); std::stringstream confStr; confStr << std::fixed << std::setprecision(2) << detection.confidence * 100; cv::putText(frame, confStr.str(), cv::Point(x1 + 10, y1 + 35), cv::FONT_HERSHEY_TRIPLEX, 0.5, 255); std::stringstream depthX; depthX << "X: " << (int)detection.spatialCoordinates.x << " mm"; cv::putText(frame, depthX.str(), cv::Point(x1 + 10, y1 + 50), cv::FONT_HERSHEY_TRIPLEX, 0.5, 255); std::stringstream depthY; depthY << "Y: " << (int)detection.spatialCoordinates.y << " mm"; cv::putText(frame, depthY.str(), cv::Point(x1 + 10, y1 + 65), cv::FONT_HERSHEY_TRIPLEX, 0.5, 255); std::stringstream depthZ; depthZ << "Z: " << (int)detection.spatialCoordinates.z << " mm"; cv::putText(frame, depthZ.str(), cv::Point(x1 + 10, y1 + 80), cv::FONT_HERSHEY_TRIPLEX, 0.5, 255); cv::rectangle(frame, cv::Rect(cv::Point(x1, y1), cv::Point(x2, y2)), color, cv::FONT_HERSHEY_SIMPLEX); } std::stringstream fpsStr; fpsStr << std::fixed << std::setprecision(2) << fps; cv::putText(frame, fpsStr.str(), cv::Point(2, imgFrame->getHeight() - 4), cv::FONT_HERSHEY_TRIPLEX, 0.4, color); cv::imshow("depth", depthFrameColor); cv::imshow("rgb", frame); int key = cv::waitKey(1); if(key == 'q' || key == 'Q') { return 0; } } return 0; } |