Device¶
Device is an OAK camera or a RAE robot. On all of our devices there’s a powerful Robotics Vision Core (RVC). The RVC is optimized for performing AI inference, CV operations, and for processing sensory inputs (eg. stereo depth, video encoders, etc.).
Device API¶
Device
object represents an OAK device. When starting the device, you have to upload a Pipeline to it, which will get executed on the VPU.
When you create the device in the code, firmware is uploaded together with the pipeline and other assets (such as NN blobs).
pipeline = depthai.Pipeline()
# Create nodes, configure them and link them together
# Upload the pipeline to the device
with depthai.Device(pipeline) as device:
# Print MxID, USB speed, and available cameras on the device
print('MxId:',device.getDeviceInfo().getMxId())
print('USB speed:',device.getUsbSpeed())
print('Connected cameras:',device.getConnectedCameras())
# Input queue, to send message from the host to the device (you can receive the message on the device with XLinkIn)
input_q = device.getInputQueue("input_name", maxSize=4, blocking=False)
# Output queue, to receive message on the host from the device (you can send the message on the device with XLinkOut)
output_q = device.getOutputQueue("output_name", maxSize=4, blocking=False)
while True:
# Get a message that came from the queue
output_q.get() # Or output_q.tryGet() for non-blocking
# Send a message to the device
cfg = depthai.ImageManipConfig()
input_q.send(cfg)
Connect to specified device¶
If you have multiple devices and only want to connect to a specific one, or if your OAK PoE camera is outside of your subnet, you can specify the device (either with MxID, IP, or USB port name) you want to connect to.
# Specify MXID, IP Address or USB path
device_info = depthai.DeviceInfo("14442C108144F1D000") # MXID
#device_info = depthai.DeviceInfo("192.168.1.44") # IP Address
#device_info = depthai.DeviceInfo("3.3.3") # USB port name
with depthai.Device(pipeline, device_info) as device:
# ...
Host clock syncing¶
When depthai library connects to a device, it automatically syncs device’s timestamp to host’s timestamp. Timestamp syncing happens continuously at around 5 second intervals, and can be configured via API (example script below).
Device clocks are synced at below 500µs accuracy for PoE cameras, and below 200µs accuracy for USB cameras at 1σ (standard deviation) with host clock.
Above is a graph representing the accuracy of the device clock with respect to the host clock. We had 3 devices connected (OAK PoE cameras), all were hardware synchronized using FSYNC Y-adapter. Raspberry Pi (the host) had an interrupt pin connected to the FSYNC line, so at the start of each frame the interrupt happened and the host clock was recorded. Then we compared frame (synced) timestamps with host timestamps and computed the standard deviation. For the histogram above we ran this test for approximately 3 hours.
Below is a graph representing the difference between the device and host clock. The graph shows the difference between the device and host clock over time. The graph is a result of the same test as the previous one.
# Configure host clock syncing example
import depthai as dai
from datetime import timedelta
# Configure pipeline
with dai.Device(pipeline) as device:
# 1st value: Interval between timesync runs
# 2nd value: Number of timesync samples per run which are used to compute a better value
# 3rd value: If true partial timesync requests will be performed at random intervals, otherwise at fixed intervals
device.setTimesync(timedelta(seconds=5), 10, True) # (These are default values)
Multiple devices¶
If you want to use multiple devices on a host, check Multiple DepthAI per Host.
Device queues¶
After initializing the device, you can create input/output queues that match XLinkIn/XLinkOut nodes in the pipeline. These queues will be located on the host computer (in RAM).
pipeline = dai.Pipeline()
xout = pipeline.createXLinkOut()
xout.setStreamName("output_name")
# ...
xin = pipeline.createXLinkIn()
xin.setStreamName("input_name")
# ...
with dai.Device(pipeline) as device:
outputQueue = device.getOutputQueue("output_name", maxSize=5, blocking=False)
inputQueue = device.getInputQueue("input_name")
outputQueue.get() # Read from the queue, blocks until message arrives
outputQueue.tryGet() # Read from the queue, returns None if there's no msg (doesn't block)
if outputQueue.has(): # Check if there are any messages in the queue
When you define an output queue, the device can push new messages to it at any time, and the host can read from it at any time.
Output queue - maxSize and blocking¶
When the host is reading very fast from the queue (inside while True loop), the queue, regardless of its size, will stay empty most of the time. But as we add things on the host side (additional processing, analysis, etc), it may happen that the device will be pushing messages to the queue faster than the host can read from it. And then the messages in the queue will start to increase - and both maxSize and blocking flags determine the behavior of the queue in this case. Two common configurations are:
with dai.Device(pipeline) as device:
# If you want only the latest message, and don't care about previous ones;
# When a new msg arrives to the host, it will overwrite the previous (oldest) one if it's still in the queue
q1 = device.getOutputQueue(name="name1", maxSize=1, blocking=False)
# If you care about every single message (eg. H264/5 encoded video; if you miss a frame, you will get artifacts);
# If the queue is full, the device will wait until the host reads a message from the queue
q2 = device.getOutputQueue(name="name2", maxSize=30, blocking=True) # Also default values (maxSize=30/blocking=True)
We used maxSize=30 just as an example, but it can be any int16 number. Since device queues are on the host computer, memory (RAM) usually isn’t that scarce, so maxSize wouldn’t matter that much. But if you are using a small SBC like RPI Zero (512MB RAM), and are streaming large frames (eg. 4K unencoded), you could quickly run out of memory if you set maxSize to a high value (and don’t read from the queue fast enough).
Some additional information¶
Queues are thread-safe - they can be accessed from any thread.
Queues are created such that each queue is its own thread which takes care of receiving, serializing/deserializing, and sending the messages forward (same for input/output queues).
The
Device
object isn’t fully thread-safe. Some RPC calls (eg.getLogLevel
,setLogLevel
,getDdrMemoryUsage
) will get thread-safe once the mutex is set in place (right now there could be races).
Watchdog¶
The watchdog is a crucial component in the operation of POE (Power over Ethernet) devices with DepthAI. When DepthAI disconnects from a POE device, the watchdog mechanism is the first to respond, initiating a reset of the camera. This reset is followed by a complete system reboot, which includes the loading of the DepthAI bootloader and the initialization of the entire networking stack.
The watchdog process is necessary to make the camera available for reconnection and typically takes about 10 seconds, which means the fastest possible reconnection time is 10 seconds.
Customizing the Watchdog Timeout¶
Set the environment variables DEPTHAI_WATCHDOG_INITIAL_DELAY and DEPTHAI_BOOTUP_TIMEOUT to your desired timeout values (in milliseconds) as follows:
DEPTHAI_WATCHDOG_INITIAL_DELAY=<my_value> DEPTHAI_BOOTUP_TIMEOUT=<my_value> python3 script.py
For Windows PowerShell, set the environment variables like this:
$env:DEPTHAI_WATCHDOG_INITIAL_DELAY=<my_value>
$env:DEPTHAI_BOOTUP_TIMEOUT=<my_value>
python3 script.py
In Windows CMD, you can set the environment variables as follows:
set DEPTHAI_WATCHDOG_INITIAL_DELAY=<my_value>
set DEPTHAI_BOOTUP_TIMEOUT=<my_value>
python3 script.py
Alternatively, you can set the timeout directly in your code:
pipeline = depthai.Pipeline()
# Create a BoardConfig object
config = depthai.BoardConfig()
# Set the parameters
config.watchdogInitialDelayMs = <my_value>
config.watchdogTimeoutMs = <my_value>
pipeline.setBoardConfig(config)
By adjusting these settings, you can tailor the watchdog functionality to better suit your specific requirements.
Environment Variables¶
The following table lists various environment variables used in the system, along with their descriptions:
Environment Variable |
Description |
---|---|
DEPTHAI_LEVEL |
Sets logging verbosity, options: ‘trace’, ‘debug’, ‘warn’, ‘error’, ‘off’ |
XLINK_LEVEL |
Sets logging verbosity of XLink library, options: ‘debug’, ‘info’, ‘warn’, ‘error’, ‘fatal’, ‘off’ |
DEPTHAI_INSTALL_SIGNAL_HANDLER |
Set to 0 to disable installing Backward signal handler for stack trace printing |
DEPTHAI_WATCHDOG |
Sets device watchdog timeout. Useful for debugging (DEPTHAI_WATCHDOG=0), to prevent device reset while the process is paused. |
DEPTHAI_WATCHDOG_INITIAL_DELAY |
Specifies delay after which the device watchdog starts. |
DEPTHAI_SEARCH_TIMEOUT |
Specifies timeout in milliseconds for device searching in blocking functions. |
DEPTHAI_CONNECT_TIMEOUT |
Specifies timeout in milliseconds for establishing a connection to a given device. |
DEPTHAI_BOOTUP_TIMEOUT |
Specifies timeout in milliseconds for waiting the device to boot after sending the binary. |
DEPTHAI_PROTOCOL |
Restricts default search to the specified protocol. Options: any, usb, tcpip. |
DEPTHAI_DEVICE_MXID_LIST |
Restricts default search to the specified MXIDs. Accepts comma separated list of MXIDs. Lists filter results in an “AND” manner and not “OR” |
DEPTHAI_DEVICE_ID_LIST |
Alias to MXID list. Lists filter results in an “AND” manner and not “OR” |
DEPTHAI_DEVICE_NAME_LIST |
Restricts default search to the specified NAMEs. Accepts comma separated list of NAMEs. Lists filter results in an “AND” manner and not “OR” |
DEPTHAI_DEVICE_BINARY |
Overrides device Firmware binary. Mostly for internal debugging purposes. |
DEPTHAI_BOOTLOADER_BINARY_USB |
Overrides device USB Bootloader binary. Mostly for internal debugging purposes. |
DEPTHAI_BOOTLOADER_BINARY_ETH |
Overrides device Network Bootloader binary. Mostly for internal debugging purposes. |
Reference¶
-
class
depthai.
Device
Represents the DepthAI device with the methods to interact with it. Implements the host-side queues to connect with XLinkIn and XLinkOut nodes
-
class
Config
Device specific configuration
-
addLogCallback
(self: depthai.DeviceBase, callback: Callable[[depthai.LogMessage], None]) → int Add a callback for device logging. The callback will be called from a separate thread with the LogMessage being passed.
- Parameter
callback
: Callback to call whenever a log message arrives
- Returns
Id which can be used to later remove the callback
- Parameter
-
close
(self: depthai.DeviceBase) → None Closes the connection to device. Better alternative is the usage of context manager: with depthai.Device(pipeline) as device:
-
factoryResetCalibration
(self: depthai.DeviceBase) → None Factory reset EEPROM data if factory backup is available.
- Throws:
std::runtime_exception If factory reset was unsuccessful
-
flashCalibration
(self: depthai.DeviceBase, calibrationDataHandler: depthai.CalibrationHandler) → bool Stores the Calibration and Device information to the Device EEPROM
- Parameter
calibrationObj
: CalibrationHandler object which is loaded with calibration information.
- Returns
true on successful flash, false on failure
- Parameter
-
flashCalibration2
(self: depthai.DeviceBase, arg0: depthai.CalibrationHandler) → None Stores the Calibration and Device information to the Device EEPROM
- Throws:
std::runtime_exception if failed to flash the calibration
- Parameter
calibrationObj
: CalibrationHandler object which is loaded with calibration information.
-
flashEepromClear
(self: depthai.DeviceBase) → None Destructive action, deletes User area EEPROM contents Requires PROTECTED permissions
- Throws:
std::runtime_exception if failed to flash the calibration
- Returns
True on successful flash, false on failure
-
flashFactoryCalibration
(self: depthai.DeviceBase, arg0: depthai.CalibrationHandler) → None Stores the Calibration and Device information to the Device EEPROM in Factory area To perform this action, correct env variable must be set
- Throws:
std::runtime_exception if failed to flash the calibration
- Returns
True on successful flash, false on failure
-
flashFactoryEepromClear
(self: depthai.DeviceBase) → None Destructive action, deletes Factory area EEPROM contents Requires FACTORY PROTECTED permissions
- Throws:
std::runtime_exception if failed to flash the calibration
- Returns
True on successful flash, false on failure
-
static
getAllAvailableDevices
() → List[depthai.DeviceInfo] Returns all available devices
- Returns
Vector of available devices
-
static
getAllConnectedDevices
() → List[depthai.DeviceInfo] Returns information of all connected devices. The devices could be both connectable as well as already connected to devices.
- Returns
Vector of connected device information
-
static
getAnyAvailableDevice
(*args, **kwargs) Overloaded function.
getAnyAvailableDevice(timeout: datetime.timedelta) -> Tuple[bool, depthai.DeviceInfo]
Waits for any available device with a timeout
- Parameter
timeout
: duration of time to wait for the any device
- Returns
Tuple of bool and DeviceInfo. Bool specifies if device was found. DeviceInfo specifies the found device
getAnyAvailableDevice() -> Tuple[bool, depthai.DeviceInfo]
Gets any available device
- Returns
Tuple of bool and DeviceInfo. Bool specifies if device was found. DeviceInfo specifies the found device
-
getAvailableStereoPairs
(self: depthai.DeviceBase) → List[depthai.StereoPair] Get stereo pairs taking into account the calibration and connected cameras.
@note This method will always return a subset of getStereoPairs.
- Returns
Vector of stereo pairs
-
getBootloaderVersion
(self: depthai.DeviceBase) → Optional[depthai.Version] Gets Bootloader version if it was booted through Bootloader
- Returns
DeviceBootloader::Version if booted through Bootloader or none otherwise
-
getCameraSensorNames
(self: depthai.DeviceBase) → Dict[depthai.CameraBoardSocket, str] Get sensor names for cameras that are connected to the device
- Returns
Map/dictionary with camera sensor names, indexed by socket
-
getChipTemperature
(self: depthai.DeviceBase) → depthai.ChipTemperature Retrieves current chip temperature as measured by device
- Returns
Temperature of various onboard sensors
-
getCmxMemoryUsage
(self: depthai.DeviceBase) → depthai.MemoryInfo Retrieves current CMX memory information from device
- Returns
Used, remaining and total cmx memory
-
getConnectedCameraFeatures
(self: depthai.DeviceBase) → List[depthai.CameraFeatures] Get cameras that are connected to the device with their features/properties
- Returns
Vector of connected camera features
-
getConnectedCameras
(self: depthai.DeviceBase) → List[depthai.CameraBoardSocket] Get cameras that are connected to the device
- Returns
Vector of connected cameras
-
getConnectedIMU
(self: depthai.DeviceBase) → str Get connected IMU type
- Returns
IMU type
-
getConnectionInterfaces
(self: depthai.DeviceBase) → List[depthai.connectionInterface] Get connection interfaces for device
- Returns
Vector of connection type
-
getCrashDump
(self: depthai.DeviceBase, clearCrashDump: bool = True) → depthai.CrashDump Retrieves crash dump for debugging.
-
getDdrMemoryUsage
(self: depthai.DeviceBase) → depthai.MemoryInfo Retrieves current DDR memory information from device
- Returns
Used, remaining and total ddr memory
-
static
getDeviceByMxId
(mxId: str) → Tuple[bool, depthai.DeviceInfo] Finds a device by MX ID. Example: 14442C10D13EABCE00
- Parameter
mxId
: MyraidX ID which uniquely specifies a device
- Returns
Tuple of bool and DeviceInfo. Bool specifies if device was found. DeviceInfo specifies the found device
- Parameter
-
getDeviceInfo
(self: depthai.DeviceBase) → depthai.DeviceInfo Get the Device Info object o the device which is currently running
- Returns
DeviceInfo of the current device in execution
-
getDeviceName
(self: depthai.DeviceBase) → object Get device name if available
- Returns
device name or empty string if not available
-
static
getEmbeddedDeviceBinary
(*args, **kwargs) Overloaded function.
getEmbeddedDeviceBinary(usb2Mode: bool, version: depthai.OpenVINO.Version = <Version.???: 7>) -> List[int]
Gets device firmware binary for a specific OpenVINO version
- Parameter
usb2Mode
: USB2 mode firmware
- Parameter
version
: Version of OpenVINO which firmware will support
- Returns
Firmware binary
getEmbeddedDeviceBinary(config: depthai.Device.Config) -> List[int]
Gets device firmware binary for a specific configuration
- Parameter
config
: FW with applied configuration
- Returns
Firmware binary
-
getEmbeddedIMUFirmwareVersion
(self: depthai.DeviceBase) → depthai.Version Get embedded IMU firmware version to which IMU can be upgraded
- Returns
Get embedded IMU firmware version to which IMU can be upgraded.
-
static
getFirstAvailableDevice
(skipInvalidDevices: bool = True) → Tuple[bool, depthai.DeviceInfo] Gets first available device. Device can be either in XLINK_UNBOOTED or XLINK_BOOTLOADER state
- Returns
Tuple of bool and DeviceInfo. Bool specifies if device was found. DeviceInfo specifies the found device
-
static
getGlobalProfilingData
() → depthai.ProfilingData Get current global accumulated profiling data
- Returns
ProfilingData from all devices
-
getIMUFirmwareUpdateStatus
(self: depthai.DeviceBase) → Tuple[bool, int] Get IMU firmware update status
- Returns
Whether IMU firmware update is done and last firmware update progress as percentage. return value true and 100 means that the update was successful return value true and other than 100 means that the update failed
-
getIMUFirmwareVersion
(self: depthai.DeviceBase) → depthai.Version Get connected IMU firmware version
- Returns
IMU firmware version
-
getInputQueue
(*args, **kwargs) Overloaded function.
getInputQueue(self: depthai.Device, name: str) -> depthai.DataInputQueue
Gets an input queue corresponding to stream name. If it doesn’t exist it throws
- Parameter
name
: Queue/stream name, set in XLinkIn node
- Returns
Smart pointer to DataInputQueue
getInputQueue(self: depthai.Device, name: str, maxSize: int, blocking: bool = True) -> depthai.DataInputQueue
Gets an input queue corresponding to stream name. If it doesn’t exist it throws. Also sets queue options
- Parameter
name
: Queue/stream name, set in XLinkIn node
- Parameter
maxSize
: Maximum number of messages in queue
- Parameter
blocking
: Queue behavior once full. True: blocking, false: overwriting of oldest messages. Default: true
- Returns
Smart pointer to DataInputQueue
-
getInputQueueNames
(self: depthai.Device) → List[str] Get all available input queue names
- Returns
Vector of input queue names
-
getIrDrivers
(self: depthai.DeviceBase) → List[Tuple[str, int, int]] Retrieves detected IR laser/LED drivers.
- Returns
driver name, I2C bus, I2C address. For OAK-D- Pro it should be [{“LM3644”, 2, 0x63}]
- Return type
Vector of tuples containing
-
getLeonCssCpuUsage
(self: depthai.DeviceBase) → depthai.CpuUsage Retrieves average CSS Leon CPU usage
- Returns
Average CPU usage and sampling duration
-
getLeonCssHeapUsage
(self: depthai.DeviceBase) → depthai.MemoryInfo Retrieves current CSS Leon CPU heap information from device
- Returns
Used, remaining and total heap memory
-
getLeonMssCpuUsage
(self: depthai.DeviceBase) → depthai.CpuUsage Retrieves average MSS Leon CPU usage
- Returns
Average CPU usage and sampling duration
-
getLeonMssHeapUsage
(self: depthai.DeviceBase) → depthai.MemoryInfo Retrieves current MSS Leon CPU heap information from device
- Returns
Used, remaining and total heap memory
-
getLogLevel
(self: depthai.DeviceBase) → depthai.LogLevel Gets current logging severity level of the device.
- Returns
Logging severity level
-
getLogOutputLevel
(self: depthai.DeviceBase) → depthai.LogLevel Gets logging level which decides printing level to standard output.
- Returns
Standard output printing severity
-
getMxId
(self: depthai.DeviceBase) → str Get MxId of device
- Returns
MxId of connected device
-
getOutputQueue
(*args, **kwargs) Overloaded function.
getOutputQueue(self: depthai.Device, name: str) -> depthai.DataOutputQueue
Gets an output queue corresponding to stream name. If it doesn’t exist it throws
- Parameter
name
: Queue/stream name, created by XLinkOut node
- Returns
Smart pointer to DataOutputQueue
getOutputQueue(self: depthai.Device, name: str, maxSize: int, blocking: bool = True) -> depthai.DataOutputQueue
Gets a queue corresponding to stream name, if it exists, otherwise it throws. Also sets queue options
- Parameter
name
: Queue/stream name, set in XLinkOut node
- Parameter
maxSize
: Maximum number of messages in queue
- Parameter
blocking
: Queue behavior once full. True specifies blocking and false overwriting of oldest messages. Default: true
- Returns
Smart pointer to DataOutputQueue
-
getOutputQueueNames
(self: depthai.Device) → List[str] Get all available output queue names
- Returns
Vector of output queue names
-
getProductName
(self: depthai.DeviceBase) → object Get product name if available
- Returns
product name or empty string if not available
-
getProfilingData
(self: depthai.DeviceBase) → depthai.ProfilingData Get current accumulated profiling data
- Returns
ProfilingData from the specific device
-
getQueueEvent
(*args, **kwargs) Overloaded function.
getQueueEvent(self: depthai.Device, queueNames: List[str], timeout: datetime.timedelta = datetime.timedelta(days=-1, seconds=86399, microseconds=999999)) -> str
Gets or waits until any of specified queues has received a message
- Parameter
queueNames
: Names of queues for which to wait for
- Parameter
timeout
: Timeout after which return regardless. If negative then wait is indefinite. Default is -1
- Returns
Queue name which received a message first
getQueueEvent(self: depthai.Device, queueName: str, timeout: datetime.timedelta = datetime.timedelta(days=-1, seconds=86399, microseconds=999999)) -> str
Gets or waits until specified queue has received a message
- Parameter
queueNames
: Name of queues for which to wait for
- Parameter
timeout
: Timeout after which return regardless. If negative then wait is indefinite. Default is -1
- Returns
Queue name which received a message
getQueueEvent(self: depthai.Device, timeout: datetime.timedelta = datetime.timedelta(days=-1, seconds=86399, microseconds=999999)) -> str
Gets or waits until any queue has received a message
- Parameter
timeout
: Timeout after which return regardless. If negative then wait is indefinite. Default is -1
- Returns
Queue name which received a message
-
getQueueEvents
(*args, **kwargs) Overloaded function.
getQueueEvents(self: depthai.Device, queueNames: List[str], maxNumEvents: int = 18446744073709551615, timeout: datetime.timedelta = datetime.timedelta(days=-1, seconds=86399, microseconds=999999)) -> List[str]
Gets or waits until any of specified queues has received a message
- Parameter
queueNames
: Names of queues for which to block
- Parameter
maxNumEvents
: Maximum number of events to remove from queue - Default is unlimited
- Parameter
timeout
: Timeout after which return regardless. If negative then wait is indefinite - Default is -1
- Returns
Names of queues which received messages first
getQueueEvents(self: depthai.Device, queueName: str, maxNumEvents: int = 18446744073709551615, timeout: datetime.timedelta = datetime.timedelta(days=-1, seconds=86399, microseconds=999999)) -> List[str]
Gets or waits until specified queue has received a message
- Parameter
queueName
: Name of queues for which to wait for
- Parameter
maxNumEvents
: Maximum number of events to remove from queue. Default is unlimited
- Parameter
timeout
: Timeout after which return regardless. If negative then wait is indefinite. Default is -1
- Returns
Names of queues which received messages first
getQueueEvents(self: depthai.Device, maxNumEvents: int = 18446744073709551615, timeout: datetime.timedelta = datetime.timedelta(days=-1, seconds=86399, microseconds=999999)) -> List[str]
Gets or waits until any queue has received a message
- Parameter
maxNumEvents
: Maximum number of events to remove from queue. Default is unlimited
- Parameter
timeout
: Timeout after which return regardless. If negative then wait is indefinite. Default is -1
- Returns
Names of queues which received messages first
-
getStereoPairs
(self: depthai.DeviceBase) → List[depthai.StereoPair] Get stereo pairs based on the device type.
- Returns
Vector of stereo pairs
-
getSystemInformationLoggingRate
(self: depthai.DeviceBase) → float Gets current rate of system information logging (“info” severity) in Hz.
- Returns
Logging rate in Hz
-
getUsbSpeed
(self: depthai.DeviceBase) → depthai.UsbSpeed Retrieves USB connection speed
- Returns
USB connection speed of connected device if applicable. Unknown otherwise.
-
getXLinkChunkSize
(self: depthai.DeviceBase) → int Gets current XLink chunk size.
- Returns
XLink chunk size in bytes
-
hasCrashDump
(self: depthai.DeviceBase) → bool Retrieves whether the is crash dump stored on device or not.
-
isClosed
(self: depthai.DeviceBase) → bool Is the device already closed (or disconnected)
Warning
This function is thread-unsafe and may return outdated incorrect values. It is only meant for use in simple single-threaded code. Well written code should handle exceptions when calling any DepthAI apis to handle hardware events and multithreaded use.
-
isEepromAvailable
(self: depthai.DeviceBase) → bool Check if EEPROM is available
- Returns
True if EEPROM is present on board, false otherwise
-
isPipelineRunning
(self: depthai.DeviceBase) → bool Checks if devices pipeline is already running
- Returns
True if running, false otherwise
-
readCalibration
(self: depthai.DeviceBase) → depthai.CalibrationHandler Fetches the EEPROM data from the device and loads it into CalibrationHandler object If no calibration is flashed, it returns default
- Returns
The CalibrationHandler object containing the calibration currently flashed on device EEPROM
-
readCalibration2
(self: depthai.DeviceBase) → depthai.CalibrationHandler Fetches the EEPROM data from the device and loads it into CalibrationHandler object
- Throws:
std::runtime_exception if no calibration is flashed
- Returns
The CalibrationHandler object containing the calibration currently flashed on device EEPROM
-
readCalibrationOrDefault
(self: depthai.DeviceBase) → depthai.CalibrationHandler Fetches the EEPROM data from the device and loads it into CalibrationHandler object If no calibration is flashed, it returns default
- Returns
The CalibrationHandler object containing the calibration currently flashed on device EEPROM
-
readCalibrationRaw
(self: depthai.DeviceBase) → List[int] Fetches the raw EEPROM data from User area
- Throws:
std::runtime_exception if any error occurred
- Returns
Binary dump of User area EEPROM data
-
readFactoryCalibration
(self: depthai.DeviceBase) → depthai.CalibrationHandler Fetches the EEPROM data from Factory area and loads it into CalibrationHandler object
- Throws:
std::runtime_exception if no calibration is flashed
- Returns
The CalibrationHandler object containing the calibration currently flashed on device EEPROM in Factory Area
-
readFactoryCalibrationOrDefault
(self: depthai.DeviceBase) → depthai.CalibrationHandler Fetches the EEPROM data from Factory area and loads it into CalibrationHandler object If no calibration is flashed, it returns default
- Returns
The CalibrationHandler object containing the calibration currently flashed on device EEPROM in Factory Area
-
readFactoryCalibrationRaw
(self: depthai.DeviceBase) → List[int] Fetches the raw EEPROM data from Factory area
- Throws:
std::runtime_exception if any error occurred
- Returns
Binary dump of Factory area EEPROM data
-
removeLogCallback
(self: depthai.DeviceBase, callbackId: int) → bool Removes a callback
- Parameter
callbackId
: Id of callback to be removed
- Returns
True if callback was removed, false otherwise
- Parameter
-
setIrFloodLightBrightness
(self: depthai.DeviceBase, mA: float, mask: int = - 1) → bool Sets the brightness of the IR Flood Light. Limits: up to 1500mA at 30% duty cycle. The duty cycle is controlled by the left camera STROBE, aligned to start of exposure. If the dot projector is also enabled, its lower duty cycle limits take precedence. The emitter is turned off by default
- Parameter
mA
: Current in mA that will determine brightness, 0 or negative to turn off
- Parameter
mask
: Optional mask to modify only Left (0x1) or Right (0x2) sides on OAK-D-Pro-W- DEV
- Returns
True on success, false if not found or other failure
- Parameter
-
setIrFloodLightIntensity
(self: depthai.DeviceBase, intensity: float, mask: int = - 1) → bool Sets the intensity of the IR Flood Light. Limits: Intensity is directly normalized to 0 - 1500mA current. The duty cycle is 30% when exposure time is longer than 30% frame time. Otherwise, duty cycle is 100% of exposure time. The duty cycle is controlled by the left camera STROBE, aligned to start of exposure. The emitter is turned off by default
- Parameter
intensity
: Intensity on range 0 to 1, that will determine brightness, 0 or negative to turn off
- Parameter
mask
: Optional mask to modify only Left (0x1) or Right (0x2) sides on OAK-D-Pro-W- DEV
- Returns
True on success, false if not found or other failure
- Parameter
-
setIrLaserDotProjectorBrightness
(self: depthai.DeviceBase, mA: float, mask: int = - 1) → bool Sets the brightness of the IR Laser Dot Projector. Limits: up to 765mA at 30% duty cycle, up to 1200mA at 6% duty cycle. The duty cycle is controlled by left camera STROBE, aligned to start of exposure. The emitter is turned off by default
- Parameter
mA
: Current in mA that will determine brightness, 0 or negative to turn off
- Parameter
mask
: Optional mask to modify only Left (0x1) or Right (0x2) sides on OAK-D-Pro-W- DEV
- Returns
True on success, false if not found or other failure
- Parameter
-
setIrLaserDotProjectorIntensity
(self: depthai.DeviceBase, intensity: float, mask: int = - 1) → bool Sets the intensity of the IR Laser Dot Projector. Limits: up to 765mA at 30% frame time duty cycle when exposure time is longer than 30% frame time. Otherwise, duty cycle is 100% of exposure time, with current increased up to max 1200mA to make up for shorter duty cycle. The duty cycle is controlled by left camera STROBE, aligned to start of exposure. The emitter is turned off by default
- Parameter
intensity
: Intensity on range 0 to 1, that will determine brightness. 0 or negative to turn off
- Parameter
mask
: Optional mask to modify only Left (0x1) or Right (0x2) sides on OAK-D-Pro-W- DEV
- Returns
True on success, false if not found or other failure
- Parameter
-
setLogLevel
(self: depthai.DeviceBase, level: depthai.LogLevel) → None Sets the devices logging severity level. This level affects which logs are transferred from device to host.
- Parameter
level
: Logging severity
- Parameter
-
setLogOutputLevel
(self: depthai.DeviceBase, level: depthai.LogLevel) → None Sets logging level which decides printing level to standard output. If lower than setLogLevel, no messages will be printed
- Parameter
level
: Standard output printing severity
- Parameter
-
setSystemInformationLoggingRate
(self: depthai.DeviceBase, rateHz: float) → None Sets rate of system information logging (“info” severity). Default 1Hz If parameter is less or equal to zero, then system information logging will be disabled
- Parameter
rateHz
: Logging rate in Hz
- Parameter
-
setTimesync
(*args, **kwargs) Overloaded function.
setTimesync(self: depthai.DeviceBase, arg0: datetime.timedelta, arg1: int, arg2: bool) -> None
Configures Timesync service on device. It keeps host and device clocks in sync First time timesync is started it waits until the initial sync is completed Afterwards the function changes the following parameters
- Parameter
period
: Interval between timesync runs
- Parameter
numSamples
: Number of timesync samples per run which are used to compute a better value. Set to zero to disable timesync
- Parameter
random
: If true partial timesync requests will be performed at random intervals, otherwise at fixed intervals
setTimesync(self: depthai.DeviceBase, enable: bool) -> None
Enables or disables Timesync service on device. It keeps host and device clocks in sync.
- Parameter
enable
: Enables or disables consistent timesyncing
-
setXLinkChunkSize
(self: depthai.DeviceBase, sizeBytes: int) → None Sets the chunk size for splitting device-sent XLink packets. A larger value could increase performance, and 0 disables chunking. A negative value is ignored. Device defaults are configured per protocol, currently 64*1024 for both USB and Ethernet.
- Parameter
sizeBytes
: XLink chunk size in bytes
- Parameter
-
startIMUFirmwareUpdate
(self: depthai.DeviceBase, forceUpdate: bool = False) → bool Starts IMU firmware update asynchronously only if IMU node is not running. If current firmware version is the same as embedded firmware version then it’s no- op. Can be overridden by forceUpdate parameter. State of firmware update can be monitored using getIMUFirmwareUpdateStatus API.
- Parameter
forceUpdate
: Force firmware update or not. Will perform FW update regardless of current version and embedded firmware version.
- Returns
Returns whether firmware update can be started. Returns false if IMU node is started.
- Parameter
-
startPipeline
(*args, **kwargs) Overloaded function.
startPipeline(self: depthai.DeviceBase) -> None
Starts the execution of the devices pipeline
- Returns
True if pipeline started, false otherwise
startPipeline(self: depthai.DeviceBase, arg0: depthai.Pipeline) -> bool
Starts the execution of a given pipeline
- Parameter
pipeline
: OpenVINO version of the pipeline must match the one which the device was booted with.
- Returns
True if pipeline started, false otherwise
-
class
-
class
dai
::
Device
: public dai::DeviceBase¶ Represents the DepthAI device with the methods to interact with it. Implements the host-side queues to connect with XLinkIn and XLinkOut nodes
Public Functions
-
Device
(const Pipeline &pipeline)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout.
- Parameters
pipeline
: Pipeline to be executed on the device
-
template<typename
T
, std::enable_if_t<std::is_same<T, bool>::value, bool> = true>Device
(const Pipeline &pipeline, T usb2Mode)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout.
- Parameters
pipeline
: Pipeline to be executed on the deviceusb2Mode
: (bool) Boot device using USB2 mode firmware
-
Device
(const Pipeline &pipeline, UsbSpeed maxUsbSpeed)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout.
- Parameters
pipeline
: Pipeline to be executed on the devicemaxUsbSpeed
: Maximum allowed USB speed
-
Device
(const Pipeline &pipeline, const dai::Path &pathToCmd)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout.
-
Device
(const Pipeline &pipeline, const DeviceInfo &devInfo)¶ Connects to device specified by devInfo.
- Parameters
pipeline
: Pipeline to be executed on the devicedevInfo
: DeviceInfo which specifies which device to connect to
-
template<typename
T
, std::enable_if_t<std::is_same<T, bool>::value, bool> = true>Device
(const Pipeline &pipeline, const DeviceInfo &devInfo, T usb2Mode)¶ Connects to device specified by devInfo.
- Parameters
pipeline
: Pipeline to be executed on the devicedevInfo
: DeviceInfo which specifies which device to connect tousb2Mode
: (bool) Boot device using USB2 mode firmware
-
Device
(const Pipeline &pipeline, const DeviceInfo &devInfo, UsbSpeed maxUsbSpeed)¶ Connects to device specified by devInfo.
- Parameters
pipeline
: Pipeline to be executed on the devicedevInfo
: DeviceInfo which specifies which device to connect tomaxUsbSpeed
: Maximum allowed USB speed
-
Device
(const Pipeline &pipeline, const DeviceInfo &devInfo, const dai::Path &pathToCmd)¶ Connects to device specified by devInfo.
- Parameters
pipeline
: Pipeline to be executed on the devicedevInfo
: DeviceInfo which specifies which device to connect topathToCmd
: Path to custom device firmware
-
Device
()¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout. Uses OpenVINO version OpenVINO::VERSION_UNIVERSAL
-
~Device
() override¶ dtor to close the device
-
std::shared_ptr<DataOutputQueue>
getOutputQueue
(const std::string &name)¶ Gets an output queue corresponding to stream name. If it doesn’t exist it throws
- Return
Smart pointer to DataOutputQueue
- Parameters
name
: Queue/stream name, created by XLinkOut node
-
std::shared_ptr<DataOutputQueue>
getOutputQueue
(const std::string &name, unsigned int maxSize, bool blocking = true)¶ Gets a queue corresponding to stream name, if it exists, otherwise it throws. Also sets queue options
- Return
Smart pointer to DataOutputQueue
- Parameters
name
: Queue/stream name, set in XLinkOut nodemaxSize
: Maximum number of messages in queueblocking
: Queue behavior once full. True specifies blocking and false overwriting of oldest messages. Default: true
-
std::vector<std::string>
getOutputQueueNames
() const¶ Get all available output queue names
- Return
Vector of output queue names
-
std::shared_ptr<DataInputQueue>
getInputQueue
(const std::string &name)¶ Gets an input queue corresponding to stream name. If it doesn’t exist it throws
- Return
Smart pointer to DataInputQueue
- Parameters
name
: Queue/stream name, set in XLinkIn node
-
std::shared_ptr<DataInputQueue>
getInputQueue
(const std::string &name, unsigned int maxSize, bool blocking = true)¶ Gets an input queue corresponding to stream name. If it doesn’t exist it throws. Also sets queue options
- Return
Smart pointer to DataInputQueue
- Parameters
name
: Queue/stream name, set in XLinkIn nodemaxSize
: Maximum number of messages in queueblocking
: Queue behavior once full. True: blocking, false: overwriting of oldest messages. Default: true
-
std::vector<std::string>
getInputQueueNames
() const¶ Get all available input queue names
- Return
Vector of input queue names
-
std::vector<std::string>
getQueueEvents
(const std::vector<std::string> &queueNames, std::size_t maxNumEvents = std::numeric_limits<std::size_t>::max(), std::chrono::microseconds timeout = std::chrono::microseconds(-1))¶ Gets or waits until any of specified queues has received a message
- Return
Names of queues which received messages first
- Parameters
queueNames
: Names of queues for which to blockmaxNumEvents
: Maximum number of events to remove from queue - Default is unlimitedtimeout
: Timeout after which return regardless. If negative then wait is indefinite - Default is -1
-
std::vector<std::string>
getQueueEvents
(const std::initializer_list<std::string> &queueNames, std::size_t maxNumEvents = std::numeric_limits<std::size_t>::max(), std::chrono::microseconds timeout = std::chrono::microseconds(-1))¶
-
std::vector<std::string>
getQueueEvents
(std::string queueName, std::size_t maxNumEvents = std::numeric_limits<std::size_t>::max(), std::chrono::microseconds timeout = std::chrono::microseconds(-1))¶ Gets or waits until specified queue has received a message
- Return
Names of queues which received messages first
- Parameters
queueName
: Name of queues for which to wait formaxNumEvents
: Maximum number of events to remove from queue. Default is unlimitedtimeout
: Timeout after which return regardless. If negative then wait is indefinite. Default is -1
-
std::vector<std::string>
getQueueEvents
(std::size_t maxNumEvents = std::numeric_limits<std::size_t>::max(), std::chrono::microseconds timeout = std::chrono::microseconds(-1))¶ Gets or waits until any queue has received a message
- Return
Names of queues which received messages first
- Parameters
maxNumEvents
: Maximum number of events to remove from queue. Default is unlimitedtimeout
: Timeout after which return regardless. If negative then wait is indefinite. Default is -1
-
std::string
getQueueEvent
(const std::vector<std::string> &queueNames, std::chrono::microseconds timeout = std::chrono::microseconds(-1))¶ Gets or waits until any of specified queues has received a message
- Return
Queue name which received a message first
- Parameters
queueNames
: Names of queues for which to wait fortimeout
: Timeout after which return regardless. If negative then wait is indefinite. Default is -1
-
std::string
getQueueEvent
(const std::initializer_list<std::string> &queueNames, std::chrono::microseconds timeout = std::chrono::microseconds(-1))¶
-
std::string
getQueueEvent
(std::string queueName, std::chrono::microseconds timeout = std::chrono::microseconds(-1))¶ Gets or waits until specified queue has received a message
- Return
Queue name which received a message
- Parameters
queueNames
: Name of queues for which to wait fortimeout
: Timeout after which return regardless. If negative then wait is indefinite. Default is -1
-
std::string
getQueueEvent
(std::chrono::microseconds timeout = std::chrono::microseconds(-1))¶ Gets or waits until any queue has received a message
- Return
Queue name which received a message
- Parameters
timeout
: Timeout after which return regardless. If negative then wait is indefinite. Default is -1
-
DeviceBase
(const Pipeline &pipeline)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout.
- Parameters
pipeline
: Pipeline to be executed on the device
-
template<typename
T
, std::enable_if_t<std::is_same<T, bool>::value, bool> = true>DeviceBase
(const Pipeline &pipeline, T usb2Mode)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout.
- Parameters
pipeline
: Pipeline to be executed on the deviceusb2Mode
: Boot device using USB2 mode firmware
-
DeviceBase
(const Pipeline &pipeline, UsbSpeed maxUsbSpeed)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout.
- Parameters
pipeline
: Pipeline to be executed on the devicemaxUsbSpeed
: Maximum allowed USB speed
-
DeviceBase
(const Pipeline &pipeline, const dai::Path &pathToCmd)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout.
-
DeviceBase
(const Pipeline &pipeline, const DeviceInfo &devInfo)¶ Connects to device specified by devInfo.
- Parameters
pipeline
: Pipeline to be executed on the devicedevInfo
: DeviceInfo which specifies which device to connect to
-
template<typename
T
, std::enable_if_t<std::is_same<T, bool>::value, bool> = true>DeviceBase
(const Pipeline &pipeline, const DeviceInfo &devInfo, T usb2Mode)¶ Connects to device specified by devInfo.
- Parameters
pipeline
: Pipeline to be executed on the devicedevInfo
: DeviceInfo which specifies which device to connect tousb2Mode
: Boot device using USB2 mode firmware
-
DeviceBase
(const Pipeline &pipeline, const DeviceInfo &devInfo, UsbSpeed maxUsbSpeed)¶ Connects to device specified by devInfo.
- Parameters
pipeline
: Pipeline to be executed on the devicedevInfo
: DeviceInfo which specifies which device to connect tomaxUsbSpeed
: Maximum allowed USB speed
-
DeviceBase
(const Pipeline &pipeline, const DeviceInfo &devInfo, const dai::Path &pathToCmd)¶ Connects to device specified by devInfo.
- Parameters
pipeline
: Pipeline to be executed on the devicedevInfo
: DeviceInfo which specifies which device to connect topathToCmd
: Path to custom device firmware
-
DeviceBase
()¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout. Uses OpenVINO version OpenVINO::VERSION_UNIVERSAL
-
DeviceBase
(OpenVINO::Version version)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout.
- Parameters
version
: OpenVINO version which the device will be booted with.
-
template<typename
T
, std::enable_if_t<std::is_same<T, bool>::value, bool> = true>DeviceBase
(OpenVINO::Version version, T usb2Mode)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout.
- Parameters
version
: OpenVINO version which the device will be booted withusb2Mode
: Boot device using USB2 mode firmware
-
DeviceBase
(OpenVINO::Version version, UsbSpeed maxUsbSpeed)¶ Connects to device specified by devInfo.
- Parameters
version
: OpenVINO version which the device will be booted withmaxUsbSpeed
: Maximum allowed USB speed
-
DeviceBase
(OpenVINO::Version version, const dai::Path &pathToCmd)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout.
-
DeviceBase
(OpenVINO::Version version, const DeviceInfo &devInfo)¶ Connects to device specified by devInfo.
- Parameters
version
: OpenVINO version which the device will be booted withdevInfo
: DeviceInfo which specifies which device to connect to
-
template<typename
T
, std::enable_if_t<std::is_same<T, bool>::value, bool> = true>DeviceBase
(OpenVINO::Version version, const DeviceInfo &devInfo, T usb2Mode)¶ Connects to device specified by devInfo.
- Parameters
version
: OpenVINO version which the device will be booted withdevInfo
: DeviceInfo which specifies which device to connect tousb2Mode
: Boot device using USB2 mode firmware
-
DeviceBase
(OpenVINO::Version version, const DeviceInfo &devInfo, UsbSpeed maxUsbSpeed)¶ Connects to device specified by devInfo.
- Parameters
version
: OpenVINO version which the device will be booted withdevInfo
: DeviceInfo which specifies which device to connect tomaxUsbSpeed
: Maximum allowed USB speed
-
DeviceBase
(OpenVINO::Version version, const DeviceInfo &devInfo, const dai::Path &pathToCmd)¶ Connects to device specified by devInfo.
- Parameters
version
: OpenVINO version which the device will be booted withdevInfo
: DeviceInfo which specifies which device to connect topathToCmd
: Path to custom device firmware
-
DeviceBase
(Config config)¶ Connects to any available device with custom config.
- Parameters
config
: Device custom configuration to boot with
-
DeviceBase
(Config config, const DeviceInfo &devInfo)¶ Connects to device ‘devInfo’ with custom config.
- Parameters
config
: Device custom configuration to boot withdevInfo
: DeviceInfo which specifies which device to connect to
-
DeviceBase
(const DeviceInfo &devInfo)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout. Uses OpenVINO version OpenVINO::VERSION_UNIVERSAL
- Parameters
devInfo
: DeviceInfo which specifies which device to connect to
-
DeviceBase
(const DeviceInfo &devInfo, UsbSpeed maxUsbSpeed)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout. Uses OpenVINO version OpenVINO::VERSION_UNIVERSAL
- Parameters
devInfo
: DeviceInfo which specifies which device to connect tomaxUsbSpeed
: Maximum allowed USB speed
-
DeviceBase
(std::string nameOrDeviceId)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout. Uses OpenVINO version OpenVINO::VERSION_UNIVERSAL
- Parameters
nameOrDeviceId
: Creates DeviceInfo with nameOrDeviceId to connect to
-
DeviceBase
(std::string nameOrDeviceId, UsbSpeed maxUsbSpeed)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout. Uses OpenVINO version OpenVINO::VERSION_UNIVERSAL
- Parameters
nameOrDeviceId
: Creates DeviceInfo with nameOrDeviceId to connect tomaxUsbSpeed
: Maximum allowed USB speed
-
template<typename
T
, std::enable_if_t<std::is_same<T, bool>::value, bool> = true>DeviceBase
(Config config, T usb2Mode)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout.
- Parameters
config
: Config with which the device will be booted withusb2Mode
: Boot device using USB2 mode firmware
-
DeviceBase
(Config config, UsbSpeed maxUsbSpeed)¶ Connects to device specified by devInfo.
- Parameters
config
: Config with which the device will be booted withmaxUsbSpeed
: Maximum allowed USB speed
-
DeviceBase
(Config config, const dai::Path &pathToCmd)¶ Connects to any available device with a DEFAULT_SEARCH_TIME timeout.
- Parameters
config
: Config with which the device will be booted withpathToCmd
: Path to custom device firmware
-
template<typename
T
, std::enable_if_t<std::is_same<T, bool>::value, bool> = true>DeviceBase
(Config config, const DeviceInfo &devInfo, T usb2Mode)¶ Connects to device specified by devInfo.
- Parameters
config
: Config with which the device will be booted withdevInfo
: DeviceInfo which specifies which device to connect tousb2Mode
: Boot device using USB2 mode firmware
-
DeviceBase
(Config config, const DeviceInfo &devInfo, UsbSpeed maxUsbSpeed)¶ Connects to device specified by devInfo.
- Parameters
config
: Config with which the device will be booted withdevInfo
: DeviceInfo which specifies which device to connect tomaxUsbSpeed
: Maximum allowed USB speed
-
DeviceBase
(Config config, const DeviceInfo &devInfo, const dai::Path &pathToCmd, bool dumpOnly = false)¶ Connects to device specified by devInfo.
- Parameters
config
: Config with which the device will be booted withdevInfo
: DeviceInfo which specifies which device to connect topathToCmd
: Path to custom device firmwaredumpOnly
: If true only the minimal connection is established to retrieve the crash dump
Public Static Attributes
-
constexpr std::size_t
EVENT_QUEUE_MAXIMUM_SIZE
= {2048}¶ Maximum number of elements in event queue.
Private Functions
-
bool
startPipelineImpl
(const Pipeline &pipeline) override¶ Allows the derived classes to handle custom setup for starting the pipeline
- See
- Note
Remember to call this function in the overload to setup the communication properly
- Return
True if pipeline started, false otherwise
- Parameters
pipeline
: OpenVINO version of the pipeline must match the one which the device was booted with
-
void
closeImpl
() override¶ Allows the derived classes to handle custom setup for gracefully stopping the pipeline
- Note
Remember to call this function in the overload to setup the communication properly
Private Members
-
std::unordered_map<std::string, std::shared_ptr<DataOutputQueue>>
outputQueueMap
¶
-
std::unordered_map<std::string, std::shared_ptr<DataInputQueue>>
inputQueueMap
¶
-
std::unordered_map<std::string, DataOutputQueue::CallbackId>
callbackIdMap
¶
-
std::mutex
eventMtx
¶
-
std::condition_variable
eventCv
¶
-
std::deque<std::string>
eventQueue
¶
-