ObjectTracker
ObjectTracker
How to place it
Python
Python
1pipeline = dai.Pipeline()
2objectTracker = pipeline.create(dai.node.ObjectTracker)Inputs and Outputs
Zero term tracking
Short term tracking
Supported object tracker types
SHORT_TERM_KCF: Kernelized Correlation Filter tracking. KCF utilizes properties of circulant matrix to enhance the processing speed. Paper here.SHORT_TERM_IMAGELESS: Short-term tracking allows to track objects on frames where object detection was skipped, by extrapolating object trajectory from previous detections.ZERO_TERM_COLOR_HISTOGRAM: Utilizes position, shape and input image information such as RGB histogram to perform object tracking.ZERO_TERM_IMAGELESS: Only utilizes rectangular shape of detected object and position information for object tracking. It does not use color information of tracking objects. It achieves higher throughput than ZERO_TERM_COLOR_HISTOGRAM. User needs to consider the trade-off between throughput and accuracy when choosing the object tracker type.
Maximum number of tracked objects
Usage
Python
Python
1pipeline = dai.Pipeline()
2objectTracker = pipeline.create(dai.node.ObjectTracker)
3
4objectTracker.setDetectionLabelsToTrack([15]) # Track only person
5# Possible tracking types: ZERO_TERM_COLOR_HISTOGRAM, ZERO_TERM_IMAGELESS, SHORT_TERM_IMAGELESS, SHORT_TERM_KCF
6objectTracker.setTrackerType(dai.TrackerType.ZERO_TERM_COLOR_HISTOGRAM)
7# Take the smallest ID when new object is tracked, possible options: SMALLEST_ID, UNIQUE_ID
8objectTracker.setTrackerIdAssignmentPolicy(dai.TrackerIdAssignmentPolicy.SMALLEST_ID)
9
10# You have to use Object tracker in combination with detection network
11# and an image frame source - mono/color camera or xlinkIn nodeExamples of functionality
Reference
class
depthai.node.ObjectTracker(depthai.Node)
method
setDetectionLabelsToTrack(self, labels: collections.abc.Sequence
[
typing.SupportsInt
])Specify detection labels to track. Parameter ``labels``: Detection labels to track. Default every label is tracked from image detection network output.
method
setMaxObjectsToTrack(self, maxObjectsToTrack: typing.SupportsInt)Specify maximum number of object to track. Parameter ``maxObjectsToTrack``: Maximum number of object to track. Maximum 60 in case of SHORT_TERM_KCF, otherwise 1000.
method
setOcclusionRatioThreshold(self, occlusionRatioThreshold: typing.SupportsFloat)Specify occlusion ratio threshold. Parameter ``occlusionRatioThreshold``: Occlusion ratio threshold. Used to filter out overlapping tracklets. Default 0.4.
method
setTrackerIdAssignmentPolicy(self, type: depthai.TrackerIdAssignmentPolicy)Specify tracker ID assignment policy. Parameter ``type``: Tracker ID assignment policy.
method
setTrackerThreshold(self, threshold: typing.SupportsFloat)Specify tracker threshold. Parameter ``threshold``: Above this threshold the detected objects will be tracked. Default 0, all image detections are tracked.
method
setTrackerType(self, type: depthai.TrackerType)Specify tracker type algorithm. Parameter ``type``: Tracker type.
method
setTrackingPerClass(self, trackingPerClass: bool)Whether tracker should take into consideration class label for tracking.
method
setTrackletBirthThreshold(self, threshold: typing.SupportsInt)Specify tracklet birth threshold. Parameter ``threshold``: Tracklet birth threshold. Minimum consecutive tracked frames required to consider a tracklet as a new instance. Default 3.
method
setTrackletMaxLifespan(self, lifespan: typing.SupportsInt)Specify tracklet lifespan. Parameter ``lifespan``: Tracklet lifespan in number of frames. Number of frames after which a LOST tracklet is removed. Default 120.
property
inputConfig
Input ObjectTrackerConfig message with ability to modify parameters at runtime. Default queue is non-blocking with size 4.
property
inputDetectionFrame
Input ImgFrame message on which object detection was performed. Default queue is non-blocking with size 4.
property
inputDetections
Input message with image detection from neural network. Default queue is non- blocking with size 4.
property
inputTrackerFrame
Input ImgFrame message on which tracking will be performed. RGBp, BGRp, NV12, YUV420p types are supported. Default queue is non-blocking with size 4.
property
out
Outputs Tracklets message that carries object tracking results.
property
passthroughDetectionFrame
Passthrough ImgFrame message on which object detection was performed. Suitable for when input queue is set to non-blocking behavior.
property
passthroughDetections
Passthrough image detections message from neural network output. Suitable for when input queue is set to non-blocking behavior.
property
passthroughTrackerFrame
Passthrough ImgFrame message on which tracking was performed. Suitable for when input queue is set to non-blocking behavior.
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.