DepthAI v2 has been superseded by DepthAI v3. You are viewing legacy documentation.

ON THIS PAGE

  • How to place it
  • Inputs and Outputs
  • Usage
  • Examples of functionality
  • Spatial coordinate system
  • Reference

SpatialLocationCalculator

SpatialLocationCalculator node calculates the spatial coordinates of the ROI (region-of-interest) based on the depth map from the inputDepth. It will average the depth values in the ROI and remove the ones out of range.You can also calculate spatial coordinates on host side, demo here. The demo also has the same logic that's performed on the device (calc.py file).
https://user-images.githubusercontent.com/18037362/146296930-9e7071f5-33b9-45f9-af21-cace7ffffc0f.gif

How to place it

Python

Python
1pipeline = dai.Pipeline()
2spatialCalc = pipeline.create(dai.node.SpatialLocationCalculator)

C++

C++
1dai::Pipeline pipeline;
2auto spatialCalc = pipeline.create<dai::node::SpatialLocationCalculator>();

Inputs and Outputs

Usage

Python

Python
1pipeline = dai.Pipeline()
2spatialCalc = pipeline.create(dai.node.SpatialLocationCalculator)
3spatialCalc.setWaitForConfigInput(False)
4
5# Set initial config
6config = dai.SpatialLocationCalculatorConfigData()
7config.depthThresholds.lowerThreshold = 100
8config.depthThresholds.upperThreshold = 10000
9
10topLeft = dai.Point2f(0.4, 0.4)
11bottomRight = dai.Point2f(0.6, 0.6)
12config.roi = dai.Rect(topLeft, bottomRight)
13
14spatial_calc.initialConfig.addROI(config)
15
16# You can later send configs from the host (XLinkIn) / Script node to the InputConfig

C++

C++
1dai::Pipeline pipeline;
2auto spatialCalc = pipeline.create<dai::node::SpatialLocationCalculator>();
3spatialCalc->setWaitForConfigInput(false);
4
5// Set initial config
6dai::SpatialLocationCalculatorConfigData config;
7config.depthThresholds.lowerThreshold = 100;
8config.depthThresholds.upperThreshold = 10000;
9
10dai::Point2f topLeft(0.4f, 0.4f);
11dai::Point2f bottomRight(0.6f, 0.6f);
12config.roi = dai::Rect(topLeft, bottomRight);
13
14spatialCalc->initialConfig.addROI(config);
15
16// You can later send configs from the host (XLinkIn) / scripting node to the InputConfig

Examples of functionality

Spatial coordinate system

OAK camera uses left-handed (Cartesian) coordinate system for all spatial coordinates.
Spatial coordinate system

Reference

class

depthai.node.SpatialLocationCalculator(depthai.Node)

method
getWaitForConfigInput(self) -> bool: bool
See also:     setWaitForConfigInput  Returns:     True if wait for inputConfig message, false otherwise
method
setWaitForConfigInput(self, wait: bool)
Specify whether or not wait until configuration message arrives to inputConfig Input.  Parameter ``wait``:     True to wait for configuration message, false otherwise.
property
initialConfig
Initial config to use when calculating spatial location data.
property
inputConfig
Input SpatialLocationCalculatorConfig message with ability to modify parameters in runtime. Default queue is non-blocking with size 4.
property
inputDepth
Input message with depth data used to retrieve spatial information about detected object. Default queue is non-blocking with size 4.
property
out
Outputs SpatialLocationCalculatorData message that carries spatial location results.
property
passthroughDepth
Passthrough message on which the calculation was performed. Suitable for when input queue is set to non-blocking behavior.

Need assistance?

Head over to Discussion Forum for technical support or any other questions you might have.