RGB video
Similar samples:
- RGB Preview (lower resolution)
Demo
Setup
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.pySource code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import depthai as dai
5
6# Create pipeline
7pipeline = dai.Pipeline()
8
9# Define source and output
10camRgb = pipeline.create(dai.node.ColorCamera)
11xoutVideo = pipeline.create(dai.node.XLinkOut)
12
13xoutVideo.setStreamName("video")
14
15# Properties
16camRgb.setBoardSocket(dai.CameraBoardSocket.CAM_A)
17camRgb.setResolution(dai.ColorCameraProperties.SensorResolution.THE_1080_P)
18camRgb.setVideoSize(1920, 1080)
19
20xoutVideo.input.setBlocking(False)
21xoutVideo.input.setQueueSize(1)
22
23# Linking
24camRgb.video.link(xoutVideo.input)
25
26# Connect to device and start pipeline
27with dai.Device(pipeline) as device:
28
29 video = device.getOutputQueue(name="video", maxSize=1, blocking=False)
30
31 while True:
32 videoIn = video.get()
33
34 # Get BGR frame from NV12 encoded video frame to show with opencv
35 # Visualizing the frame on slower hosts might have overhead
36 cv2.imshow("video", videoIn.getCvFrame())
37
38 if cv2.waitKey(1) == ord('q'):
39 breakPipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.