ImageManip Tiling
Frame tiling could be useful for eg. feeding large frame into a NeuralNetwork whose input size isn't as large. In such case, you can tile the large frame into multiple smaller ones and feed smaller frames to the NeuralNetwork.In this example we use 2 ImageManip for splitting the original1000x500 preview frame into two 500x500 frames.Demo

Setup
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the scriptCommand Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.pySource code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import depthai as dai
5
6# Create pipeline
7pipeline = dai.Pipeline()
8
9camRgb = pipeline.create(dai.node.ColorCamera)
10camRgb.setPreviewSize(1000, 500)
11camRgb.setInterleaved(False)
12maxFrameSize = camRgb.getPreviewHeight() * camRgb.getPreviewWidth() * 3
13
14# In this example we use 2 imageManips for splitting the original 1000x500
15# preview frame into 2 500x500 frames
16manip1 = pipeline.create(dai.node.ImageManip)
17manip1.initialConfig.setCropRect(0, 0, 0.5, 1)
18manip1.setMaxOutputFrameSize(maxFrameSize)
19camRgb.preview.link(manip1.inputImage)
20
21manip2 = pipeline.create(dai.node.ImageManip)
22manip2.initialConfig.setCropRect(0.5, 0, 1, 1)
23manip2.setMaxOutputFrameSize(maxFrameSize)
24camRgb.preview.link(manip2.inputImage)
25
26xout1 = pipeline.create(dai.node.XLinkOut)
27xout1.setStreamName('out1')
28manip1.out.link(xout1.input)
29
30xout2 = pipeline.create(dai.node.XLinkOut)
31xout2.setStreamName('out2')
32manip2.out.link(xout2.input)
33
34# Connect to device and start pipeline
35with dai.Device(pipeline) as device:
36 # Output queue will be used to get the rgb frames from the output defined above
37 q1 = device.getOutputQueue(name="out1", maxSize=4, blocking=False)
38 q2 = device.getOutputQueue(name="out2", maxSize=4, blocking=False)
39
40 while True:
41 if q1.has():
42 cv2.imshow("Tile 1", q1.get().getCvFrame())
43
44 if q2.has():
45 cv2.imshow("Tile 2", q2.get().getCvFrame())
46
47 if cv2.waitKey(1) == ord('q'):
48 breakPipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.