Script UART communication
This example uses Script node for UART communication. Note that OAK cameras don't have UART pins easily disposed, and we soldered wires on OAK-FFC-4P to expose UART pins.This should only be run on OAK-FFC-4P, as other OAK cameras might have different GPIO configuration.
Demo

Setup
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the scriptCommand Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.pySource code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2'''
3NOTE: This should only be run on OAK-FFC-4P, as other OAK cameras might have different GPIO configuration!
4'''
5import depthai as dai
6import time
7
8# Start defining a pipeline
9pipeline = dai.Pipeline()
10
11script = pipeline.create(dai.node.Script)
12script.setScript("""
13 import serial
14 import time
15
16 ser = serial.Serial("/dev/ttyS0", baudrate=115200)
17 i = 0
18 while True:
19 i += 1
20 time.sleep(0.1)
21 serString = f'TEST_{i}'
22 ser.write(serString.encode())
23""")
24# Define script for output
25script.setProcessor(dai.ProcessorType.LEON_CSS)
26
27
28config = dai.Device.Config()
29# Get argument first
30GPIO = dai.BoardConfig.GPIO
31config.board.gpio[15] = GPIO(GPIO.OUTPUT, GPIO.ALT_MODE_2)
32config.board.gpio[16] = GPIO(GPIO.INPUT, GPIO.ALT_MODE_2)
33config.board.uart[0] = dai.BoardConfig.UART()
34
35
36with dai.Device(config) as device:
37 device.startPipeline(pipeline)
38 print("Pipeline started")
39 while True:
40 time.sleep(1)Pipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.