IMU and Video Sync
This example demonstrates the use of the DepthAI Sync node to synchronize IMU (Inertial Measurement Unit) data with video frames from a color camera. It highlights the capability to process and display the latest rotation vector from the IMU alongside the video stream in real-time.Similar samples:
Demo
Command Line
1~/depthai-python/examples/Sync $ python3 imu_video_synced.py
2IMU type: BNO086, firmware version: 3.9.7
3
4Device timestamp imu: 0:00:05.379914
5Device timestamp video:0:00:05.385096
6Quaternion: i: -0.0549 j: -0.0335 k: 0.0018 real: 0.9979
7
8Device timestamp imu: 0:00:05.410274
9Device timestamp video:0:00:05.418425
10Quaternion: i: -0.0549 j: -0.0334 k: 0.0018 real: 0.9979
11
12Device timestamp imu: 0:00:05.445439
13Device timestamp video:0:00:05.451753
14Quaternion: i: -0.0548 j: -0.0334 k: 0.0018 real: 0.9979
15
16Device timestamp imu: 0:00:05.475084
17Device timestamp video:0:00:05.485082
18Quaternion: i: -0.0547 j: -0.0334 k: 0.0018 real: 0.9979
19
20Device timestamp imu: 0:00:05.510046
21Device timestamp video:0:00:05.518411
22Quaternion: i: -0.0546 j: -0.0334 k: 0.0018 real: 0.9979Setup
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the scriptCommand Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.pySource code
Python
C++
Python
PythonGitHub
1import depthai as dai
2import numpy as np
3import cv2
4from datetime import timedelta
5
6device = dai.Device()
7
8imuType = device.getConnectedIMU()
9imuFirmwareVersion = device.getIMUFirmwareVersion()
10print(f"IMU type: {imuType}, firmware version: {imuFirmwareVersion}")
11
12if imuType != "BNO086":
13 print("Rotation vector output is supported only by BNO086!")
14 exit(0)
15
16pipeline = dai.Pipeline()
17
18color = pipeline.create(dai.node.ColorCamera)
19imu = pipeline.create(dai.node.IMU)
20sync = pipeline.create(dai.node.Sync)
21xoutImu = pipeline.create(dai.node.XLinkOut)
22xoutImu.setStreamName("imu")
23
24xoutGrp = pipeline.create(dai.node.XLinkOut)
25xoutGrp.setStreamName("xout")
26
27color.setCamera("color")
28
29imu.enableIMUSensor(dai.IMUSensor.ROTATION_VECTOR, 120)
30imu.setBatchReportThreshold(1)
31imu.setMaxBatchReports(10)
32
33sync.setSyncThreshold(timedelta(milliseconds=10))
34sync.setSyncAttempts(-1)
35
36color.video.link(sync.inputs["video"])
37imu.out.link(sync.inputs["imu"])
38
39sync.out.link(xoutGrp.input)
40
41
42with device:
43 device.startPipeline(pipeline)
44 groupQueue = device.getOutputQueue("xout", 3, True)
45 while True:
46 groupMessage = groupQueue.get()
47 imuMessage = groupMessage["imu"]
48 colorMessage = groupMessage["video"]
49 print()
50 print("Device timestamp imu: " + str(imuMessage.getTimestampDevice()))
51 print("Device timestamp video:" + str(colorMessage.getTimestampDevice()))
52 latestRotationVector = imuMessage.packets[-1].rotationVector
53 imuF = "{:.4f}"
54 print(f"Quaternion: i: {imuF.format(latestRotationVector.i)} j: {imuF.format(latestRotationVector.j)} "
55 f"k: {imuF.format(latestRotationVector.k)} real: {imuF.format(latestRotationVector.real)}")
56 print()
57 cv2.imshow("video", colorMessage.getCvFrame())
58 if cv2.waitKey(1) == ord("q"):
59 breakHow it Works
- Initialize the DepthAI device.
- Check the connected IMU type and firmware version.
- Create a pipeline and add a ColorCamera and IMU node.
- Set up the Sync node to synchronize the IMU data with the video frames.
- Link the output of the ColorCamera and IMU nodes to the Sync node.
- Start the pipeline and continuously receive synchronized data.
- Display the video frames and print the IMU rotation vector data, including quaternion values.
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.