Auto Exposure on ROI
This example shows how to dynamically set the Auto Exposure (AE) of the RGB camera dynamically, during application runtime, based on bounding box position.By default, AutoExposure region is adjusted based on neural network output. If desired, the region can be set manually. You can do so by pressing one of the following buttons:w- move AE region ups- move AE region downa- move AE region leftd- move AE region rightn- deactivate manual region (switch back to nn-based roi)
Demo
Setup
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the scriptCommand Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.pySource code
Python
Python
PythonGitHub
1#!/usr/bin/env python3
2
3from pathlib import Path
4import sys
5import cv2
6import depthai as dai
7import numpy as np
8
9# Press WASD to move a manual ROI window for auto-exposure control.
10# Press N to go back to the region controlled by the NN detections.
11
12# Get argument first
13nnPath = str((Path(__file__).parent / Path('../models/mobilenet-ssd_openvino_2021.4_6shave.blob')).resolve().absolute())
14if len(sys.argv) > 1:
15 nnPath = sys.argv[1]
16
17if not Path(nnPath).exists():
18 import sys
19 raise FileNotFoundError(f'Required file/s not found, please run "{sys.executable} install_requirements.py"')
20
21previewSize = (300, 300)
22
23# Create pipeline
24pipeline = dai.Pipeline()
25
26# Define source and outputs
27camRgb = pipeline.create(dai.node.ColorCamera)
28camRgb.setPreviewSize(*previewSize)
29camRgb.setInterleaved(False)
30
31camControlIn = pipeline.create(dai.node.XLinkIn)
32camControlIn.setStreamName('camControl')
33camControlIn.out.link(camRgb.inputControl)
34
35# Define a neural network that will make predictions based on the source frames
36nn = pipeline.create(dai.node.MobileNetDetectionNetwork)
37nn.setConfidenceThreshold(0.5)
38nn.setBlobPath(nnPath)
39nn.setNumInferenceThreads(2)
40nn.input.setBlocking(False)
41camRgb.preview.link(nn.input)
42
43# Linking
44xoutRgb = pipeline.create(dai.node.XLinkOut)
45xoutRgb.setStreamName("rgb")
46camRgb.preview.link(xoutRgb.input)
47
48nnOut = pipeline.create(dai.node.XLinkOut)
49nnOut.setStreamName("nn")
50nn.out.link(nnOut.input)
51
52# MobilenetSSD label texts
53labelMap = ["background", "aeroplane", "bicycle", "bird", "boat", "bottle", "bus", "car", "cat", "chair", "cow",
54 "diningtable", "dog", "horse", "motorbike", "person", "pottedplant", "sheep", "sofa", "train", "tvmonitor"]
55
56def clamp(num, v0, v1):
57 return max(v0, min(num, v1))
58
59def asControl(roi):
60 camControl = dai.CameraControl()
61 camControl.setAutoExposureRegion(*roi)
62 return camControl
63
64class AutoExposureRegion:
65 step = 10
66 position = (0, 0)
67 size = (100, 100)
68 resolution = camRgb.getResolutionSize()
69 maxDims = previewSize[0], previewSize[1]
70
71 def grow(self, x=0, y=0):
72 self.size = (
73 clamp(x + self.size[0], 1, self.maxDims[0]),
74 clamp(y + self.size[1], 1, self.maxDims[1])
75 )
76
77 def move(self, x=0, y=0):
78 self.position = (
79 clamp(x + self.position[0], 0, self.maxDims[0]),
80 clamp(y + self.position[1], 0, self.maxDims[1])
81 )
82
83 def endPosition(self):
84 return (
85 clamp(self.position[0] + self.size[0], 0, self.maxDims[0]),
86 clamp(self.position[1] + self.size[1], 0, self.maxDims[1]),
87 )
88
89 def toRoi(self):
90 roi = np.array([*self.position, *self.size])
91 # Convert to absolute camera coordinates
92 roi = roi * self.resolution[1] // 300
93 roi[0] += (self.resolution[0] - self.resolution[1]) // 2 # x offset for device crop
94 return roi
95
96 @staticmethod
97 def bboxToRoi(bbox):
98 startX, startY = bbox[:2]
99 width, height = bbox[2] - startX, bbox[3] - startY
100 roi = frameNorm(np.empty(camRgb.getResolutionSize()), (startX, startY, width, height))
101 return roi
102
103# Connect to device and start pipeline
104with dai.Device(pipeline) as device:
105
106 # Output queues will be used to get the rgb frames and nn data from the outputs defined above
107 qControl = device.getInputQueue(name="camControl")
108 qRgb = device.getOutputQueue(name="rgb", maxSize=4, blocking=False)
109 qDet = device.getOutputQueue(name="nn", maxSize=4, blocking=False)
110 frame = None
111 detections = []
112
113 nnRegion = True
114 region = AutoExposureRegion()
115
116 # nn data (bounding box locations) are in <0..1> range - they need to be normalized with frame width/height
117 def frameNorm(frame, bbox):
118 normVals = np.full(len(bbox), frame.shape[0])
119 normVals[::2] = frame.shape[1]
120 return (np.clip(np.array(bbox), 0, 1) * normVals).astype(int)
121
122 def displayFrame(name, frame):
123 for detection in detections:
124 bbox = frameNorm(frame, (detection.xmin, detection.ymin, detection.xmax, detection.ymax))
125 cv2.rectangle(frame, (bbox[0], bbox[1]), (bbox[2], bbox[3]), (255, 0, 0), 2)
126 cv2.putText(frame, labelMap[detection.label], (bbox[0] + 10, bbox[1] + 20), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
127 cv2.putText(frame, f"{int(detection.confidence * 100)}%", (bbox[0] + 10, bbox[1] + 40), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
128 if not nnRegion:
129 cv2.rectangle(frame, region.position, region.endPosition(), (0, 255, 0), 2)
130 cv2.imshow(name, frame)
131
132 while True:
133 # Instead of get (blocking), we use tryGet (non-blocking) which will return the available data or None otherwise
134 inRgb = qRgb.tryGet()
135 inDet = qDet.tryGet()
136
137 if inRgb is not None:
138 frame = inRgb.getCvFrame()
139
140 if inDet is not None:
141 detections = inDet.detections
142
143 if nnRegion and len(detections) > 0:
144 bbox = (detections[0].xmin, detections[0].ymin, detections[0].xmax, detections[0].ymax)
145 qControl.send(asControl(AutoExposureRegion.bboxToRoi(bbox)))
146
147 if frame is not None:
148 displayFrame("rgb", frame)
149
150 key = cv2.waitKey(1)
151 if key == ord('n'):
152 print("AE ROI controlled by NN")
153 nnRegion = True
154 elif key in [ord('w'), ord('a'), ord('s'), ord('d'), ord('+'), ord('-')]:
155 nnRegion = False
156 if key == ord('a'):
157 region.move(x=-region.step)
158 if key == ord('d'):
159 region.move(x=region.step)
160 if key == ord('w'):
161 region.move(y=-region.step)
162 if key == ord('s'):
163 region.move(y=region.step)
164 if key == ord('+'):
165 region.grow(x=10, y=10)
166 region.step = region.step + 1
167 if key == ord('-'):
168 region.grow(x=-10, y=-10)
169 region.step = max(region.step - 1, 1)
170 print(f"Setting static AE ROI: {region.toRoi()} (on frame: {[*region.position, *region.endPosition()]})")
171 qControl.send(asControl(region.toRoi()))
172 elif key == ord('q'):
173 breakPipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.