Queue add callback
This example shows how to use queue callbacks. It sends both mono frames and color frames from the device to the host via oneXLinkOut
node. In the callback function newFrame()
we decode from which camera did the frame come from so we can later show the frame with correct title to the user.Demo

Setup
Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the scriptCommand Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.py
Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2import cv2
3import depthai as dai
4import queue
5
6# Create pipeline
7pipeline = dai.Pipeline()
8
9# Add all three cameras
10camRgb = pipeline.create(dai.node.ColorCamera)
11left = pipeline.create(dai.node.MonoCamera)
12right = pipeline.create(dai.node.MonoCamera)
13
14# Create XLink output
15xout = pipeline.create(dai.node.XLinkOut)
16xout.setStreamName("frames")
17
18# Properties
19camRgb.setPreviewSize(300, 300)
20left.setCamera("left")
21left.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
22right.setCamera("right")
23right.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
24
25# Stream all the camera streams through the same XLink node
26camRgb.preview.link(xout.input)
27left.out.link(xout.input)
28right.out.link(xout.input)
29
30q = queue.Queue()
31
32def newFrame(inFrame):
33 global q
34 # Get "stream name" from the instance number
35 num = inFrame.getInstanceNum()
36 name = "color" if num == 0 else "left" if num == 1 else "right"
37 frame = inFrame.getCvFrame()
38 # This is a different thread and you could use it to
39 # run image processing algorithms here
40 q.put({"name": name, "frame": frame})
41
42# Connect to device and start pipeline
43with dai.Device(pipeline) as device:
44
45 # Add callback to the output queue "frames" for all newly arrived frames (color, left, right)
46 device.getOutputQueue(name="frames", maxSize=4, blocking=False).addCallback(newFrame)
47
48 while True:
49 # You could also get the data as non-blocking (block=False)
50 data = q.get(block=True)
51 cv2.imshow(data["name"], data["frame"])
52
53 if cv2.waitKey(1) == ord('q'):
54 break
Pipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.