DepthAI v2 has been superseded by DepthAI v3. You are viewing legacy documentation.
DepthAI Tutorials
DepthAI API References

ON THIS PAGE

  • Demo
  • Setup
  • Source code
  • Pipeline

Video & MobilenetSSD

This example shows how to MobileNetv2SSD on the RGB input frame, which is read from the specified file, and not from the RGB camera, and how to display both the RGB frame and the metadata results from the MobileNetv2SSD on the frame. DepthAI is used here only as a processing unit

Similar samples:

Demo

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai-python repository first and then run the script
Command Line
1git clone https://github.com/luxonis/depthai-python.git
2cd depthai-python/examples
3python3 install_requirements.py
For additional information, please follow the installation guide.

Source code

Python

Python
GitHub
1#!/usr/bin/env python3
2
3from pathlib import Path
4import sys
5import cv2
6import depthai as dai
7import numpy as np
8from time import monotonic
9
10# Get argument first
11parentDir = Path(__file__).parent
12nnPath = str((parentDir / Path('../models/mobilenet-ssd_openvino_2021.4_8shave.blob')).resolve().absolute())
13videoPath = str((parentDir / Path('../models/construction_vest.mp4')).resolve().absolute())
14if len(sys.argv) > 2:
15    nnPath = sys.argv[1]
16    videoPath = sys.argv[2]
17
18if not Path(nnPath).exists() or not Path(videoPath).exists():
19    import sys
20    raise FileNotFoundError(f'Required file/s not found, please run "{sys.executable} install_requirements.py"')
21
22# MobilenetSSD label texts
23labelMap = ["background", "aeroplane", "bicycle", "bird", "boat", "bottle", "bus", "car", "cat", "chair", "cow",
24            "diningtable", "dog", "horse", "motorbike", "person", "pottedplant", "sheep", "sofa", "train", "tvmonitor"]
25
26# Create pipeline
27pipeline = dai.Pipeline()
28
29# Define sources and outputs
30nn = pipeline.create(dai.node.MobileNetDetectionNetwork)
31
32xinFrame = pipeline.create(dai.node.XLinkIn)
33nnOut = pipeline.create(dai.node.XLinkOut)
34
35xinFrame.setStreamName("inFrame")
36nnOut.setStreamName("nn")
37
38# Properties
39nn.setConfidenceThreshold(0.5)
40nn.setBlobPath(nnPath)
41nn.setNumInferenceThreads(2)
42nn.input.setBlocking(False)
43
44# Linking
45xinFrame.out.link(nn.input)
46nn.out.link(nnOut.input)
47
48# Connect to device and start pipeline
49with dai.Device(pipeline) as device:
50
51    # Input queue will be used to send video frames to the device.
52    qIn = device.getInputQueue(name="inFrame")
53    # Output queue will be used to get nn data from the video frames.
54    qDet = device.getOutputQueue(name="nn", maxSize=4, blocking=False)
55
56    frame = None
57    detections = []
58
59    # nn data, being the bounding box locations, are in <0..1> range - they need to be normalized with frame width/height
60    def frameNorm(frame, bbox):
61        normVals = np.full(len(bbox), frame.shape[0])
62        normVals[::2] = frame.shape[1]
63        return (np.clip(np.array(bbox), 0, 1) * normVals).astype(int)
64
65    def to_planar(arr: np.ndarray, shape: tuple) -> np.ndarray:
66        return cv2.resize(arr, shape).transpose(2, 0, 1).flatten()
67
68    def displayFrame(name, frame):
69        for detection in detections:
70            bbox = frameNorm(frame, (detection.xmin, detection.ymin, detection.xmax, detection.ymax))
71            cv2.putText(frame, labelMap[detection.label], (bbox[0] + 10, bbox[1] + 20), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
72            cv2.putText(frame, f"{int(detection.confidence * 100)}%", (bbox[0] + 10, bbox[1] + 40), cv2.FONT_HERSHEY_TRIPLEX, 0.5, 255)
73            cv2.rectangle(frame, (bbox[0], bbox[1]), (bbox[2], bbox[3]), (255, 0, 0), 2)
74        # Show the frame
75        cv2.imshow(name, frame)
76
77    cap = cv2.VideoCapture(videoPath)
78    while cap.isOpened():
79        read_correctly, frame = cap.read()
80        if not read_correctly:
81            break
82
83        img = dai.ImgFrame()
84        img.setData(to_planar(frame, (300, 300)))
85        img.setTimestamp(monotonic())
86        img.setWidth(300)
87        img.setHeight(300)
88        qIn.send(img)
89
90        inDet = qDet.tryGet()
91
92        if inDet is not None:
93            detections = inDet.detections
94
95        if frame is not None:
96            displayFrame("rgb", frame)
97
98        if cv2.waitKey(1) == ord('q'):
99            break

C++

1#include <chrono>
2#include <iostream>
3
4#include "utility.hpp"
5
6// Includes common necessary includes for development using depthai library
7#include "depthai/depthai.hpp"
8
9// MobilenetSSD label texts
10static const std::vector<std::string> labelMap = {"background", "aeroplane", "bicycle",     "bird",  "boat",        "bottle", "bus",
11                                                  "car",        "cat",       "chair",       "cow",   "diningtable", "dog",    "horse",
12                                                  "motorbike",  "person",    "pottedplant", "sheep", "sofa",        "train",  "tvmonitor"};
13
14int main(int argc, char** argv) {
15    using namespace std;
16    using namespace std::chrono;
17    // Default blob path provided by Hunter private data download
18    // Applicable for easier example usage only
19    std::string nnPath(BLOB_PATH);
20    std::string videoPath(VIDEO_PATH);
21
22    // If path to blob specified, use that
23    if(argc > 2) {
24        nnPath = std::string(argv[1]);
25        videoPath = std::string(argv[2]);
26    }
27
28    // Print which blob we are using
29    printf("Using blob at path: %s\n", nnPath.c_str());
30    printf("Using video at path: %s\n", videoPath.c_str());
31
32    // Create pipeline
33    dai::Pipeline pipeline;
34
35    // Define source and outputs
36    auto nn = pipeline.create<dai::node::MobileNetDetectionNetwork>();
37
38    auto xinFrame = pipeline.create<dai::node::XLinkIn>();
39    auto nnOut = pipeline.create<dai::node::XLinkOut>();
40
41    xinFrame->setStreamName("inFrame");
42    nnOut->setStreamName("nn");
43
44    // Properties
45    nn->setConfidenceThreshold(0.5);
46    nn->setBlobPath(nnPath);
47    nn->setNumInferenceThreads(2);
48    nn->input.setBlocking(false);
49
50    // Linking
51    xinFrame->out.link(nn->input);
52    nn->out.link(nnOut->input);
53
54    // Connect to device and start pipeline
55    dai::Device device(pipeline);
56
57    // Input queue will be used to send video frames to the device.
58    auto qIn = device.getInputQueue("inFrame");
59    // Output queue will be used to get nn data from the video frames.
60    auto qDet = device.getOutputQueue("nn", 4, false);
61
62    // Add bounding boxes and text to the frame and show it to the user
63    auto displayFrame = [](std::string name, cv::Mat frame, std::vector<dai::ImgDetection>& detections) {
64        auto color = cv::Scalar(255, 0, 0);
65        // nn data, being the bounding box locations, are in <0..1> range - they need to be normalized with frame width/height
66        for(auto& detection : detections) {
67            int x1 = detection.xmin * frame.cols;
68            int y1 = detection.ymin * frame.rows;
69            int x2 = detection.xmax * frame.cols;
70            int y2 = detection.ymax * frame.rows;
71
72            uint32_t labelIndex = detection.label;
73            std::string labelStr = to_string(labelIndex);
74            if(labelIndex < labelMap.size()) {
75                labelStr = labelMap[labelIndex];
76            }
77            cv::putText(frame, labelStr, cv::Point(x1 + 10, y1 + 20), cv::FONT_HERSHEY_TRIPLEX, 0.5, color);
78            std::stringstream confStr;
79            confStr << std::fixed << std::setprecision(2) << detection.confidence * 100;
80            cv::putText(frame, confStr.str(), cv::Point(x1 + 10, y1 + 40), cv::FONT_HERSHEY_TRIPLEX, 0.5, color);
81            cv::rectangle(frame, cv::Rect(cv::Point(x1, y1), cv::Point(x2, y2)), color, cv::FONT_HERSHEY_SIMPLEX);
82        }
83        // Show the frame
84        cv::imshow(name, frame);
85    };
86
87    cv::Mat frame;
88    cv::VideoCapture cap(videoPath);
89
90    cv::namedWindow("inFrame", cv::WINDOW_NORMAL);
91    cv::resizeWindow("inFrame", 1280, 720);
92    std::cout << "Resize video window with mouse drag!" << std::endl;
93
94    while(cap.isOpened()) {
95        // Read frame from video
96        cap >> frame;
97        if(frame.empty()) break;
98
99        auto img = std::make_shared<dai::ImgFrame>();
100        frame = resizeKeepAspectRatio(frame, cv::Size(300, 300), cv::Scalar(0));
101        toPlanar(frame, img->getData());
102        img->setTimestamp(steady_clock::now());
103        img->setWidth(300);
104        img->setHeight(300);
105        qIn->send(img);
106
107        auto inDet = qDet->get<dai::ImgDetections>();
108        auto detections = inDet->detections;
109
110        displayFrame("inFrame", frame, detections);
111
112        int key = cv::waitKey(1);
113        if(key == 'q' || key == 'Q') return 0;
114    }
115    return 0;
116}

Pipeline

Need assistance?

Head over to Discussion Forum for technical support or any other questions you might have.