Components¶
Components are part of the OakCamera class and abstract DepthAI API nodes; their initialization, configuration, and linking. This improves ease of use when developing OAK aplications.
Available components¶
Reference¶
-
class
depthai_sdk.components.
Component
SDK component is used as an abstraction to the current DepthAI API node or group of nodes.
-
on_pipeline_started
(device) This function gets called after the pipeline has been started. It is called from the main thread. It can be used to eg. initialize XlinkIn queues.
- Parameters
device (depthai.Device) –
- Return type
-