Roboflow Integration

This example showcases the usage of the ROBOFLOW platform to train a custom object detection model and use it with DepthAI SDK.

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
# Download & deploy a model from Roboflow universe:
# # https://universe.roboflow.com/david-lee-d0rhs/american-sign-language-letters/dataset/6

with OakCamera() as oak:
    color = oak.create_camera('color')
    model_config = {
        'source': 'roboflow', # Specify that we are downloading the model from Roboflow
        'model':'american-sign-language-letters/6',
        'key':'181b0f6e43d59ee5ea421cd77f6d9ea2a4b059f8' # Fake API key, replace with your own!
    }
    nn = oak.create_nn(model_config, color)
    oak.visualize(nn, fps=True)
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.