YOLO SDK

This example showcases the implementation of Yolov3 object detection network with DepthAI SDK.

For more information about tracker configuration, please refer to config tracker reference.

Note

Visualization in current example is done with blocking behavor. This means that the program will halt at oak.start() until the window is closed. This is done to keep the example simple. For more advanced usage, see Blocking behavior section.

Demo

YOLO demo

Setup

Please run the install script to download all required dependencies. Please note that this script must be ran from git context, so you have to download the depthai repository first and then run the script
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
    color = oak.create_camera('color')
    nn = oak.create_nn('yolo-v3-tf', color)
    oak.visualize([nn, color], scale=2 / 3, fps=True)  # 1080P -> 720P
    # oak.show_graph()
    oak.start(blocking=True)

Got questions?

Head over to Discussion Forum for technical support or any other questions you might have.