# Agent Tools

Luxonis is built to work with AI coding agents and assistants. Whether you use Claude Code, Cursor, Codex, or a chat window,
there's a Luxonis-aware path to get from an idea to a working OAK app.

This section covers the three ways to put an agent to work:

### Luxonis Agent Toolkit

A plugin that gives your coding agent specialist OAK skills and the Luxonis MCP server for current documentation, examples, device
information, and models.

[Install the Toolkit](https://docs.luxonis.com/software-v3/agent-tools/agent-skills.md)

### Luxonis Chat

An AI assistant that answers OAK, DepthAI, and hardware questions using the Luxonis documentation as its knowledge base.

[Open Luxonis Chat](https://support.luxonis.com)

### Agent-ready repos & docs

Our example repos and docs ship agent-oriented files (`AGENTS.md`, `llms.txt`) so any agent can navigate them without guessing.

[How agents read our docs](https://docs.luxonis.com/software-v3/agent-tools/agent-ready-repos.md)

## Which one do I use?

 * Setting up a camera or building an application? Start with the [Luxonis Agent
   Toolkit](https://docs.luxonis.com/software-v3/agent-tools/agent-skills.md). It guides the work from camera setup through a
   verified application foundation.
 * Building something on a device? Start with [Agent Skills](https://docs.luxonis.com/software-v3/agent-tools/agent-skills.md),
   they drive your camera setup and app scaffolding end to end.
 * Have a quick question? Ask [Luxonis Chat](https://support.luxonis.com) instead of searching the docs by hand.