# Concepts

Understanding the core components and terminologies is essential for effective utilization of our conversion tools. This page
introduces several key concepts that you will encounter as you navigate through the documentation.

## Conversion

Conversion is a process of converting the model format. The format dictates model storage and deployment.

## RVC Platform

Historically, Luxonis devices were released in multiple generations. We refer to them as to Robotics Vision Core (RVC) Platforms
each coming with its own set of capabilities and requirements. Find more information in the
[Hardware](https://docs.luxonis.com/hardware.md) section.

### RVC Compiled Formats

Model formats suitable for specific RVC platform:

 * RVC2 - .superblob (and .blob as legacy)
 * RVC3 - .blob
 * RVC4 - .dlc

#### SHAVEs

Streaming Hybrid Architecture Vector Engines (SHAVEs) are the hardware compute cores on the RVC2 VPU responsible for executing
neural network workloads. In DepthAI v2, models are compiled into .blob files, each built for a single, fixed number of SHAVEs. By
contrast, DepthAI v3 introduces .superblob files, which package all possible SHAVE configurations in one model file (See the
Setting Model SHAVEs section in the [Inference](https://docs.luxonis.com/software-v3/ai-inference/inference.md) section for more
information). This makes it possible to choose the desired number of SHAVEs dynamically during pipeline initialization allowing
greater flexibility, as the same model file can be reused across different SHAVE allocations without requiring recompilation.

## Quantization

Quantization is a method used to make AI models smaller, faster, and more efficient. This is achieved by reducing the precision of
the model's weights and activations.

### Why Quantization Matters

Modern AI models often use large amounts of numerical data, which by default is stored in 32-bit floating-point format (a precise
but memory-heavy way to store numbers). While this precision is helpful during training, it's often more than necessary when
running the model in real-world applications. This simplification leads to:

 * Faster execution (less data to process)
 * Reduced memory usage (smaller model size)
 * Lower power consumption
 * Minimal drop in accuracy (if done well)

### Description

For our RVC4 devices, we utilize [Qualcomm Neural Processing SDK
quantization](https://docs.qualcomm.com/bundle/publicresource/topics/80-63442-2/quantized_models.html). In brief, it works as
follows:

 1. Identify the range of input data (true-min and -max values).
 2. Determine the encoding range (encoding-min and -max values), ensuring it meets specific requirements (e.g., zero
    representation).
 3. Convert each 32-bit floating-point value to either:
    * a 16-bit floating-point value, or
    * an 8-bit fixed-point value between 0 and 255.

### Calibration Data

Data is used to determine the input range and the encoding range of the model's weights and activations during quantization. A
well-choosen calibration data allows reduction of the precision without significant loss of information. To achieve this, it must:

 * be representative of the data the model encountered during training, and
 * cover a full range of values the model is expected to handle.

It is recommended that you build out the calibration dataset from validation images. Using a larger, more diverse calibration set
should mean better general performance of the model once quantized.