# hailo

Python API: `modelconverter.platforms.hailo`

Conversion support for Hailo devices.

Holds the exporter, which compiles an ONNX or TFLite model into the Hailo `.hef` format, and the inferer, which runs a translated
`.har` model in the SDK's quantized inference context.

> **Note**
> Both are built on `hailo_sdk_client`, which exists only inside the Hailo Docker image, so neither imports on the host.

## Child Pages

 * [exporter](https://docs.luxonis.com/software-v3/ai-inference/conversion/rvc-conversion/offline/modelconverter/modelconverter-api-reference/platforms/hailo/exporter.md)
 * [inferer](https://docs.luxonis.com/software-v3/ai-inference/conversion/rvc-conversion/offline/modelconverter/modelconverter-api-reference/platforms/hailo/inferer.md)