# tool_versions

Python API: `modelconverter.utils.tool_versions`

Default conversion tool versions of the supported platforms.

Each platform is converted by a vendor toolchain that ships in its own Docker image, and several versions of it may be available.
This module holds the version used when the user does not pass `--tool-version`.

## Functions

### get_default_tool_version

```python
def get_default_tool_version(platform: Literal['rvc2', 'rvc3', 'rvc4', 'hailo']) -> str:
```

Return the default conversion tool version for a platform.

Parameters

 * `platform` (`Literal['rvc2', 'rvc3', 'rvc4', 'hailo']`): Name of the platform.

Returns

 * `str`: Version string of the toolchain used for `platform` by default.