# base_threaded_host_node

Python API: `depthai_nodes.node.base_threaded_host_node`

## Classes

### BaseThreadedHostNode

An abstract base class for threaded host nodes.

Designed to encapsulate and abstract the configuration of platform-specific attributes, providing a clean and consistent interface
for derived classes.

#### Methods

##### init

```python
def __init__(self):
```

Initialize logging and the platform-specific output image format.

Raises

 * `ValueError`: If the pipeline device platform has no configured image-frame format.

##### run

```python
def run(self):
```

Run the threaded host-node loop.

#### Attributes

##### IMG_FRAME_TYPES

### CombinedMeta

## Attributes

### ThreadedHostNodeMeta