# fastsam

Python API: `depthai_nodes.node.parsers.utils.fastsam`

## Functions

### adjust_bboxes_to_image_border

```python
def adjust_bboxes_to_image_border(boxes: np.ndarray, image_shape: tuple[int, int], threshold: int = 20) -> np.ndarray:
```

Source:
[https://github.com/ultralytics/ultralytics/blob/8094df3c474fe83d874fd83da19f704205e1eef3/ultralytics/models/fastsam/utils.py#L6](https://github.com/ultralytics/ultralytics/blob/8094df3c474fe83d874fd83da19f704205e1eef3/ultralytics/models/fastsam/utils.py#L6)
(Ultralytics) Adjust bounding boxes to stick to image border if they are within a certain threshold.

Parameters

 * `boxes` (`np.ndarray`): Bounding boxes
 * `image_shape` (`tuple[int, int]`): Image shape
 * `threshold` (`int`): Pixel threshold

Returns

 * `np.ndarray`: Adjusted bounding boxes

### bbox_iou

```python
def bbox_iou(box1: np.ndarray, boxes: np.ndarray, iou_thres: float = 0.9, image_shape: tuple[int, int] = (640, 640), raw_output: bool = False) -> np.ndarray:
```

Source:
[https://github.com/ultralytics/ultralytics/blob/8094df3c474fe83d874fd83da19f704205e1eef3/ultralytics/models/fastsam/utils.py#L30](https://github.com/ultralytics/ultralytics/blob/8094df3c474fe83d874fd83da19f704205e1eef3/ultralytics/models/fastsam/utils.py#L30)
(Ultralytics - rewritten to numpy) Compute the Intersection-Over-Union of a bounding box with respect to an array of other
bounding boxes.

Parameters

 * `box1` (`np.ndarray`): Array of shape (4, ) representing a single bounding box.
 * `boxes` (`np.ndarray`): Array of shape (n, 4) representing multiple bounding boxes.
 * `iou_thres` (`float`): IoU threshold
 * `image_shape` (`tuple[int, int]`): Image shape (height, width)
 * `raw_output` (`bool`): If True, return the raw IoU values instead of the indices

Returns

 * `np.ndarray`: Indices of boxes with IoU > thres, or the raw IoU values if raw_output is True

### box_prompt

```python
def box_prompt(masks: np.ndarray, bbox: tuple[int, int, int, int], orig_shape: tuple[int, int]) -> np.ndarray:
```

Modifies the bounding box properties and calculates IoU between masks and bounding box.

Source:
[https://github.com/ultralytics/ultralytics/blob/8094df3c474fe83d874fd83da19f704205e1eef3/ultralytics/models/fastsam/prompt.py#L284](https://github.com/ultralytics/ultralytics/blob/8094df3c474fe83d874fd83da19f704205e1eef3/ultralytics/models/fastsam/prompt.py#L284)
Modified so it uses numpy instead of torch.

Parameters

 * `masks` (`np.ndarray`): The resulting masks of the FastSAM model
 * `bbox` (`tuple[int, int, int, int]`): The prompt bounding box coordinates
 * `orig_shape` (`tuple[int, int]`): The original shape of the image

Returns

 * `np.ndarray`: The modified masks

### build_mask_coeffs

```python
def build_mask_coeffs(parsed_results: np.ndarray, masks_outputs_values: list[np.ndarray], protos_len: int) -> np.ndarray:
```

Gather mask coefficients for all detections, grouped by head.

Parameters

 * `parsed_results` (`np.ndarray`): FastSAM decoded outputs
 * `masks_outputs_values` (`list[np.ndarray]`): Model mask outputs
 * `protos_len` (`int`): Number of protos

Returns

 * `np.ndarray`

### compute_fastsam_mask

```python
def compute_fastsam_mask(outputs_values: list[np.ndarray], masks_outputs_values: list[np.ndarray], protos_output: np.ndarray, protos_len: int, *, conf_threshold: float, n_classes: int, iou_threshold: float, mask_conf: float, prompt: str, points: tuple[int, int] | None, point_label: int | None, bbox: tuple[int, int, int, int] | None) -> tuple[np.ndarray, int]:
```

Decode FastSAM outputs and apply the configured mask prompt.

Parameters

 * `outputs_values` (`list[np.ndarray]`): Detection tensors ordered by output head.
 * `masks_outputs_values` (`list[np.ndarray]`): Mask coefficient tensors ordered to match the detection heads.
 * `protos_output` (`np.ndarray`): Batched prototype tensor with shape `(1, channels, height, width)`.
 * `protos_len` (`int`): Number of prototype channels used by each mask coefficient vector.
 * `conf_threshold` (`float`): Minimum detection confidence used to filter candidates.
 * `n_classes` (`int`): Number of object classes encoded in the detection tensors.
 * `iou_threshold` (`float`): Intersection-over-union threshold for non-maximum suppression.
 * `mask_conf` (`float`): Probability threshold used to binarize mask logits.
 * `prompt` (`str`): Mask selection mode: `"everything"`, `"bbox"`, or `"point"`.
 * `points` (`tuple[int, int] | None`): Prompt point in image pixel coordinates for point selection.
 * `point_label` (`int | None`): Point-prompt label used to include or exclude matching masks.
 * `bbox` (`tuple[int, int, int, int] | None`): Bounding-box prompt in image pixel coordinates.

Returns

 * `tuple[np.ndarray, int]`: A pair of the merged instance mask and the number of selected masks. No selected masks produces a
   background mask with value -1 and count 0.

### decode_fastsam_output

```python
def decode_fastsam_output(outputs: list[np.ndarray], strides: list[int], anchors: list[np.ndarray | None], img_shape: tuple[int, int], conf_thres: float = 0.5, iou_thres: float = 0.45, num_classes: int = 1) -> np.ndarray:
```

Decode the output of the FastSAM model.

Parameters

 * `outputs` (`list[np.ndarray]`): List of FastSAM outputs
 * `strides` (`list[int]`): List of strides
 * `anchors` (`list[np.ndarray | None]`): List of anchors
 * `img_shape` (`tuple[int, int]`): Image shape
 * `conf_thres` (`float`): Confidence threshold
 * `iou_thres` (`float`): IoU threshold
 * `num_classes` (`int`): Number of classes

Returns

 * `np.ndarray`: NMS output

### format_results

```python
def format_results(bboxes: np.ndarray, masks: np.ndarray, filter: int = 0) -> list[dict[str, Any]]:
```

Formats detection results into list of annotations each containing ID, segmentation, bounding box, score and area.

Source:
[https://github.com/ultralytics/ultralytics/blob/8094df3c474fe83d874fd83da19f704205e1eef3/ultralytics/models/fastsam/prompt.py#L59](https://github.com/ultralytics/ultralytics/blob/8094df3c474fe83d874fd83da19f704205e1eef3/ultralytics/models/fastsam/prompt.py#L59)

Parameters

 * `bboxes` (`np.ndarray`): The bounding boxes of the detected objects
 * `masks` (`np.ndarray`): The masks of the detected objects
 * `filter` (`int`): The filter value

Returns

 * `list[dict[str, Any]]`: The formatted annotations

### merge_masks

```python
def merge_masks(masks: np.ndarray) -> np.ndarray:
```

Merge masks to a 2D array where each object is represented by a unique label.

Parameters

 * `masks` (`np.ndarray`): 3D array of masks

Returns

 * `np.ndarray`: 2D array of masks

### point_prompt

```python
def point_prompt(bboxes: np.ndarray, masks: np.ndarray, points: list[tuple[int, int]], pointlabel: list[int], orig_shape: tuple[int, int]) -> np.ndarray:
```

Adjusts points on detected masks based on user input and returns the modified results.

Source:
[https://github.com/ultralytics/ultralytics/blob/8094df3c474fe83d874fd83da19f704205e1eef3/ultralytics/models/fastsam/prompt.py#L317](https://github.com/ultralytics/ultralytics/blob/8094df3c474fe83d874fd83da19f704205e1eef3/ultralytics/models/fastsam/prompt.py#L317)
Modified so it uses numpy instead of torch.

Parameters

 * `bboxes` (`np.ndarray`): The bounding boxes of the detected objects
 * `masks` (`np.ndarray`): The masks of the detected objects
 * `points` (`list[tuple[int, int]]`): The points to adjust
 * `pointlabel` (`list[int]`): The point labels
 * `orig_shape` (`tuple[int, int]`): The original shape of the image

Returns

 * `np.ndarray`: The modified masks

### process_masks

```python
def process_masks(parsed_results: np.ndarray, mask_coeffs: np.ndarray, protos: np.ndarray, orig_shape: tuple[int, int], mask_conf: float) -> np.ndarray:
```

Process output into full-size masks for all detections.

Parameters

 * `parsed_results` (`np.ndarray`): FastSAM decoded outputs
 * `mask_coeffs` (`np.ndarray`): Mask coefficients
 * `protos` (`np.ndarray`): Protos from model output
 * `orig_shape` (`tuple[int, int]`): Input shape of the model
 * `mask_conf` (`float`): Mask confidence

Returns

 * `np.ndarray`