# medipipe

Python API: `depthai_nodes.node.parsers.utils.medipipe`

mediapipe.py.

Description: This script contains utility functions for decoding the output of the MediaPipe hand tracking model.

This script contains code that is based on or directly taken from a public GitHub repository:
[https://github.com/geaxgx/depthai_hand_tracker](https://github.com/geaxgx/depthai_hand_tracker)

Original code author(s): geaxgx

License: MIT License

Copyright (c) [2021] [geax]

## Classes

### HandRegion

Store a detected palm and its derived rotated region.

#### Methods

##### init

```python
def __init__(pd_score=None, pd_box=None, pd_kps=None):
```

Store palm detection values before deriving a rotated region.

Parameters

 * `pd_score`: Optional detection confidence.
 * `pd_box`: Optional normalized `[x, y, width, height]` box.
 * `pd_kps`: Optional normalized palm keypoints.

#### Attributes

##### pd_box

Normalized `[x, y, width, height]` box in the square image.

##### pd_kps

Normalized `[x, y]` palm keypoints in the square image.

##### pd_score

Palm detection confidence.

##### rect_h

Normalized rectangle height, which may exceed 1.

##### rect_h_a

Rectangle height in square-image pixels.

##### rect_points

Four rectangle corners in pixels. Coordinates refer to the square image during processing and the source image on return.

##### rect_w

Normalized rectangle width, which may exceed 1.

##### rect_w_a

Rectangle width in square-image pixels.

##### rect_x_center

Normalized rotated-rectangle center X coordinate.

##### rect_x_center_a

Rectangle center X coordinate in square-image pixels.

##### rect_y_center

Normalized rotated-rectangle center Y coordinate.

##### rect_y_center_a

Rectangle center Y coordinate in square-image pixels.

##### rotation

Rectangle rotation relative to the Y axis, in radians.

## Functions

### calculate_scale

```python
def calculate_scale(min_scale, max_scale, stride_index, num_strides):
```

Interpolate an anchor scale across feature strides.

Parameters

 * `min_scale`: Scale at the first stride.
 * `max_scale`: Scale at the last stride.
 * `stride_index`: Zero-based stride index.
 * `num_strides`: Number of strides; when one, use the midpoint scale.

Returns

 * Interpolated anchor scale.

### compute_mediapipe_palm_detections

```python
def compute_mediapipe_palm_detections(bboxes: np.ndarray, scores: np.ndarray, *, anchors: np.ndarray, conf_threshold: float, iou_threshold: float, max_det: int, scale: int, label_names: list[str] | None = None) -> tuple[np.ndarray, np.ndarray, np.ndarray, np.ndarray, list[str] | None]:
```

Decode MediaPipe palms into rotated detections and apply suppression.

Parameters

 * `bboxes` (`np.ndarray`): Per-anchor palm box and landmark predictions.
 * `scores` (`np.ndarray`): Per-anchor palm score logits.
 * `anchors` (`np.ndarray`): Precomputed anchor coordinates used to decode model predictions.
 * `conf_threshold` (`float`): Minimum detection confidence used to filter candidates.
 * `iou_threshold` (`float`): Intersection-over-union threshold for non-maximum suppression.
 * `max_det` (`int`): Maximum number of detection candidates to retain or consider during suppression.
 * `scale` (`int`): Side length of the square model input in pixels.
 * `label_names` (`list[str] | None`): Optional class-name lookup indexed by predicted class ID.

Returns

 * `tuple[np.ndarray, np.ndarray, np.ndarray, np.ndarray, list[str] | None]`: Normalized center-XY/width/height boxes, confidence
   scores, angles in degrees, zero-valued class IDs, and optional class names.

### decode

```python
def decode(bboxes, scores, anchors, threshold=0.5, scale=192):
```

Decode palm predictions and attach rotated pixel rectangles.

Parameters

 * `bboxes`: Per-anchor box and landmark offsets of shape `(N, 18)`.
 * `scores`: One score logit per anchor.
 * `anchors`: Precomputed anchors matching the model input dimensions.
 * `threshold`: Minimum sigmoid score for keeping a detection.
 * `scale`: Side length of the square model input in pixels.

Returns

 * List of `HandRegion` objects containing normalized palm geometry and pixel-space rotated rectangles.

### decode_bboxes

```python
def decode_bboxes(score_thresh, scores, bboxes, anchors, scale=128, best_only=False):
```

Decode palm boxes and seven landmarks using SSD anchors.

Parameters

 * `score_thresh`: Minimum sigmoid confidence for retaining a palm.
 * `scores`: One score logit per anchor.
 * `bboxes`: Per-anchor box and landmark offsets of shape `(N, 18)`.
 * `anchors`: Normalized center-XY/width/height anchors matching the prediction count.
 * `scale`: Model input side length used to normalize the predicted offsets.
 * `best_only`: Compatibility flag for highest-score selection; the standard decoding path uses false.

Returns

 * List of `HandRegion` objects with normalized palm boxes and keypoints. Negative-width or negative-height boxes are discarded.

Raises

 * `IndexError`: If predictions and anchors cannot be selected together. The current highest-score path also raises when a
   candidate meets the threshold.

### detections_to_rect

```python
def detections_to_rect(regions):
```

Add normalized rotated-rectangle geometry to each palm in place.

Parameters

 * `regions`: Hand regions with palm boxes and landmarks. The wrist-to-middle-finger direction determines rotation.

### generate_anchors

```python
def generate_anchors(options):
```

Generate SSD anchors using MediaPipe's anchor layout.

Based on the MediaPipe `ssd_anchors_calculator.cc` implementation.

Parameters

 * `options` (`SSDAnchorOptions`): Layer sizes, strides, scales, and aspect ratios.

Returns

 * Array of anchors in `[x_center, y_center, width, height]` format.

### generate_handtracker_anchors

```python
def generate_handtracker_anchors(input_size_width, input_size_height):
```

Generate anchors for the MediaPipe palm-detection layout.

Parameters

 * `input_size_width`: Model input width in pixels.
 * `input_size_height`: Model input height in pixels.

Returns

 * Array of normalized center-XY/width/height anchors for strides 8, 16, 16, and 16.

### normalize_radians

```python
def normalize_radians(angle):
```

Wrap an angle to the interval [-pi, pi).

Parameters

 * `angle`: Input angle in radians.

Returns

 * Equivalent angle between -pi inclusive and pi exclusive.

### rect_transformation

```python
def rect_transformation(regions, w, h, no_shift=False):
```

Convert rotated regions to pixel rectangles in place.

Parameters

 * `regions`: Regions already populated by `detections_to_rect()`.
 * `w`: Source image width in pixels.
 * `h`: Source image height in pixels.
 * `no_shift`: If false, shift toward the fingers and expand the square by 2.9; if true, keep the center and use the original
   longer side.

### rotated_rect_to_points

```python
def rotated_rect_to_points(cx, cy, w, h, rotation):
```

Convert a rotated rectangle into integer pixel corners.

Parameters

 * `cx`: Rectangle center X coordinate.
 * `cy`: Rectangle center Y coordinate.
 * `w`: Rectangle width in pixels.
 * `h`: Rectangle height in pixels.
 * `rotation`: Rotation angle in radians.

Returns

 * Four integer XY coordinate lists in perimeter order.

## Attributes

### SSDAnchorOptions