# data

Python API: `luxonis_ml.data`

Public entry point for Luxonis Data Format workflows.

The luxonis_ml.data package brings together the high-level APIs used to create, convert, load, and augment datasets in the Luxonis
Data Format (LDF). LDF is the dataset representation used across the Luxonis training stack for vision datasets with one or more
media sources, task groups, annotation types, metadata fields, local files, and remote object storage.

This module is intentionally a map of the package rather than the canonical home for every detailed contract. Details live next to
the implementation that owns them:

 * [luxonis_ml.data.datasets](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets.md)
   documents dataset lifecycle, storage layout, splits, cloning, merging, remote synchronization, and dataset plugins.
 * [luxonis_ml.ldf.annotation](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md)
   documents
   [DatasetRecord](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md),
   [Detection](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md),
   [Category](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md),
   and all annotation payload schemas.
 * [luxonis_ml.data.parsers](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/parsers.md)
   documents
   [LuxonisParser](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/parsers/luxonis_parser.md),
   the supported external formats, the directory layout each one expects, the native LDF layout, split-ratio modes, and
   parser-specific caveats.
 * [luxonis_ml.data.loaders](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders.md)
   documents
   [LuxonisLoader](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/luxonis_loader.md),
   loader outputs, label key conventions, color spaces, filtering, and preprocessing.
 * [luxonis_ml.data.augmentations](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/augmentations.md)
   documents
   [AlbumentationsEngine](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/augmentations/albumentations_engine.md),
   transform ordering, resizing, batch transforms, and custom transforms.

Table of Contents

 * [Core
   Workflow](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data.md)
 * [Tutorial
   Dataset](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data.md)
 * [Records, Tasks, and
   Labels](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data.md)
 * [Adding Records with a
   Generator](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data.md)
 * [Defining
   Splits](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data.md)
 * [Annotation
   Payloads](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data.md)
 * [Command Line
   Interface](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data.md)
 * [Extension
   Points](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data.md)

## Core Workflow

Most data pipelines follow the same sequence:

 1. Create or open a
    [LuxonisDataset](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md).
 2. Add records from an iterable or parse an external dataset with
    [LuxonisParser](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/parsers/luxonis_parser.md).
 3. Define dataset splits.
 4. Load one or more splits with
    [LuxonisLoader](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/luxonis_loader.md).
 5. Optionally apply augmentations through
    [AlbumentationsEngine](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/augmentations/albumentations_engine.md).
 6. Optionally clone, merge, export, push, pull, inspect, sanitize, or delete the dataset.

High-level APIs

| API | Use it when you need to | More detail |
| --- | --- | --- |
|
[LuxonisDataset](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md)
| Create, mutate, split, clone, merge, export, synchronize, or delete LDF datasets. |
[luxonis_ml.data.datasets](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets.md)
|
|
[LuxonisParser](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/parsers/luxonis_parser.md)
| Convert a supported external dataset layout into LDF. |
[luxonis_ml.data.parsers](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/parsers.md)
|
|
[LuxonisLoader](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/luxonis_loader.md)
| Iterate image-like inputs, labels, and sample metadata from one or more dataset splits. |
[luxonis_ml.data.loaders](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders.md)
|
|
[AlbumentationsEngine](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/augmentations/albumentations_engine.md)
| Apply runtime image and label augmentation while loading samples. |
[luxonis_ml.data.augmentations](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/augmentations.md)
|

> **Example**
> A minimal flow starts with the dataset, then constructs a loader.

```python
from luxonis_ml.data import LuxonisDataset, LuxonisLoader

dataset = LuxonisDataset("parking_lot")
loader = LuxonisLoader(dataset, view="train")

for sample in loader:
    images = sample.images
    labels = sample.labels
    metadata = sample.metadata
```

> **Note**
> Importing from luxonis_ml.data is the recommended public API for common workflows. Import from lower modules when you need implementation-specific models such as annotation schemas, parser classes, or loader base classes.

## Tutorial Dataset

Most examples in the data package use a small `parking_lot` dataset with cars and motorcycles. It contains object-detection boxes,
instance keypoints, semantic segmentation masks for color/type/brand/binary vehicle classes, and metadata suitable for trying the
full LDF workflow.

The dataset can be used to exercise task naming conventions:

 * keypoint annotations for classes with different skeletons should be separated into task groups such as
   `"instance_keypoints_car"` and `"instance_keypoints_motorbike"`;
 * semantic segmentation is usually placed in its own task group, such as `"segmentation"`, because loaders add a background class
   for segmentation tasks.

Hands-on notebooks and scripts for preparing and interacting with LuxonisML datasets are maintained in the Luxonis AI tutorials
repository: `https://github.com/luxonis/ai-tutorials/tree/main/training`.

The original `parking_lot` sample archive used by these examples is available at
`https://drive.google.com/uc?export=download&id=1OAuLlL_4wRSzZ33BuxM6Uw2QYYgv_19N`.

## Records, Tasks, and Labels

Dataset ingestion is record-based. A record points to one file or to multiple synchronized files, optionally assigns a task name,
and optionally provides an annotation payload.

> **Example**
> The two supported media-key styles are easy to distinguish.

```pycon
>>> single_source = {"file": "image.jpg", "annotation": None}
>>> multi_source = {"files": {"rgb": "rgb.png", "depth": "depth.png"}}
>>> "file" in single_source, "files" in multi_source
(True, True)
```

Task names group annotations that should be consumed together by a model or loader. Loader label keys use `"task_name/task_type"`.
If no task name is provided, the task name is the empty string and keys start with `"/"`.

> **Example**
> ```pycon
>>> task_name = "detection"
>>> task_type = "boundingbox"
>>> f"{task_name}/{task_type}"
'detection/boundingbox'
>>> f"{''}/segmentation"
'/segmentation'
```

> **See Also**
> [luxonis_ml.ldf.annotation](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md) for the exact record model, annotation payload schemas, normalized coordinate conventions, metadata categories, and instance-association rules.

## Adding Records with a Generator

[LuxonisDataset.add](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md) takes an iterator of records. A generator function is the usual choice, because you do not build the full list of records in memory.

The generator below reads one annotation file for each directory. It yields the bounding box and the keypoints of one object under a shared `instance_id`. It yields each segmentation mask under a separate task name.

```python
import json
from pathlib import Path

import cv2
import numpy as np

from luxonis_ml.data import LuxonisDataset

dataset_root = Path("data/parking_lot")

def generator():
    for annotation_file in dataset_root.rglob("annotations.json"):
        data = json.loads(annotation_file.read_text())
        width = data["dimensions"]["width"]
        height = data["dimensions"]["height"]
        image = str(annotation_file.parent / data["filename"])

        for instance_id, box in data["BoundingBoxAnnotation"].items():
            x, y = box["origin"]
            w, h = box["dimension"]
            yield {
                "file": image,
                "task_name": f"instance_keypoints_{box['labelName']}",
                "annotation": {
                    "class": box["labelName"],
                    "instance_id": int(instance_id),
                    "boundingbox": {
                        "x": x / width,
                        "y": y / height,
                        "w": w / width,
                        "h": h / height,
                    },
                },
            }

        for instance_id, pose in data["KeypointsAnnotation"].items():
            yield {
                "file": image,
                "task_name": f"instance_keypoints_{pose['labelName']}",
                "annotation": {
                    "instance_id": int(instance_id),
                    "keypoints": {
                        "keypoints": [
                            (
                                keypoint["location"][0] / width,
                                keypoint["location"][1] / height,
                                keypoint["visibility"],
                            )
                            for keypoint in pose["keypoints"]
                        ]
                    },
                },
            }

        masks = data["VehicleTypeSegmentation"]
        mask_path = annotation_file.parent / masks["filename"]
        mask = cv2.cvtColor(cv2.imread(str(mask_path)), cv2.COLOR_BGR2RGB)

        for instance in masks["instances"]:
            color = np.array(instance["pixelValue"], dtype=np.uint8)
            yield {
                "file": image,
                "task_name": "segmentation",
                "annotation": {
                    "class": instance["labelName"],
                    "segmentation": {
                        "mask": (mask == color)
                        .all(axis=-1)
                        .astype(np.uint8)
                    },
                },
            }

dataset = LuxonisDataset("parking_lot")
dataset.add(generator())
```

> **Note**
> The shared `instance_id` links the box and the keypoints of one object. Give the keypoints of each class a separate task name, because the loader stacks the keypoints of one task into a single array.

## Defining Splits

[LuxonisDataset.make_splits](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md) assigns the records to named splits. Pass the ratios of the splits, or pass the exact files of each split.

```python
dataset.make_splits({"train": 0.7, "val": 0.2, "test": 0.1})

dataset.make_splits(
    {
        "train": ["image_1.jpg", "image_2.jpg"],
        "val": ["image_3.jpg"],
        "test": ["image_4.jpg"],
    }
)
```

A call with no argument splits 80/10/10. A ratio is a number from 0 to 1, and the ratios must sum to 1.

A split from ratios uses only the records that no split holds yet. A second call with ratios thus needs new records, or it raises an error. A call with explicit file lists adds only the files that no split holds yet. If no named file is new, the call logs a warning and keeps the old splits. Thus you can parse the same data twice.

Pass `replace_old_splits=True` to drop the old splits. A later call with ratios then splits every record again. A later call with file lists splits only the files that you name.

## Annotation Payloads

LDF supports a small set of annotation payload families:

 * classification through a `"class"` value;
 * normalized `xywh` bounding boxes through `"boundingbox"`;
 * normalized `(x, y, visibility)` keypoint triplets through `"keypoints"`;
 * semantic segmentation masks through polygon points, binary masks, or COCO RLE values under `"segmentation"`;
 * instance segmentation masks through the same mask encodings under `"instance_segmentation"`;
 * arbitrary `.npy` array targets through `"array"`;
 * flexible metadata values through `"metadata"`.

Any annotation with a class contributes a classification target. When separate records describe the same physical object, use the same `instance_id` so boxes, keypoints, and instance masks can be associated reliably.

> **See Also**
> [luxonis_ml.ldf.annotation](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md) for examples, exact field names, mask encoding details, metadata categories, and loader output shapes.

## Command Line Interface

The data package also provides dataset operations through `luxonis_ml data`. The CLI mirrors the Python APIs for parsing, listing, inspecting, validating, sanitizing, exporting, synchronizing, cloning, merging, and deleting datasets.

```bash
luxonis_ml data --help
luxonis_ml data parse --help
luxonis_ml data parse <data_directory>
luxonis_ml data ls
luxonis_ml data info <dataset_name>
luxonis_ml data inspect <dataset_name>
luxonis_ml data health <dataset_name>
luxonis_ml data sanitize <dataset_name>
luxonis_ml data export <dataset_name> --type native
luxonis_ml data export <dataset_name> --type coco
luxonis_ml data export <dataset_name> --type ultralyticsndjson
luxonis_ml data push <dataset_name>
luxonis_ml data pull <dataset_name>
luxonis_ml data clone <dataset_name> <new_name>
luxonis_ml data merge <source_name> <target_name>
luxonis_ml data delete <dataset_name>
```

> **See Also**
> [luxonis_ml.data.main](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/__main__.md) for command implementation details, and [luxonis_ml.data.parsers](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/parsers.md) for the directory layout of every supported format, including the native LDF layout that `--type native` writes.

## Extension Points

Datasets and loaders are registry-backed. Third-party packages can expose entry points in the `dataset_plugins` and `loader_plugins` groups. This module loads those plugins at import time and registers them in [DATASETS_REGISTRY](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/base_dataset.md) and [LOADERS_REGISTRY](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/base_loader.md).

> **See Also**
> [BaseDataset](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/base_dataset.md), [BaseLoader](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/base_loader.md), [DatasetIterator](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/base_dataset.md), [DATASETS_REGISTRY](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/base_dataset.md), and [LOADERS_REGISTRY](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/base_loader.md).

## Child Pages

 * [augmentations](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/augmentations.md)
 * [datasets](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets.md)
 * [exporters](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/exporters.md)
 * [loaders](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders.md)
 * [parsers](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/parsers.md)
 * [utils](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/utils.md)
 * [Data CLI](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/__main__.md)