# datasets

Python API: `luxonis_ml.data.datasets`

Dataset handles, records, metadata, and storage abstractions for LDF.

This package owns the persistent Luxonis Data Format (LDF) dataset contract. The primary entry point is
[LuxonisDataset](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md),
which creates or opens a dataset and provides methods for adding records, defining splits, setting class order and keypoint
skeletons, merging or cloning datasets, exporting datasets, and synchronizing remote media.

The exact annotation payload schemas live in
[luxonis_ml.ldf.annotation](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md).
This package-level documentation focuses on dataset lifecycle and storage.

Table of Contents

 * [Dataset
   Lifecycle](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets.md)
 * [Creation and Append
   Modes](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets.md)
 * [Dataset
   Records](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets.md)
 * [Storage
   Layout](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets.md)
 * [Cloning, Merging, and
   Synchronization](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets.md)
 * [Class
   Ordering](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets.md)

## Dataset Lifecycle

A dataset is identified by `dataset_name` and optional storage settings. Constructing
[LuxonisDataset](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md)
opens an existing dataset when one is present, or initializes a new one when no matching dataset exists.

```python
from luxonis_ml.data import BucketStorage, LuxonisDataset

dataset = LuxonisDataset(
    "parking_lot",
    bucket_storage=BucketStorage.LOCAL,
)
```

Typical mutation flow:

 1. Yield
    [DatasetRecord](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md)-compatible
    dictionaries from a generator.
 2. Pass the generator to
    [LuxonisDataset.add](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md).
 3. Call
    [LuxonisDataset.make_splits](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md)
    to define split membership.
 4. Optionally clone, merge, export, push, pull, inspect, sanitize, or delete through
    [LuxonisDataset](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md)
    methods or the CLI.

```python
def records():
    yield {
        "file": "path/to/image.jpg",
        "task_name": "detection",
        "annotation": {
            "class": "car",
            "boundingbox": {
                "x": 0.1,
                "y": 0.2,
                "w": 0.3,
                "h": 0.4,
            },
        },
    }

dataset.add(records())
dataset.make_splits({"train": 0.8, "val": 0.1, "test": 0.1})
```

> **Note**
> Although `"train"`, `"val"`, and `"test"` are conventional split names, [LuxonisDataset.make_splits](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md) accepts arbitrary split names when a project needs custom views.

## Creation and Append Modes

[LuxonisDataset](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md)
creates local datasets by default. Pass `bucket_storage=BucketStorage.GCS`, `BucketStorage.S3`, or another supported storage
backend to create a remote-backed dataset. Remote datasets keep the same local metadata structure as local datasets, while media
files are synchronized with object storage.

Opening an existing dataset with the same name reuses it. To force a clean local dataset, pass `delete_local=True`. To force a
clean remote dataset, delete both sides with `delete_local=True` and `delete_remote=True` before adding records.

```python
dataset = LuxonisDataset(
    "parking_lot",
    bucket_storage=BucketStorage.LOCAL,
    delete_local=True,
)
dataset.add(records(), batch_size=100_000_000)
dataset.make_splits((0.8, 0.1, 0.1))
```

To append new data, open the dataset with `delete_local=False` and call
[LuxonisDataset.add](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md)
again. New annotation records are appended, while records for media with the same informational UUID replace previous annotations
for that media item.

The
[LuxonisDataset.add](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md)
`batch_size` controls how many annotation records are buffered before writing a Parquet shard. For remote datasets, the same batch
boundary also controls when media and annotation shards are pushed to cloud storage.

## Dataset Records

[LuxonisDataset.add](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md)
takes an iterator of
[DatasetRecord](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md)-compatible
items. A record may use `"file"` for a single source or `"files"` for multiple synchronized sources.

Record-level fields

| Field | Meaning |
| --- | --- |
| `file` | Path to a single media source. |
| `files` | Mapping from source names to synchronized media paths. |
| `task_name` | Optional group name used by loaders and metadata. |
| `sample_metadata` | Optional record-level metadata preserved with the sample and returned by
[LuxonisLoader](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/luxonis_loader.md)
as
[LoaderOutput.metadata](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/typing.md).
|
| `annotation` | Optional annotation payload validated by
[Detection](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md).
|

Multi-source records preserve source names for
[LuxonisLoader](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/luxonis_loader.md),
allowing training code to receive dictionaries such as `{"rgb": ..., "depth": ...}`. Record-level metadata is separate from
annotation metadata: `sample_metadata` describes the sample, while `annotation["metadata"]` creates metadata label tasks.

```json
{
  "file": "images/frame_001.jpg",
  "task_name": "detection",

  "sample_metadata": {
    "record_id": 123,
    "camera": "left",
    "tags": ["night", "warehouse"]
  },

  "annotation": {
    "class": "person",
    "boundingbox": {
      "x": 0.1,
      "y": 0.2,
      "w": 0.3,
      "h": 0.4
    }
  }
}
```

Frontend note: `sample_metadata` is sample data, not an annotation target.

> **See Also**
> [DatasetRecord](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md) for record validation, [Detection](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md) for payload grouping, and [luxonis_ml.ldf.annotation](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md) for detailed annotation schemas.

## Storage Layout

By default, local datasets live under `LUXONISML_BASE_PATH / data / LUXONISML_TEAM_ID / datasets / dataset_name`. The default base
path is `Path.home() / "luxonis_ml"` and the default team identifier is `"offline"`.

Dataset storage layout

| Path | Contents |
| --- | --- |
| `annotations/*.parquet` | Parquet shards containing media paths, source names, task names, class names, instance IDs, task
types, serialized annotation payloads, serialized `sample_metadata` JSON, and UUIDs. |
| `media/` | Local copies of remote media, named `<uuid><suffix>`. Local-only datasets may keep this directory empty and continue
referencing the original files. |
| `metadata/metadata.json` | Dataset metadata, source descriptors, class mappings, task metadata, categorical encodings, skeleton
definitions, and LDF version metadata. |
| `metadata/splits.json` | Mapping from split names to dataset sample identifiers. |

Remote datasets use the same local metadata structure and synchronize media and annotation state with the configured object store.
In the bucket, the dataset lives at `<bucket_storage>://<bucket>/<team_id>/datasets/<dataset_name>/` and keeps the same
`annotations/`, `media/`, and `metadata/` subfolders. Array annotations add a fourth `arrays/` subfolder.

A remote dataset renames its media objects. Each file becomes `<uuid><original suffix>`, where the UUID comes from the content of
the file. The original file names stay in the `file` column of the Parquet shards.

> **Warning**
> Deletion flags control local and remote state independently. To recreate a remote dataset completely, pass `delete_local=True` and `delete_remote=True`. To rebuild a damaged local copy from an existing remote dataset, pass `delete_local=True` and `delete_remote=False`.

> **Warning**
> The local path holds no bucket-storage component. A local dataset and a remote dataset with the same name therefore share one local directory. Use distinct names, or expect the two to overwrite each other's local state.

## Cloning, Merging, and Synchronization

[LuxonisDataset.clone](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md)
creates a copy under a new dataset name.
[LuxonisDataset.merge_with](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md)
combines two datasets either in place or into a new dataset.

```python
clone = dataset.clone(new_dataset_name="parking_lot_clone")

dataset1.merge_with(dataset2, inplace=True)

merged = dataset1.merge_with(
    dataset2,
    inplace=False,
    new_dataset_name="parking_lot_merged",
)
```

Remote synchronization is explicit and controlled by
[UpdateMode](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/utils/enums.md):

```python
from luxonis_ml.data import BucketStorage, UpdateMode

dataset.pull_from_cloud(update_mode=UpdateMode.MISSING)
dataset.push_to_cloud(
    bucket_storage=BucketStorage.GCS,
    update_mode=UpdateMode.ALL,
)
```

> **Important**
> Annotation shards and metadata are always synchronized. Media update mode controls whether all media files or only missing media files are transferred.

## Class Ordering

[LuxonisDataset.set_class_order_per_task](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md)
applies a view-time class order per task without rewriting stored metadata. The provided mapping must use exact task names and
exact class names already present in the dataset.

```python
dataset.set_class_order_per_task(
    {
        "vehicle_detection": ["car", "motorcycle"],
        "color_segmentation": ["background", "red", "green", "blue"],
    }
)
```

Call this before constructing
[LuxonisLoader](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/luxonis_loader.md),
because loader initialization uses the dataset's active class ordering. If later additions introduce new classes, call
[set_class_order_per_task](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md)
again with the complete desired order.

## Child Pages

 * [annotation](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/annotation.md)
 * [base_dataset](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/base_dataset.md)
 * [luxonis_dataset](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/luxonis_dataset.md)
 * [metadata](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/metadata.md)
 * [migration](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/migration.md)
 * [source](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/source.md)
 * [utils](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/datasets/utils.md)