# base_exporter

Python API: `luxonis_ml.data.exporters.base_exporter`

## Classes

| Name | Description |
| --- | --- |
|
[`BaseExporter`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/exporters/base_exporter.md)
| Base class for dataset exporters. |

### class `BaseExporter`

```python
class BaseExporter(ABC)
```

Base class for dataset exporters.

Attributes

| Name | Type | Description |
| --- | --- | --- |
| `current_size` | `int` | Current partition size in bytes. |
| `dataset_identifier` |  | Name or identifier used for exported paths. |
| `image_indices` | `dict` | Per-image export indices used by concrete exporters. |
| `max_partition_size` |  | Optional maximum partition size in bytes. |
| `max_partition_size_gb` |  | Optional maximum partition size in GiB. |
| `output_path` |  | Directory where the export is written. |
| `part` |  | Current partition index, or `None` when partitioning is disabled. |

Methods

| Name | Description |
| --- | --- |
|
[`__init__`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/exporters/base_exporter.md)
| |
|
[`export`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/exporters/base_exporter.md)
| Convert the prepared dataset into the exporter's format. |
|
[`supported_ann_types`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/exporters/base_exporter.md)
| Return task types supported by this exporter. |

#### method `__init__`

```python
def __init__(
    dataset_identifier: str,
    output_path: Path,
    max_partition_size_gb: float | None,
)
```

#### method `export`

```python
def export(prepared_ldf: PreparedLDF)
```

Convert the prepared dataset into the exporter's format.

Args

| Name | Type | Description | Default |
| --- | --- | --- | --- |
| `prepared_ldf` | `PreparedLDF` | Dataset data prepared for export. | required |

Raises

| Type | Description |
| --- | --- |
| `NotImplementedError` | Always raised by the abstract base implementation. |

#### method `supported_ann_types`

```python
def supported_ann_types() -> list[str]
```

Return task types supported by this exporter.

Returns

| Type | Description |
| --- | --- |
| `list[str]` | Supported annotation task types. |

Raises

| Type | Description |
| --- | --- |
| `NotImplementedError` | Always raised by the abstract base implementation. |