# loaders

Python API: `luxonis_ml.data.loaders`

Dataset loaders for LDF samples.

This package owns runtime sample access.
[LuxonisLoader](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/luxonis_loader.md)
reads one or more dataset splits, resolves media paths, assembles labels by task key, optionally applies augmentations, and
returns data in a shape suitable for training pipelines.

Table of Contents

 * [Basic
   Usage](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders.md)
 * [Constructor
   Options](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders.md)
 * [Label
   Keys](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders.md)
 * [Output
   Layouts](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders.md)
 * [Sample
   Metadata](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders.md)
 * [Runtime
   Options](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders.md)

## Basic Usage

```python
from luxonis_ml.data import LuxonisDataset, LuxonisLoader

dataset = LuxonisDataset("parking_lot")
loader = LuxonisLoader(dataset, view="train")

sample = loader[0]

images = sample.images
labels = sample.labels
metadata = sample.metadata
```

[LuxonisLoader](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/luxonis_loader.md)
implements indexed access and iteration. The returned value is always
[LoaderOutput](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/typing.md).

[LoaderOutput.images](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/typing.md)
maps source names to arrays. Single-source datasets use the conventional `"image"` source name; multi-source datasets preserve the
names from the record `"files"` mapping.

[LoaderOutput.metadata](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/typing.md)
contains record-level metadata from `DatasetRecord.sample_metadata`. By default it also includes a `"filenames"` mapping from
source name to the loaded file basename.

Legacy two-value unpacking still works when code only needs inputs and labels:

```python
image_or_images, labels = loader[0]
```

Metadata is not yielded by tuple unpacking. Access it through `loader[0].metadata`.

## Constructor Options

[LuxonisLoader](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/luxonis_loader.md)
is configured at runtime and does not mutate stored dataset state. Common options include:

 * `view` to load one split or a list of splits.
 * `augmentation_engine` and `augmentation_config` to enable augmentations.
 * `height`, `width`, and `keep_aspect_ratio` to define the resize behavior expected by the augmentation engine.
 * `color_space` to request `"RGB"`, `"BGR"`, or `"GRAY"` output globally or per source name.
 * `seed` for reproducible random augmentations.
 * `exclude_empty_annotations` to omit empty labels.
 * `keep_categorical_as_strings` to preserve categorical metadata values.
 * `update_mode` to control media synchronization for remote datasets.
 * `filter_task_names` to load only selected task groups.
 * `autopopulate_metadata` to include automatic metadata such as source filenames in
   [LoaderOutput.metadata](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/typing.md).

When a remote dataset is loaded, annotations and metadata are refreshed. Media files are downloaded according to
[UpdateMode](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/utils/enums.md):
`ALL` overwrites local media and `MISSING` downloads only media that cannot be resolved locally.

## Label Keys

The `labels` dictionary is keyed by `"task_name/task_type"`. If a dataset was created without a task name, the default task name
is the empty string and keys start with `"/"`.

> **Example**
> ```pycon
>>> task_name = "detection"
>>> task_type = "boundingbox"
>>> f"{task_name}/{task_type}"
'detection/boundingbox'
>>> f"{''}/metadata/camera_angle"
'/metadata/camera_angle'
```

Metadata labels use `"task_name/metadata/key"` so each metadata field can be consumed independently.

Sample metadata does not use label keys. It is returned separately through [LoaderOutput.metadata](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/typing.md):

```python
sample = loader[0]
print(sample.metadata)

# {
#     "filenames": {"image": "frame_001.jpg"},
#     "record_id": 123,
#     "camera": "left",
# }
```

## Output Layouts

Common label layouts

| Task type | Shape or structure | Meaning |
| --- | --- | --- |
| `classification` | (C) | One-hot class vector. |
| `boundingbox` | (N, 5) | Rows are [c, x, y, w, h]. |
| `segmentation` | (C, H, W) | One-hot semantic mask in channel-first layout. |
| `instance_segmentation` | (N, H, W) | One binary mask per instance. |
| `keypoints` | (N, 3K) | Flattened (x, y, v) keypoint triplets. |
| `metadata` | Original value structure. | Values keyed by metadata field name. |

> **See Also**
> [luxonis_ml.ldf.annotation](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/ldf/annotation.md) for the ingestion schemas that are converted into these loader outputs.

## Sample Metadata

Record-level metadata comes from `DatasetRecord.sample_metadata` and is available as [LoaderOutput.metadata](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/typing.md).

```python
sample = loader[0]

sample.metadata
# {
#     "filenames": {"image": "frame_001.jpg"},
#     "record_id": 123,
#     "camera": "left",
# }
```

Pass `autopopulate_metadata=False` to return only stored metadata:

```python
loader = LuxonisLoader(dataset, autopopulate_metadata=False)
metadata = loader[0].metadata
```

Augmented outputs additionally carry an `"augmentations"` mapping from configured augmentation paths to the runtime parameters the engine selected. Unlike `"filenames"`, it is added regardless of `autopopulate_metadata`, as it describes the returned arrays rather than the dataset record:

```python
{
    "record_id": 123,
    "augmentations": {
        "HorizontalFlip": {},
        "OneOf/RandomBrightnessContrast": {"alpha": 1.02, "beta": -0.03},
    },
}
```

Both keys are reserved. A record defining one of them keeps its own value, and the loader warns rather than overwriting it.

When a batch augmentation combines several samples, metadata from the input samples is preserved in `"batch_augmentation_metadata"`:

```python
{
    "record_id": 123,

    "batch_augmentation_metadata": [
        {
            "input_index": 0,
            "sample_metadata": {"record_id": 123},
        },
        {
            "input_index": 1,
            "sample_metadata": {"record_id": 456},
        },
    ],
}
```

Annotation metadata is different: values under `annotation["metadata"]` are converted into label tasks such as `"detection/metadata/weather"`.

## Runtime Options

[LuxonisLoader](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/luxonis_loader.md) owns runtime concerns that are intentionally separate from dataset storage:

 * selected views through `view`;
 * color-space conversion through `color_space`;
 * optional resizing through `height` and `width`;
 * aspect-ratio preservation through `keep_aspect_ratio`;
 * augmentation engine construction through `augmentation_engine` and `augmentation_config`;
 * remote media synchronization through `update_mode`;
 * empty-annotation filtering through `exclude_empty_annotations`;
 * metadata category encoding through `keep_categorical_as_strings`;
 * task filtering through `filter_task_names`.

```python
loader = LuxonisLoader(
    dataset,
    view=["train", "val"],
    height=640,
    width=640,
    keep_aspect_ratio=True,
    color_space="RGB",
    filter_task_names=["detection"],
    exclude_empty_annotations=True,
)
```

> **Important**
> Augmentations require output `height` and `width` so the loader can construct a deterministic resizing stage.

> **See Also**
> [luxonis_ml.data.augmentations](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/augmentations.md) for augmentation configuration and target conversion details.

## Child Pages

 * [base_loader](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/base_loader.md)
 * [luxonis_loader](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/data/loaders/luxonis_loader.md)