# cyclopts

Python API: `luxonis_ml.telemetry.cli.cyclopts`

## Functions

| Name | Description |
| --- | --- |
|
[`instrument_cyclopts`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/cli/cyclopts.md)
| Wrap Cyclopts commands to emit telemetry events. |

### function `instrument_cyclopts`

```python
def instrument_cyclopts(
    app: cyclopts.App,
    telemetry: Telemetry,
    *,
    allowlist: set[str] | None = None,
    include_system_metadata: bool | None = None,
    exclude_commands: set[str] | None = None,
)
```

Wrap Cyclopts commands to emit telemetry events.

The wrapper walks the app recursively, so it also instruments the commands of every sub-app. Aliases share one app object, so the
wrapper instruments each sub-app once.

> **Note**
> The wrapper skips the generated help and version callbacks. Use [luxonis_ml.telemetry.cli.skip_telemetry](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/cli/cyclopts.md) on a single callback to exclude that command as well.

Args

| Name | Type | Description | Default |
| --- | --- | --- | --- |
| `app` | `cyclopts.App` | The Cyclopts application to instrument. | required |
| `telemetry` | `Telemetry` | The telemetry client that captures the events. | required |
| `allowlist` | `set[str] | None` | Names of the command arguments you allow in the event. One allowlist covers every instrumented
command. If omitted, no argument value is sent. The wrapper always drops `self`, `ctx`, and `context`, and it drops any Click or
Typer context object. | `None` |
| `include_system_metadata` | `bool | None` | Whether to attach system metadata to the events. If omitted, the telemetry
configuration decides. | `None` |
| `exclude_commands` | `set[str] | None` | Full command names to leave uninstrumented, such as `{"data parse"}`. Nested names use
a space between the parts. | `None` |