# context

Python API: `luxonis_ml.telemetry.context`

## Functions

| Name | Description |
| --- | --- |
|
[`base_context`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/context.md)
| Create base context for all events. |
|
[`host_context`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/context.md)
| Return coarse host metadata for optional event context. |
|
[`host_context_provider`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/context.md)
| Context provider that exposes coarse host metadata. |
|
[`is_ci`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/context.md)
| Best-effort detection of CI environments. |
|
[`is_luxonis_cloud`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/context.md)
| Return True when telemetry runs inside the Luxonis cloud. |
|
[`normalized_processor`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/context.md)
| Return a coarse processor family for telemetry. |
|
[`system_context`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/context.md)
| Return extended runtime metadata for optional event context. |
|
[`system_context_provider`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/context.md)
| Context provider that exposes extended runtime metadata. |

### function `base_context`

```python
def base_context(
    *,
    library_name: str,
    library_version: str | None,
    session_id: str,
    source_component: str | None,
) -> dict[str, Any]
```

Create base context for all events.

> **Note**
> `$process_person_profile` is False on purpose. It keeps the PostHog captures anonymous, so PostHog creates no person profile. Do not change it to True.

Args

| Name | Type | Description | Default |
| --- | --- | --- | --- |
| `library_name` | `str` | Name of the emitting library. | required |
| `library_version` | `str | None` | Version string for the library. | required |
| `session_id` | `str` | Random session ID. It stays the same for the lifetime of one
[luxonis_ml.telemetry.Telemetry](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/client.md)
instance, not for the lifetime of the process. The PostHog backend also uses it as the default `distinct_id`. | required |
| `source_component` | `str | None` | Optional component name for the emitter. If omitted, the library name is reused. | required
|

Returns

| Type | Description |
| --- | --- |
| `dict[str, Any]` | The shared base context attached to events. It holds `$process_person_profile`, `$session_id`,
`source_product`, `source_component`, and `sdk_version`. |

### function `host_context`

```python
def host_context() -> dict[str, Any]
```

Return coarse host metadata for optional event context.

Returns

| Type | Description |
| --- | --- |
| `dict[str, Any]` | A mapping of `os`, `os_version`, `arch`, and `python_version`. |

### function `host_context_provider`

```python
def host_context_provider(_telemetry: object) -> dict[str, Any]
```

Context provider that exposes coarse host metadata.

### function `is_ci`

```python
def is_ci() -> bool
```

Best-effort detection of CI environments.

### function `is_luxonis_cloud`

```python
def is_luxonis_cloud() -> bool
```

Return True when telemetry runs inside the Luxonis cloud.

### function `normalized_processor`

```python
def normalized_processor() -> str
```

Return a coarse processor family for telemetry.

The raw `platform.processor` string never leaves the machine.
[host_context](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/context.md)
still sends the `platform.machine` value as `arch`.

Returns

| Type | Description |
| --- | --- |
| `str` | One of `"arm64"`, `"arm"`, `"x86_64"`, `"x86"`, `"powerpc"`, `"riscv"`, or `"unknown"`. |

### function `system_context`

```python
def system_context() -> dict[str, Any]
```

Return extended runtime metadata for optional event context.

Returns

| Type | Description |
| --- | --- |
| `dict[str, Any]` | The keys of
[host_context](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/context.md),
plus `ci`, `is_luxonis_cloud`, `processor` (a coarse family from
[normalized_processor](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/context.md)),
`cpu_count`, and `is_docker`. |

### function `system_context_provider`

```python
def system_context_provider(_telemetry: object) -> dict[str, Any]
```

Context provider that exposes extended runtime metadata.

## Module Attributes

| Name | Description |
| --- | --- |
|
[`RESERVED_METADATA_KEYS`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/context.md)
| |

### constant `RESERVED_METADATA_KEYS`

```python
RESERVED_METADATA_KEYS = frozenset(
    {'$process_person_profile', '$session_id', 'source_product', 'source_component', 'sdk_version'},
)
```