# singleton

Python API: `luxonis_ml.telemetry.singleton`

## Classes

| Name | Description |
| --- | --- |
|
[`TelemetryKey`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/singleton.md)
| |

### class `TelemetryKey`

```python
class TelemetryKey
```

Attributes

| Name | Type | Description |
| --- | --- | --- |
| `library_name` | `str` |  |
| `source_component` | `str` |  |

## Functions

| Name | Description |
| --- | --- |
|
[`get_or_init`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/singleton.md)
| Return an existing telemetry instance or initialize one. |
|
[`get_telemetry`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/singleton.md)
| Return a telemetry instance by singleton identity. |
|
[`initialize_telemetry`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/singleton.md)
| Initialize and return a telemetry instance for one emitter. |
|
[`shutdown_on_exit`](https://docs.luxonis.com/software-v3/ai-inference/model-source/training/luxonis-ml/luxonis-ml-api-reference/telemetry/singleton.md)
| Register an exit handler to flush telemetry on shutdown. |

### function `get_or_init`

```python
def get_or_init(
    library_name: str,
    *,
    source_component: str | None = None,
    library_version: str | None = None,
    config: TelemetryConfig | None = None,
    context_providers: list[ContextProvider] | None = None,
    system_context_providers: list[SystemContextProvider] | None = None,
    register_exit_handler: bool = True,
) -> Telemetry
```

Return an existing telemetry instance or initialize one.

> **Note**
> A second call for the same key does not rebuild the instance, and it reconciles the arguments in two different ways:

 * `config` and `library_version` are immutable. A value that differs from the existing one is ignored, and the function logs a
   warning.
 * `context_providers` and `system_context_providers` are additive. New providers are merged into the existing instance.

This lets several integration points contribute telemetry context without a rebuild of the singleton.

Args

| Name | Type | Description | Default |
| --- | --- | --- | --- |
| `library_name` | `str` | Name of the library emitting telemetry. | required |
| `source_component` | `str | None` | Optional emitter/component name for the singleton instance. If omitted, the library name is
reused. | `None` |
| `library_version` | `str | None` | Version string for the library. | `None` |
| `config` | `TelemetryConfig | None` | Optional telemetry configuration. | `None` |
| `context_providers` | `list[ContextProvider] | None` | Callables that return extra context to attach to every event. | `None` |
| `system_context_providers` | `list[SystemContextProvider] | None` | Callables that return extra context to attach only when
system metadata is requested. | `None` |
| `register_exit_handler` | `bool` | Whether to flush telemetry on process exit. | `True` |

Returns

| Type | Description |
| --- | --- |
| `Telemetry` | The existing or newly initialized telemetry instance for the `(library_name, source_component)` key. |

### function `get_telemetry`

```python
def get_telemetry(
    library_name: str | None = None,
    *,
    source_component: str | None = None,
) -> Telemetry | None
```

Return a telemetry instance by singleton identity.

Args

| Name | Type | Description | Default |
| --- | --- | --- | --- |
| `library_name` | `str | None` | Optional library/product name to filter by. | `None` |
| `source_component` | `str | None` | Optional emitter/component name to filter by. | `None` |

Returns

| Type | Description |
| --- | --- |
| `Telemetry | None` | The matching telemetry instance when the lookup resolves to one instance. Ambiguous lookups return `None`.
|

### function `initialize_telemetry`

```python
def initialize_telemetry(
    *,
    library_name: str,
    source_component: str | None = None,
    library_version: str | None = None,
    config: TelemetryConfig | None = None,
    context_providers: list[ContextProvider] | None = None,
    system_context_providers: list[SystemContextProvider] | None = None,
    register_exit_handler: bool = True,
) -> Telemetry
```

Initialize and return a telemetry instance for one emitter.

Args

| Name | Type | Description | Default |
| --- | --- | --- | --- |
| `library_name` | `str` | Name of the library emitting telemetry. | required |
| `source_component` | `str | None` | Optional emitter/component name. If omitted, the library name is reused. | `None` |
| `library_version` | `str | None` | Optional version string for the library. | `None` |
| `config` | `TelemetryConfig | None` | Optional telemetry configuration. | `None` |
| `context_providers` | `list[ContextProvider] | None` | Optional list of context provider callables. | `None` |
| `system_context_providers` | `list[SystemContextProvider] | None` | Optional list of system context provider callables. | `None`
|
| `register_exit_handler` | `bool` | Whether to flush telemetry on process exit. | `True` |

Returns

| Type | Description |
| --- | --- |
| `Telemetry` | The initialized telemetry instance for the exact `(library_name, source_component)` key. |

### function `shutdown_on_exit`

```python
def shutdown_on_exit()
```

Register an exit handler to flush telemetry on shutdown.