# FeatureTracker

FeatureTracker node detects key points (features) on a frame and tracks them on the next frame. The valid features are obtained
from the Harris score or Shi-Tomasi. The default number of target features is 320 and the default maximum number of features is
480.

## How to place it

#### Python

```python
with dai.Pipeline() as pipeline:
    featureTracker = pipeline.create(dai.node.FeatureTracker)
```

#### C++

```cpp
dai::Pipeline pipeline;
auto featureTracker = pipeline.create<dai::node::FeatureTracker>();
```

## Inputs and Outputs

## Usage

#### Python

```python
with dai.Pipeline() as pipeline:
    featureTracker = pipeline.create(dai.node.FeatureTracker)

    # Set number of shaves and number of memory slices to maximum
    featureTracker.setHardwareResources(2, 2)
    # Specify to wait until configuration message arrives to inputConfig Input.
    featureTracker.setWaitForConfigInput(True)

    # You have to use Feature tracker in combination with
    # an image frame source - mono/color camera or xlinkIn node
```

#### C++

```cpp
dai::Pipeline pipeline;
auto featureTracker = pipeline.create<dai::node::FeatureTracker>();

// Set number of shaves and number of memory slices to maximum
featureTracker->setHardwareResources(2, 2);
// Specify to wait until configuration message arrives to inputConfig Input.
featureTracker->setWaitForConfigInput(true);

// You have to use Feature tracker in combination with
// an image frame source - mono/color camera or xlinkIn node
```

## Examples of functionality

 * [Feature Tracker](https://docs.luxonis.com/software-v3/depthai/examples/feature_tracker/feature_tracker.md)

## How it works

### Image cells

To have features all around the image, it is divided into cells which are then processed separately. Each cell has a target
feature count = frame target features / number of cells. The number of cells can be configured in horizontal and in vertical
direction. The default number of cells is 4 (horizontal) x 4 (vertical). This means that the default number of target features per
cell is: 320 / (4 * 4) = 20. Note that if an already tracked point happens to have its new coordinate in a full cell, it will not
be removed, therefore number of features can exceed this limit.

### Initial Harris Threshold

This threshold controls the minimum strength of a feature which will be detected. Setting this value to 0 enables the automatic
thresholds, which are used to adapt to different scenes. If there is a lot of texture, this value needs to be increased, to limit
the number of detected points. Each cell has its own threshold.

### Entry conditions for new features

The entry conditions for new features are:

 * features must not be too close to each other (minimum distance criteria - default value is 50, the unit of measurement being
   squared euclidean distance in pixels),
 * Harris score of the feature is high enough,
 * there is enough room in the cell for the feature (target feature count is not achieved).

### Harris Threshold for Tracked Features

Once a feature was detected and we started tracking it, we need to update its Harris score on each image. This threshold defines
the point where such a feature must be removed. The goal is to track points for as long as possible, so the conditions for entry
points are higher than the ones for already tracked points. This is why, this value is usually smaller than the detection
threshold.

### Feature Maintenance

The algorithm has to decide which feature will be removed and which will be kept in the subsequent frames. Note that tracked
features have priority over new features. It will remove the features which:

 * have too large tracking error (wasn't tracked correctly),
 * have too small Harris score (configurable threshold).

### New position calculation

A position of the previous features on the current frame can be calculated in two ways:

 1. Using the pyramidal Lucas-Kanade optical flow method.
 2. Using a dense motion estimation hardware block (Block matcher).

## Reference

### dai::node::FeatureTracker

Kind: class

FeatureTracker node. Performs feature tracking and reidentification using motion estimation between 2 consecutive frames.

#### std::shared_ptr< FeatureTrackerConfig > initialConfig

Kind: variable

Initial config to use for feature tracking.

#### Input inputConfig

Kind: variable

Input FeatureTrackerConfig message with ability to modify parameters in runtime. Default queue is non-blocking with size 4.

#### Input inputImage

Kind: variable

Input message with frame data on which feature tracking is performed. Default queue is non-blocking with size 4.

#### Output outputFeatures

Kind: variable

Outputs TrackedFeatures message that carries tracked features results.

#### Output passthroughInputImage

Kind: variable

Passthrough message on which the calculation was performed. Suitable for when input queue is set to non-blocking behavior.

#### FeatureTracker()

Kind: function

#### FeatureTracker(std::unique_ptr< Properties > props)

Kind: function

#### void setHardwareResources(int numShaves, int numMemorySlices)

Kind: function

Specify allocated hardware resources for feature tracking. 2 shaves/memory slices are required for optical flow, 1 for corner
detection only. parameters: numShaves: Number of shaves. Maximum 2.; numMemorySlices: Number of memory slices. Maximum 2.

#### DeviceNodeCRTP()

Kind: function

#### DeviceNodeCRTP(const std::shared_ptr< Device > & device)

Kind: function

#### DeviceNodeCRTP(std::unique_ptr< Properties > props)

Kind: function

#### DeviceNodeCRTP(std::unique_ptr< Properties > props, bool confMode)

Kind: function

#### DeviceNodeCRTP(const std::shared_ptr< Device > & device, std::unique_ptr< Properties > props, bool confMode)

Kind: function

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.