# Script

Script node allows users to run custom Python scripts on the device. Due to the computational resource constraints, script node
shouldn't be used for heavy computing (eg. image manipulation/CV), but for managing the flow of the pipeline (business logic).
Example use cases would be controlling nodes like
[ImageManip](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/image_manip.md),
[ColorCamera](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/color_camera.md),
[SpatialLocationCalculator](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/spatial_location_calculator.md),
decoding [NeuralNetwork](https://docs.luxonis.com/software-v3/depthai/depthai-components/nodes/neural_network.md) results, or
interfacing with GPIOs.

## How to place it

#### Python

```python
pipeline = dai.Pipeline()
script = pipeline.create(dai.node.Script)
```

#### C++

```cpp
dai::Pipeline pipeline;
auto script = pipeline.create<dai::node::Script>();
```

## Inputs and Outputs

Users can define as many inputs and outputs as they need. Inputs and outputs can be any
[components_messages](https://docs.luxonis.com/software-v3/depthai/depthai-components/messages/message_group.md) type.

## Usage

#### Python

```python
script = pipeline.create(dai.node.Script)
script.setScript("""
    import time
    import marshal
    num = 123
    node.warn(f"Number {num}") # Print to host
    x = [1, "Hello", {"Foo": "Bar"}]
    x_serial = marshal.dumps(x)
    b = Buffer(len(x_serial))
    while True:
        time.sleep(1)
        b.setData(x_serial)
        node.io['out'].send(b)
""")
script.outputs['out'].link(xout.input)

# ...
# After initializing the device, enable log levels
device.setLogLevel(dai.LogLevel.WARN)
device.setLogOutputLevel(dai.LogLevel.WARN)
```

#### C++

```cpp
auto script = pipeline.create<dai::node::Script>();
script->setScript(R"(
    import time
    import marshal
    num = 123
    node.warn(f"Number {num}") # Print to host
    x = [1, "Hello", {"Foo": "Bar"}]
    x_serial = marshal.dumps(x)
    b = Buffer(len(x_serial))
    while True:
        time.sleep(1)
        b.setData(x_serial)
        node.io['out'].send(b)
)");
script->outputs["out"].link(xout->input);

// ...
// After initializing the device, enable log levels
device.setLogLevel(dai::LogLevel.WARN);
device.setLogOutputLevel(dai::LogLevel.WARN);
```

## Interfacing with GPIOs

In the script node you can interface with GPIOs of the VPU using module GPIO. Currently supported functions are:

```python
# Module
import GPIO

# General
GPIO.setup(gpio, dir, pud, exclusive)
GPIO.release(gpio)
GPIO.write(gpio, value)
GPIO.read(gpio)

# Interrupts
GPIO.waitInterruptEvent(gpio = -1) # blocks until any interrupt or interrupt by specified gpio is fired. Interrupts with callbacks are ignored here
GPIO.hasInterruptEvent(gpio = -1) # returns whether interrupt happened on any or specified gpio. Interrupts with callbacks are ignored here
GPIO.setInterrupt(gpio, edge, priority, callback = None) # adds interrupt to specified pin
GPIO.clearInterrupt(gpio) # clears interrupt of specified pin

# PWM
GPIO.setPwm(gpio, highCount, lowCount, repeat=0) # repeat == 0 means indefinite
GPIO.enablePwm(gpio, enable)

# Enumerations
GPIO.Direction: GPIO.IN, GPIO.OUT
GPIO.State: GPIO.LOW, GPIO.HIGH
GPIO.PullDownUp: GPIO.PULL_NONE, GPIO.PULL_DOWN, GPIO.PULL_UP
GPIO.Edge: GPIO.RISING, GPIO.FALLING, GPIO.LEVEL_HIGH, GPIO.LEVEL_LOW
```

Here's an example of toggling GPIO pin 40 inside Script node from the host. On
[OAK-SoM-Pro](https://shop.luxonis.com/products/oak-som-pro), GPIO 40 drives FSYNC signal for both 4-lane cameras, and we have
used the code below for this exact reason.

```python
import GPIO
MX_PIN = 40

ret = GPIO.setup(MX_PIN, GPIO.OUT, GPIO.PULL_DOWN)
toggleVal = True

while True:
  data = node.io['in'].get()  # Wait for a message from the host computer

  node.warn('GPIO toggle: ' + str(toggleVal))
  toggleVal = not toggleVal
  ret = GPIO.write(MX_PIN, toggleVal)  # Toggle the GPIO
```

## Time synchronization

Script node has access to both device (internal) clock and also synchronized host clock. Host clock is synchronized with device
clock at below 2.5ms precision at 1σ, [Host clock
syncing](https://docs.luxonis.com/software-v3/depthai/depthai-components/device.md).

```python
import time
interval = 60
ctrl = CameraControl()
ctrl.setCaptureStill(True)
previous = 0
while True:
    time.sleep(0.001)

    tnow_full = Clock.nowHost() # Synced clock with host
    # Clock.now() -> internal/device clock
    # Clock.offsetToHost() -> Offset between internal/device clock and host clock

    now = tnow_full.seconds
    if now % interval == 0 and now != previous:
        previous = now
        node.warn(f'{tnow_full}')
        node.io['out'].send(ctrl)
```

## Using DepthAI [Messages](https://docs.luxonis.com/software-v3/depthai/depthai-components/messages.md)

The depthai module is implicitly imported to the script node. You can create new depthai messages and assign data to it, for
example:

```python
buf = Buffer(100) # Assign 100 bytes to the Buffer message

# Create CameraControl message, set manual focus
control = CameraControl()
control.setManualFocus(100)

imgFrame = ImgFrame(300*300*3) # Buffer with 300x300x3 bytes
```

## Available modules and libraries

#### RVC2

Available modules

```text
"posix", "errno", "pwd", "_sre", "_codecs", "_weakref", "_functools", "_operator",
"_collections", "_abc", "itertools", "atexit", "_stat", "time", "_datetime", "math",
"_thread", "_io", "_symtable", "marshal", "_ast", "gc", "_warnings", "_string", "_struct"
```

Available Modules for LEON_CSS:

```text
"binascii", "_random", "_socket", "_md5", "_sha1", "_sha256", "_sha512", "select",
"array", "unicodedata"
```

Libraries

```text
"__main__", "_collections_abc", "_frozen_importlib", "_frozen_importlib_external",
"_sitebuiltins", "abc", "codecs", "datetime", "encodings", "encodings.aliases",
"encodings.ascii", "encodings.latin_1", "encodings.mbcs", "encodings.utf_8", "genericpath",
"io", "os", "posixpath", "site", "stat", "threading", "types", "struct", "copyreg",
"reprlib", "operator", "keyword", "heapq", "collections", "functools", "sre_constants",
"sre_parse", "sre_compile", "enum", "re", "json", "json.decoder", "json.encoder",
"json.scanner", "textwrap"
```

Libraries for LEON_CSS:

```text
"http", "http.client", "http.server", "html", "mimetypes", "copy", "shutil", "fnmatch",
"socketserver", "contextlib", "email", "email._encoded_words", "email._header_value_parser",
"email._parseaddr", "email._policybase", "email.base64mime", "email.charset",
"email.contentmanager",  "email.encoders", "email.errors", "email.feedparser",
"email.generator", "email.header", "email.headerregistry", "email.iterators", "email.message",
"email.parser", "email.policy", "email.quoprimime", "email.utils", "string", "base64",
"quopri", "random", "warnings", "bisect", "hashlib", "logging", "traceback", "linecache",
"socket", "token", "tokenize", "weakref", "_weakrefset", "collections.abc", "selectors",
"urllib", "urllib.parse", "calendar", "locale", "uu", "encodings.idna", "stringprep"
```

The difference between module and library is that module is a precompiled C source with Python bindings, whereas library is Python
source code packed into a library and precompiled into Python bytecode (before loaded into our Firmware). Networking/protocol
modules/libraries that are available on the LEON_CSS can only be used on [OAK POE
device](https://docs.luxonis.com/hardware.md#poe-designs). You can specify on which processor the script will run, eg. for
LEON_CSS:

```python
script = pipeline.create(dai.node.Script)
script.setProcessor(dai.ProcessorType.LEON_CSS)
```

#### RVC4

Script node on the OAK4 is using the base python environment, which means that all modules and libraries that are available in the
base python environment are also available in the script node. To add additional modules or libraries, you can use the pip command
in the base python environment.

## Examples of functionality

 * [Script simple](https://docs.luxonis.com/software-v3/depthai/examples/script/script_simple.md) - Simple example of using Script
   node to send and receive messages.
 * [Script switch cameras](https://docs.luxonis.com/software-v3/depthai/examples/script/script_switch_all_cameras.md) - Example of
   using Script node to switch between multiple cameras.

## Reference

### dai::node::Script

Kind: class

#### InputMap inputs

Kind: variable

Inputs to Script node. Can be accessed using subscript operator (Eg: inputs['in1']) By default inputs are set to blocking with
queue size 8

#### OutputMap outputs

Kind: variable

Outputs from Script node. Can be accessed subscript operator (Eg: outputs['out1'])

#### void setScriptPath(const std::filesystem::path & path, const std::string & name)

Kind: function

Specify local filesystem path to load the script parameters: path: Filesystem path to load the script; name: Optionally set a name
of this script, otherwise the name defaults to the path

#### void setScript(const std::string & script, const std::string & name)

Kind: function

Sets script data to be interpreted parameters: script: Script string to be interpreted; name: Optionally set a name of this script

#### void setScript(const std::vector< std::uint8_t > & data, const std::string & name)

Kind: function

Sets script data to be interpreted parameters: data: Binary data that represents the script to be interpreted; name: Optionally
set a name of this script

#### std::filesystem::path getScriptPath()

Kind: function

Get filesystem path from where script was loaded.

return: std::filesystem::path from where script was loaded, otherwise returns empty path

#### std::string getScriptName()

Kind: function

Get the script name in utf-8.

When name set with setScript() or setScriptPath() , returns that name. When script loaded with setScriptPath() with name not
provided, returns the utf-8 string of that path. Otherwise, returns "<script>" return: std::string of script name in utf-8

#### void setProcessor(ProcessorType type)

Kind: function

Set on which processor the script should run parameters: type: Processor type - Leon CSS or Leon MSS

#### ProcessorType getProcessor()

Kind: function

Get on which processor the script should run return: Processor type - Leon CSS or Leon MSS

#### void buildInternal()

Kind: function

Function called from within the

#### void buildStage1()

Kind: function

Build stages;.

#### DeviceNodeCRTP()

Kind: function

#### DeviceNodeCRTP(const std::shared_ptr< Device > & device)

Kind: function

#### DeviceNodeCRTP(std::unique_ptr< Properties > props)

Kind: function

#### DeviceNodeCRTP(std::unique_ptr< Properties > props, bool confMode)

Kind: function

#### DeviceNodeCRTP(const std::shared_ptr< Device > & device, std::unique_ptr< Properties > props, bool confMode)

Kind: function

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.