Bootloader Version
We suggest using Device Manager, a GUI tool for interfacing with the bootloader and its configurations.
Demo
Command Line
1~/depthai-python/examples$ python3 bootloader_version.py
2 Found device with name: 1.1
3 Version: 0.0.26
4 USB Bootloader - supports only Flash memory
5 Memory 'Memory.FLASH' size: 33554432, info: JEDEC ID: 01 02 19Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import depthai as dai
4
5(res, info) = dai.DeviceBootloader.getFirstAvailableDevice()
6
7if res == True:
8 print(f'Found device with name: {info.name}')
9 bl = dai.DeviceBootloader(info)
10 print(f'Version: {bl.getVersion()}')
11
12 supportedMemTypes = [dai.DeviceBootloader.Memory.FLASH, dai.DeviceBootloader.Memory.EMMC]
13 if bl.getType() == dai.DeviceBootloader.Type.USB:
14 print("USB Bootloader - supports only Flash memory")
15 supportedMemTypes = [dai.DeviceBootloader.Memory.FLASH];
16 else:
17 print(f"NETWORK Bootloader, is User Bootloader: {bl.isUserBootloader()}")
18
19 try:
20 for mem in supportedMemTypes:
21 memInfo = bl.getMemoryInfo(mem)
22 if memInfo.available:
23 print(f"Memory '{mem}' size: {memInfo.size}, info: {memInfo.info}")
24 appInfo = bl.readApplicationInfo(mem)
25 if appInfo.hasApplication:
26 print(f"Application name: {appInfo.applicationName}, firmware version: {appInfo.firmwareVersion}")
27 else:
28 print(f"Memory '{mem.name}' not available...")
29 except Exception as ex:
30 print(f"Couldn't retrieve memory details: {ex}")
31else:
32 print('No devices found')Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.