Calibration Reader
This example shows how to read calibration data stored on device over XLink. This example will print camera extrinsic and intrinsic parameters, along with other calibration values written on device (EEPROM).Similar samples
Camera intrinsics
Calibration also contains camera intrinsics and extrinsics parameters.Command Line
1import depthai as dai
2
3with dai.Device() as device:
4 calibData = device.readCalibration()
5 intrinsics = calibData.getCameraIntrinsics(dai.CameraBoardSocket.RIGHT)
6 print('Right mono camera focal length in pixels:', intrinsics[0][0])
Python
1f_x = width * (1 / (2 * math.tan((HFOV / 2) * (math.pi / 180))))
Code
1f_x_640 = 640 * (1 / (2 * math.tan((71.9 / 2) * (math.pi / 180)))) # = 441.25
Code
1f_x_1280 = 1280 * (1 / (2 * math.tan((71.9 / 2) * (math.pi / 180)))) # = 882.5
Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import depthai as dai
4import numpy as np
5import sys
6from pathlib import Path
7
8# Connect Device
9with dai.Device() as device:
10 calibFile = str((Path(__file__).parent / Path(f"calib_{device.getMxId()}.json")).resolve().absolute())
11 if len(sys.argv) > 1:
12 calibFile = sys.argv[1]
13
14 calibData = device.readCalibration()
15 calibData.eepromToJsonFile(calibFile)
16
17 M_rgb, width, height = calibData.getDefaultIntrinsics(dai.CameraBoardSocket.CAM_A)
18 print("RGB Camera Default intrinsics...")
19 print(M_rgb)
20 print(width)
21 print(height)
22
23 if "OAK-1" in calibData.getEepromData().boardName or "BW1093OAK" in calibData.getEepromData().boardName:
24 M_rgb = np.array(calibData.getCameraIntrinsics(dai.CameraBoardSocket.CAM_A, 1280, 720))
25 print("RGB Camera resized intrinsics...")
26 print(M_rgb)
27
28 D_rgb = np.array(calibData.getDistortionCoefficients(dai.CameraBoardSocket.CAM_A))
29 print("RGB Distortion Coefficients...")
30 [print(name + ": " + value) for (name, value) in
31 zip(["k1", "k2", "p1", "p2", "k3", "k4", "k5", "k6", "s1", "s2", "s3", "s4", "τx", "τy"],
32 [str(data) for data in D_rgb])]
33
34 print(f'RGB FOV {calibData.getFov(dai.CameraBoardSocket.CAM_A)}')
35
36 else:
37 M_rgb, width, height = calibData.getDefaultIntrinsics(dai.CameraBoardSocket.CAM_A)
38 print("RGB Camera Default intrinsics...")
39 print(M_rgb)
40 print(width)
41 print(height)
42
43 M_rgb = np.array(calibData.getCameraIntrinsics(dai.CameraBoardSocket.CAM_A, 3840, 2160))
44 print("RGB Camera resized intrinsics... 3840 x 2160 ")
45 print(M_rgb)
46
47
48 M_rgb = np.array(calibData.getCameraIntrinsics(dai.CameraBoardSocket.CAM_A, 4056, 3040 ))
49 print("RGB Camera resized intrinsics... 4056 x 3040 ")
50 print(M_rgb)
51
52
53 M_left, width, height = calibData.getDefaultIntrinsics(dai.CameraBoardSocket.CAM_B)
54 print("LEFT Camera Default intrinsics...")
55 print(M_left)
56 print(width)
57 print(height)
58
59 M_left = np.array(calibData.getCameraIntrinsics(dai.CameraBoardSocket.CAM_B, 1280, 720))
60 print("LEFT Camera resized intrinsics... 1280 x 720")
61 print(M_left)
62
63
64 M_right = np.array(calibData.getCameraIntrinsics(dai.CameraBoardSocket.CAM_C, 1280, 720))
65 print("RIGHT Camera resized intrinsics... 1280 x 720")
66 print(M_right)
67
68 D_left = np.array(calibData.getDistortionCoefficients(dai.CameraBoardSocket.CAM_B))
69 print("LEFT Distortion Coefficients...")
70 [print(name+": "+value) for (name, value) in zip(["k1","k2","p1","p2","k3","k4","k5","k6","s1","s2","s3","s4","τx","τy"],[str(data) for data in D_left])]
71
72 D_right = np.array(calibData.getDistortionCoefficients(dai.CameraBoardSocket.CAM_C))
73 print("RIGHT Distortion Coefficients...")
74 [print(name+": "+value) for (name, value) in zip(["k1","k2","p1","p2","k3","k4","k5","k6","s1","s2","s3","s4","τx","τy"],[str(data) for data in D_right])]
75
76 print(f"RGB FOV {calibData.getFov(dai.CameraBoardSocket.CAM_A)}, Mono FOV {calibData.getFov(dai.CameraBoardSocket.CAM_B)}")
77
78 R1 = np.array(calibData.getStereoLeftRectificationRotation())
79 R2 = np.array(calibData.getStereoRightRectificationRotation())
80 M_right = np.array(calibData.getCameraIntrinsics(calibData.getStereoRightCameraId(), 1280, 720))
81
82 H_left = np.matmul(np.matmul(M_right, R1), np.linalg.inv(M_left))
83 print("LEFT Camera stereo rectification matrix...")
84 print(H_left)
85
86 H_right = np.matmul(np.matmul(M_right, R1), np.linalg.inv(M_right))
87 print("RIGHT Camera stereo rectification matrix...")
88 print(H_right)
89
90 lr_extrinsics = np.array(calibData.getCameraExtrinsics(dai.CameraBoardSocket.CAM_B, dai.CameraBoardSocket.CAM_C))
91 print("Transformation matrix of where left Camera is W.R.T right Camera's optical center")
92 print(lr_extrinsics)
93
94 l_rgb_extrinsics = np.array(calibData.getCameraExtrinsics(dai.CameraBoardSocket.CAM_B, dai.CameraBoardSocket.CAM_A))
95 print("Transformation matrix of where left Camera is W.R.T RGB Camera's optical center")
96 print(l_rgb_extrinsics)
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.