Casting NN subtraction
Demo
This example requires the DepthAI v3 API, see installation instructions.Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3import cv2
4import depthai as dai
5from pathlib import Path
6
7SHAPE = 720
8
9p = dai.Pipeline()
10
11camRgb = p.create(dai.node.ColorCamera)
12nn = p.create(dai.node.NeuralNetwork)
13script = p.create(dai.node.Script)
14rgbXout = p.create(dai.node.XLinkOut)
15cast = p.create(dai.node.Cast)
16castXout = p.create(dai.node.XLinkOut)
17
18camRgb.setVideoSize(SHAPE, SHAPE)
19camRgb.setPreviewSize(SHAPE, SHAPE)
20camRgb.setInterleaved(False)
21
22nnBlobPath = (Path(__file__).parent / Path('../models/diff_openvino_2022.1_6shave.blob')).resolve().absolute()
23nn.setBlobPath(nnBlobPath)
24
25script.setScript("""
26old = node.io['in'].get()
27while True:
28 frame = node.io['in'].get()
29 node.io['img1'].send(old)
30 node.io['img2'].send(frame)
31 old = frame
32""")
33
34rgbXout.setStreamName("rgb")
35castXout.setStreamName("cast")
36cast.setOutputFrameType(dai.RawImgFrame.Type.GRAY8)
37
38# Linking
39camRgb.preview.link(script.inputs['in'])
40script.outputs['img1'].link(nn.inputs['img1'])
41script.outputs['img2'].link(nn.inputs['img2'])
42camRgb.video.link(rgbXout.input)
43nn.out.link(cast.input)
44cast.output.link(castXout.input)
45
46# Pipeline is defined, now we can connect to the device
47with dai.Device(p) as device:
48 qCam = device.getOutputQueue(name="rgb", maxSize=4, blocking=False)
49 qCast = device.getOutputQueue(name="cast", maxSize=4, blocking=False)
50
51
52 while True:
53 colorFrame = qCam.get()
54 assert isinstance(colorFrame, dai.ImgFrame)
55 cv2.imshow("Color", colorFrame.getCvFrame())
56
57 inCast = qCast.get()
58 assert isinstance(inCast, dai.ImgFrame)
59 cv2.imshow("Diff", inCast.getCvFrame())
60
61 if cv2.waitKey(1) == ord('q'):
62 breakPipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.