Multi-Input Frame Concatenation
Demo

Setup
Source code
Python
C++
Python
PythonGitHub
1#!/usr/bin/env python3
2
3from pathlib import Path
4import sys
5import numpy as np
6import cv2
7import depthai as dai
8SHAPE = 300
9
10# Get argument first
11nnPath = str((Path(__file__).parent / Path('../models/concat_openvino_2021.4_6shave.blob')).resolve().absolute())
12if len(sys.argv) > 1:
13 nnPath = sys.argv[1]
14
15if not Path(nnPath).exists():
16 import sys
17 raise FileNotFoundError(f'Required file/s not found, please run "{sys.executable} install_requirements.py"')
18
19p = dai.Pipeline()
20p.setOpenVINOVersion(dai.OpenVINO.VERSION_2021_4)
21
22camRgb = p.createColorCamera()
23camRgb.setPreviewSize(SHAPE, SHAPE)
24camRgb.setInterleaved(False)
25camRgb.setColorOrder(dai.ColorCameraProperties.ColorOrder.BGR)
26
27def create_mono(p, socket):
28 mono = p.create(dai.node.MonoCamera)
29 mono.setBoardSocket(socket)
30 mono.setResolution(dai.MonoCameraProperties.SensorResolution.THE_400_P)
31
32 # ImageManip for cropping (face detection NN requires input image of 300x300) and to change frame type
33 manip = p.create(dai.node.ImageManip)
34 manip.initialConfig.setResize(300, 300)
35 manip.initialConfig.setFrameType(dai.RawImgFrame.Type.BGR888p)
36 mono.out.link(manip.inputImage)
37 return manip.out
38
39# NN that detects faces in the image
40nn = p.createNeuralNetwork()
41nn.setBlobPath(nnPath)
42nn.setNumInferenceThreads(2)
43
44camRgb.preview.link(nn.inputs['img2'])
45create_mono(p, dai.CameraBoardSocket.CAM_B).link(nn.inputs['img1'])
46create_mono(p, dai.CameraBoardSocket.CAM_C).link(nn.inputs['img3'])
47
48# Send bouding box from the NN to the host via XLink
49nn_xout = p.createXLinkOut()
50nn_xout.setStreamName("nn")
51nn.out.link(nn_xout.input)
52
53# Pipeline is defined, now we can connect to the device
54with dai.Device(p) as device:
55 qNn = device.getOutputQueue(name="nn", maxSize=4, blocking=False)
56 shape = (3, SHAPE, SHAPE * 3)
57
58 while True:
59 inNn = np.array(qNn.get().getFirstLayerFp16())
60 # Planar INT8 frame
61 frame = inNn.reshape(shape).astype(np.uint8).transpose(1, 2, 0)
62
63 cv2.imshow("Concat", frame)
64
65 if cv2.waitKey(1) == ord('q'):
66 breakPipeline
Need assistance?
Head over to Discussion Forum for technical support or any other questions you might have.