# Crash report

In case of a firmware crash, OAK cameras will automatically generate a crash report and store it in the device. The crash report
contains information about the crash, such as the stack trace, the device's configuration, and the device's state at the time of
the crash. The crash report can be read from the device and sent to Luxonis for debugging purposes.

## Demo

In case a crash report was found on the device, this example will read it and save it to a json file:

```bash
> python crash_report.py
    Crash dump found on your device!
    Saved to crashDump_0_184430102163DB0F00_3575b77f20e796b4e79953bf3d2ba22f0416ee8b.json
    Please report to developers!
```

Please send the crash reports together [with an MRE](https://stackoverflow.com/help/minimal-reproducible-example) (DepthAI issue)
to our [Discuss Forum](https://discuss.luxonis.com/). Thank you!

## Setup

This example requires the DepthAI v3 API, see [installation instructions](https://docs.luxonis.com/software-v3/depthai.md).

## Source code

#### Python

```python
#!/usr/bin/env python3

import cv2
import depthai as dai
from json import dump
from os.path import exists

# Connect to device and start pipeline
with dai.Device() as device:

    if device.hasCrashDump():
        crashDump = device.getCrashDump()
        commitHash = crashDump.depthaiCommitHash
        deviceId = crashDump.deviceId

        json = crashDump.serializeToJson()
        
        i = -1
        while True:
            i += 1
            destPath = "crashDump_" + str(i) + "_" + deviceId + "_" + commitHash + ".json"
            if exists(destPath):
                continue

            with open(destPath, 'w', encoding='utf-8') as f:
                dump(json, f, ensure_ascii=False, indent=4)

            print("Crash dump found on your device!")
            print(f"Saved to {destPath}")
            print("Please report to developers!")
            break
    else:
        print("There was no crash dump found on your device!")
```

#### C++

```cpp
#include <fstream>
#include <iostream>

// Includes common necessary includes for development using depthai library
#include "depthai/depthai.hpp"

static bool fileExists(dai::Path path) {
    std::ifstream file(path);
    return file.is_open();
}

int main() {
    using namespace std;

    // Connect to device and start pipeline
    dai::Device device;
    if(device.hasCrashDump()) {
        auto crashDump = device.getCrashDump();
        std::string commitHash = crashDump.depthaiCommitHash;
        std::string deviceId = crashDump.deviceId;

        auto json = crashDump.serializeToJson();

        for(int i = 0;; i++) {
            dai::Path destPath = "crashDump_" + to_string(i) + "_" + deviceId + "_" + commitHash + ".json";
            if(fileExists(destPath)) continue;

            std::ofstream ob(destPath);
            ob << std::setw(4) << json << std::endl;

            std::cout << "Crash dump found on your device!" << std::endl;
            std::cout << "Saved to " << destPath.string() << std::endl;
            std::cout << "Please report to developers!" << std::endl;
            break;
        }
    } else {
        std::cout << "There was no crash dump found on your device!" << std::endl;
    }

    return 0;
}
```

### Need assistance?

Head over to [Discussion Forum](https://discuss.luxonis.com/) for technical support or any other questions you might have.